Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Bluetooth Forum Discussions

user_2112781
Level 4
10 likes received 10 likes given 5 likes given
Level 4

Hello,

I would like to change the BLE address  of the device but directly from the device running itself.

I know that the address is stored in the EEPROM in the DS1 at offset 0xFF000015 to 0xFF00001b and I can change it directly via bleappfwu_writeMem and when I reboot I indeed get the desired address.

But is there a better way to change the value of the BLE address stored in the EEPROM ? I found blecm_set_static_random_bd_addr but once again, the address must be set to 0xffffffffffff in the EEPROM before calling it.

0 Likes
1 Solution
VictorZ_46
Employee
5 comments on blog 25 sign-ins 250 likes received
Employee

You shall not change device bdaddr on every reboot.  And you should not change address by writing into a hardcoded memory address.  You can use blecm_set_static_random_bd_addr function.  As you correctly noticed this generates a random address and saves it in the NVRAM.  But in addition to that, device type is changed from public to private.  The address should not be changed for the lifetime of the device.  Otherwise you will be violating Bluetooth SIG policy.

View solution in original post

0 Likes
11 Replies
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

I have asked the developers if they could respond and verify this functionality is supported within the SDK.

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

Note that I confirmed with the developers that what you are trying to accomplish through the API changing the BD_ADDR is unsupported.

0 Likes
user_2112781
Level 4
10 likes received 10 likes given 5 likes given
Level 4

Thank you for your answer.

Just to be clear,  I don't want to change it dynamically and keep the device running with the new address.  I would just like to be able to change it and have it up and and running after reboot. This works when I first set the address to FFFFFFFFFFFF then upload the firmware to the board and call blecm_set_static_random_bd_addr,  I get a new random address but I can't call this a second time as I would need to set the address again to FFFFFFFFFFFF.

0 Likes
VictorZ_46
Employee
5 comments on blog 25 sign-ins 250 likes received
Employee

You shall not change device bdaddr on every reboot.  And you should not change address by writing into a hardcoded memory address.  You can use blecm_set_static_random_bd_addr function.  As you correctly noticed this generates a random address and saves it in the NVRAM.  But in addition to that, device type is changed from public to private.  The address should not be changed for the lifetime of the device.  Otherwise you will be violating Bluetooth SIG policy.

0 Likes
user_2112781
Level 4
10 likes received 10 likes given 5 likes given
Level 4

victorz, the address type does not seem to be changed, I always see it as public (0x0).

Can we change the address type advertised ?

0 Likes
StBa_721356
Level 5
50 likes received 25 likes received 10 likes received
Level 5

I guess one can use blecm_startAdv() to specify if the own address is random by setting the advAdrType parameter to 1.

See the documentation of blecm_startAdv() in Connectable vs. nonconnectable Advertisements.

hachc_2137126
Level 5
10 likes given 5 likes given First like received
Level 5

Hi victorz,

  Regarding to your description here

You shall not change device bdaddr on every reboot.

  I don't see the same expression from the BT spec as below, which is cited from section 10.8.1 of Part C. of Volume 3.

A device may choose to initialize its static address to a new value after each

power cycle. A device shall not change its static address value once initialized

until the device is power cycled.

Note: If the static address of a device is changed then the address stored in

peer devices will not be valid and the ability to reconnect using the old address

will be lost.

  So, if we need to change the BD address in every reboot, then what would be the limit of write cycle to EEPROM that storing the BD_ADDRESS, in case that we need to write it to '0xFFFFFFFFFFFF' before calling 'blecm_set_static_random_bd_addr'?

0 Likes
ShengY_96
Employee
50 likes received 25 likes received 10 likes received
Employee

The API: blecm_set_static_random_bd_addr() is undefined with SDK: WICED-Smart-SDK 2.2.3.

Which version of SDK contain this API? Could you please share a demo code if convenient?

0 Likes
MichaelF_56
Moderator
Moderator 250 sign-ins 25 comments on blog 10 comments on blog
Moderator

I think what you are referring to is called a resolvable private address (RPA) and it is currently unsupported.


RPA is a feature that allows your device to change it's BD_ADDR such that a paired device can still understand it's the same device.  I believe that an iOS device supports RPA and changes the BD_ADDR every 15 minutes.  It can do this because during the pairing process a special key is distributed to the peer.  Therefore, when a peer sees the advertisement from the iPhone, it can decode the BD_ADDR and understand that it is the same device that it was paired with initially.

The BCM20736/7 supports connections from devices that change BD_ADDRs in this manner, however, these devices do not have logic built in to change their own BD_ADDR.

victorz

0 Likes
Anonymous
Not applicable

Hello all,

I am using the EEPROM with normal OTA settings as recommended (SS1,SS2,DS1,DS2).

I know that the BLE address is stored in the EEPROM in the DS1 at offset 0xFF000015 to 0xFF00001b and I can change it directly via bleappfwu_writeMem and when I reboot I indeed get the desired address.

HOWEVER if we are running in DS2 what address is the BLE address retrieved from? 0xFF000015 appears to be in SS1, is this correct? I attempted to use 0xFF000115 without success (SS2 offset applied).

I am not able to set a new BLE address when the device is running in DS2. I get a previously set address. Here is the code that writes the address

   ble_trace1("EEPROM: %d",NV_IS_EEPROM());

   if (!NV_IS_EEPROM())

   {

      // Erase sector if SF before writing.

      temp = bleappfwu_eraseMem(BD_ADDR_MEM_START, BD_ADDR_LEN);

   }

   // Write this to the active SS.

   temp = bleappfwu_writeMem(p_bd_addr, BD_ADDR_MEM_START, BD_ADDR_LEN);

   ble_trace1("Write Status: %d",temp);

0 Likes
Anonymous
Not applicable

Hello mima_1250261​,

I'm seeing the same problem.

Did you find a way to change Bluetooth address after performing OTA firmware update (SS2 is activated)?

0 Likes