Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Bluetooth Forum Discussions

Anonymous
Not applicable

I have BCM920737_LE_KIT 3ea

I would like to check a dual mode of Bluetooth 4.1

Is it possible in BCM920737_LE_KIT?

Let me how to test a dual mode topology of Bluetooth 4.1

Support multiple roles simultaneously

Dual Mode Topology

Enables a dual mode (BR/EDR-Low Energy) device such as a smartphone to act

as a Bluetooth Smart Ready Hub and Bluetooth Smart peripheral at the same time.

The device can then communicate with Bluetooth Smart peripherals on one side

and another Bluetooth Smart Ready hub device on the other side.

Link Layer Topology

Manages the connections between the devices used in a Dual Mode Topology

implementation (see Dual Mode Topology description).

0 Likes
1 Solution

This thread summarizes the feature: Additional master/slave questions on BCM20736/7 family

To investigate our support for Simultaneous Master/Slave, take a look at the hello_client and hello_sensor applications within the SDK.

View solution in original post

0 Likes
3 Replies
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

the 2073x solns discussed in this forum are ble only. if you can get hold of a 20702 dongle, it is a dual mode device...

0 Likes
Anonymous
Not applicable

BCM2073X PRODUCT MATRIX

20737's FEATURE is

On-chip stack, ARM Cortex M3,

1.2V operation, wireless charging,

simultaneous central and peripheral

operation, NFC pairing, RSA security

library, LE audio

I would like to test 'simultaneous central and peripheral operation'

0 Likes

This thread summarizes the feature: Additional master/slave questions on BCM20736/7 family

To investigate our support for Simultaneous Master/Slave, take a look at the hello_client and hello_sensor applications within the SDK.

0 Likes