- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Where are the options to control the PA/LNA on the CYBT-483039-02 documented?
The instructions to enable the PA to increase transmit power are provided in
Are there additional commands?
- How to disable the Power Amp
- How to enable the Low Noise Amp
- How to disable the Low Noise Amp
Are there recommendations on chip power output when using PA/LNA to maximize transmit power or receive sensitivity?
Are there additional notes to control power of the base CYW20719 chip?
- A summary of the chip power options is @ Change List CYW20719-B1 and CYW20719-B2
- Methods to communicate and change chip power @ BLE Proximity Profile - CYW20719 / CYW20735 and How to change the frequency & power level of 20719 with some additional links to additional support and more comments
Reference the PA/LNA datasheet https://www.skyworksinc.com/-/media/SkyWorks/Documents/Products/2301-2400/RFX2401C_204359B.pdf
Aside: It's not clear which chip CYW20719-B1 or CYW20719-B2 in on the CYBT-483039-02 module Reference Which version of CYW20719 is on CYBT-483039-02 ??
Greg
Solved! Go to Solution.
- Tags:
- ble pa enabled
- cybt-483039-02
- cyw20719
- cyw20719-b1
- cyw20719-based
- cyw20719b1
- cyw20719b2
- external pa
- low noise amplifier
- power amplifier
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi GrCa_1363456 ,
1) How to disable the Power Amp , How to enable the Low Noise Amp , How to disable the Low Noise Amp
A: No, there are no additional commands. The PA/LNA for this module is not a configurable device, it is a boost for outgoing and incoming signals.
If you disable the PA/LNA, you will not have any BT/BLE activity. There is no option for passthrough for the PA/LNA on this module.
The KBA does not tell how to turn on the PA/LNA, it describes how to enable the interface for the TX and RX signals to the PA/LNA. Without the signaling, the output power would be significantly degraded. The PA/LNA for this module is always on, but the boost for the output will not occur without the control lines enabled and running in sync with the CYW20719 silicon Bluetooth interface.
2)
The CYW20719 has a maximum output power of +4dBm. To maximize the output power, you would set the silicon device output power to the maximum level and the PA/LNA will boost this by the defined PA amount, which is a maximum of 25dB boost. The boost is not configurable, the maximum term is because there is part to part variation for the PA/LNA. NOTE that if you do boost the module to 4 + 25 dBm = 29dBm, you will be in violation of a number of regulatory limits. To this end, the output power for 20dBm is the limit for US and Canada, 10dBm is the limit for most other regions that leverage ETSI requirements. NOTE that the saturated output power of the PA/LNA is 22dBm, so even if you configure to greater than this, it will be saturated and will not be able to output more than 22dBm. The 25dBm boost still applies, because you can have a negative signal inputted and it will boost it by the maximum amount not to exceed 22dBm total Pout.
Please Note: If the customer is looking to have high power and low power in the same module, this is not the best part for them as it is design to specifically boost to the maximum allowable output power for BT/BLE.
Thanks,
Anjana