Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

hachc_2293006
Level 2
Level 2
First like received First like given

Scenario:

Design is to detect probe. If no probe absent, enter Sleep/Low Power Mode for 6 seconds and repeat

If probe is present, then Enable BLE Timer for 1sec.

On first entry to 1 sec timer call back. Abort Low Pwer mode.

Measure probe,  enable ADVertisement and wait for pairign etc.

Issue: We do not get registered even call back for BLECM_APP_EVT_LINK_UP alone

But all other event callback (BLECM_APP_EVT_LINK_UP and BLECM_APP_EVT_ADV_TIMEOUT ) are called back properly.

Note: Tried executing without calling

        bleprofile_enteringDiscLowPowerMode(DEV_LPM_DISC_LOW_POWER_MODES_SLEEP); and

        bleprofile_abortingDiscLowPowerMode(DEV_LPM_DISC_LOW_POWER_MODES_SLEEP);

in code

Then, in this case all 3 registered app event are called.

--------------------------------------------------------------------------------------------------------------

Code:

On create()

{

.................

    bleprofile_Init(bleprofile_p_cfg);

    bleprofile_GPIOInit(bleprofile_gpio_p_cfg);

.

.......

// register connection up and connection down handler.

    bleprofile_regAppEvtHandler(BLECM_APP_EVT_LINK_DOWN, cookp_connection_down);

    bleprofile_regAppEvtHandler(BLECM_APP_EVT_LINK_UP, cookp_connection_up);

    bleprofile_regAppEvtHandler(BLECM_APP_EVT_ADV_TIMEOUT, cookp_advertisement_stopped);

.............

    // Low powe mode initialize

    devlpm_init();

    devlpm_registerForLowPowerQueries(cookp_lpm_queriable, 0);

    bleprofile_enteringDiscLowPowerMode(DEV_LPM_DISC_LOW_POWER_MODES_SLEEP);

}

UINT32 cookp_lpm_queriable(LowPowerModePollType type, UINT32 context)

{

  if(!cp_lp_abort){

    if(cookp_probe_chk()){

       ble_trace0("LPQ No");

       cookp_reg_timer();

       return 0;

    }

    else {

     ble_trace0("LPQ yes");

     return 1000000 * 6;

   }

  }

  return 0;

}

void timer_cb()

{

      if(!cp_lp_abort){ /* if probe detected on wake up */

       cp_lp_abort = TRUE;

       bleprofile_abortingDiscLowPowerMode(DEV_LPM_DISC_LOW_POWER_MODES_SLEEP);

      }

..................

}

const BLE_PROFILE_CFG cookp_cfg =

{

    /*.fine_timer_interval            =*/ 500, //COOKP_FINE_TIMER, // ms    Note: tried with and without Fine timer , same result

    /*.default_adv                    =*/ HIGH_UNDIRECTED_DISCOVERABLE,

    /*.button_adv_toggle              =*/ 0,    // pairing button make adv toggle (if 1) or always on (if 0)

    /*.high_undirect_adv_interval     =*/ 32,   // slots

    /*.low_undirect_adv_interval      =*/ 1024, // slots

    /*.high_undirect_adv_duration     =*/ 10,   // seconds

    /*.low_undirect_adv_duration      =*/ 20,  // seconds

    /*.high_direct_adv_interval       =*/ 0,    // seconds

    /*.low_direct_adv_interval        =*/ 0,    // seconds

    /*.high_direct_adv_duration       =*/ 0,    // seconds

    /*.low_direct_adv_duration        =*/ 0,    // seconds

    /*.local_name                     =*/ COOKP_DEVICE_NAME, // [LOCAL_NAME_LEN_MAX];

    /*.cod                            =*/ BIT16_TO_8(COOKP_DEVICE_APPEARENCE),0x00, // [COD_LEN];

    /*.ver                            =*/ "1.00",         // [VERSION_LEN];

    /*.encr_required                  =*/ 0, //(SECURITY_ENABLED | SECURITY_REQUEST),    // data encrypted and device sends security request on every connection

    /*.disc_required                  =*/ 0,    // if 1, disconnection after confirmation

    /*.test_enable                    =*/ 0,    // TEST MODE is enabled when 1

    /*.tx_power_level                 =*/ 0x04, // dbm

    /*.con_idle_timeout               =*/ 0,   // second  0-> no timeout

    /*.powersave_timeout              =*/ 0,    // second  0-> no timeout

    /*.hdl                            =*/ {COOKP_MAIN_CHAR_HANDLE, 0x00, 0x00, 0x00, 0x00}, // [HANDLE_NUM_MAX];

    /*.serv                           =*/ {COOKP_MAIN_SERVICE_UUID, 0x00, 0x00, 0x00, 0x00},

    /*.cha                            =*/ {COOKP_MAIN_CHAR_UUID, 0x00, 0x00, 0x00, 0x00},

    /*.findme_locator_enable          =*/ 0,    // if 1 Find me locator is enable

    /*.findme_alert_level             =*/ 0,    // alert level of find me

    /*.client_grouptype_enable        =*/ 0,    // if 1 grouptype read can be used

    /*.linkloss_button_enable         =*/ 0,    // if 1 linkloss button is enable

    /*.pathloss_check_interval        =*/ 0,    // second

    /*.alert_interval                 =*/ 0,    // interval of alert

    /*.high_alert_num                 =*/ 0,    // number of alert for each interval

    /*.mild_alert_num                 =*/ 0,    // number of alert for each interval

    /*.status_led_enable              =*/ 0,    // if 1 status LED is enable

    /*.status_led_interval            =*/ 0,    // second

    /*.status_led_con_blink           =*/ 0,    // blink num of connection

    /*.status_led_dir_adv_blink       =*/ 0,    // blink num of dir adv

    /*.status_led_un_adv_blink        =*/ 0,    // blink num of undir adv

    /*.led_on_ms                      =*/ 0,    // led blink on duration in ms

    /*.led_off_ms                     =*/ 0,    // led blink off duration in ms

    /*.buz_on_ms                      =*/ 0,  // buzzer on duration in ms

    /*.button_power_timeout           =*/ 0,    // seconds

    /*.button_client_timeout          =*/ 0,    // seconds

    /*.button_discover_timeout        =*/ 0,    // seconds

    /*.button_filter_timeout          =*/ 0,    // seconds

#ifdef BLE_UART_LOOPBACK_TRACE

    /*.button_uart_timeout            =*/ 15,   // seconds

#endif

};

1 Reply
BoonT_56
Employee
Employee
500 likes received 250 likes received 100 likes received

After the connection up/down handlers, include the following:

bleprofile_regAppEvtHandler(BLECM_APP_EVT_ENTERING_HIDOFF,(BLECM_NO_PARAM_FUNC)cookp_enter_hidoff);

bleprofile_regAppEvtHandler(BLECM_APP_EVT_ABORTING_HIDOFF,(BLECM_NO_PARAM_FUNC)cookp_abort_hidoff);

Then,

void cookp_enter_hidoff(void)

{

// Do nothing

}

void cookp_abort_hidoff(void)

{

// Do nothing

}

Let me know if it helps.