Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Smart Bluetooth Forum Discussions

This widget could not be displayed.
Anonymous
Not applicable

Hello all

Is there a driver for the bcm920702DG_FLSH that came in the WICED Smart box?

I downloaded and installed the big WIDCOMM driver, but no dice.  Bluetooth Software Download | Broadcom

Thanks!

Jason

0 Likes
1 Solution
This widget could not be displayed.
Anonymous
Not applicable
0 Likes
4 Replies
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

I'm not immediately familiar with the part number you provided.  Are you referring to the dongle that we ship with BCM920732 TAG Board?


Have you tried Windows Update.  If yes, can you provide the PID/VID of the device from device manager.

Also, the Plugable drivers mentioned here seem to work well with the BCM20702 based dongle you are using as well: http://community.broadcom.com/message/1939#1939

0 Likes
This widget could not be displayed.
Anonymous
Not applicable

Thanks for the help!

Yes, the dongle is the one that is included with the TAG board. It is a Broadcom eval board; hence the "9" in the BCM920702 part number.

Unfortunately, the link, the installed driver and windows update did not work. The VID is 0A5C, PID is 22BE, Rev is 0112. The description comes up as "BCM20702A0"

I would appreciate anything you can do to help!

Jason

0 Likes

It may make more sense to just buy a BCM20702 based dongle from one of our partners like Pluggable.

0 Likes
This widget could not be displayed.
Anonymous
Not applicable

Bummer

0 Likes
This widget could not be displayed.