Is it possible to change the ATT_MTU (in order to support larger MTUs than the default 23 octets after an EXCHANGE_MTU request)?
There's a #define in bleapp/lestack/att/leatt.h:
#define LEATT_ATT_MTU 23
I can change this, but it has no affect for some targets (e.g. the sample target "automation_io-BCM920737TAG_Q32 download" is unaffected, probably because it is all in ROM). Presumably the in-ROM profiles have a hard-coded MTU size which cannot be renogiated. Does the BT stack for this module support EXCHANGE_MTU at all?
thanks Stuart
Solved! Go to Solution.
It's possible that you need to login again as this material is in the same forum as where you posted this message.
Here's a cut and paste for convenience (you can also type MTU in the search box above and see it that way):
------------------
This question arose from a customer and I thought others "out there" might have the same curiosity:
For iOS 7, Apple has increased the available MTU size. This allows for larger payloads to be sent and can help simplify the application software.
I was wondering how large of payloads are possible using the Broadcom BLE stack. For example, I am using the bleprofile_sendNotification() API function.
Here are my questions.
1 - What is the maximum MTU for the BCM20732?
2 - How many packets can be sent in parallel for a given connection event?
Answer:
#1. Max MTU is 23 bytes by default.
#2. Depends on how you define 'in parallel'. You cannot send more than one packet per RX/TX pair. You can have up to 255 RX/TX pairs per connection event (assuming that the other side is also BRCM silicon), default is 4, but whether it really uses all available RX/TX pairs depends on whether the master schedules more polls, other tasks like ADV/scans/connections that need to be serviced or the amount of data available to transmit on either side. If you define it as how many packets can be outstanding (unacked), then this is 15, before flow control kicks in. This is configurable, though at the cost of available RAM.
Note: There is a strong relationship between battery life and size of the MTU. Typically a smaller MTU = longer battery life but ultimately depends on how much data the application needs to send and how often.
Max MTU is 23 bytes.
You may find some of the advice in this post helpful: Maximum Transmission Unit (MTU) Size in BCM20732
I cannot read the post you provided a link to.
Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.
It's possible that you need to login again as this material is in the same forum as where you posted this message.
Here's a cut and paste for convenience (you can also type MTU in the search box above and see it that way):
------------------
This question arose from a customer and I thought others "out there" might have the same curiosity:
For iOS 7, Apple has increased the available MTU size. This allows for larger payloads to be sent and can help simplify the application software.
I was wondering how large of payloads are possible using the Broadcom BLE stack. For example, I am using the bleprofile_sendNotification() API function.
Here are my questions.
1 - What is the maximum MTU for the BCM20732?
2 - How many packets can be sent in parallel for a given connection event?
Answer:
#1. Max MTU is 23 bytes by default.
#2. Depends on how you define 'in parallel'. You cannot send more than one packet per RX/TX pair. You can have up to 255 RX/TX pairs per connection event (assuming that the other side is also BRCM silicon), default is 4, but whether it really uses all available RX/TX pairs depends on whether the master schedules more polls, other tasks like ADV/scans/connections that need to be serviced or the amount of data available to transmit on either side. If you define it as how many packets can be outstanding (unacked), then this is 15, before flow control kicks in. This is configurable, though at the cost of available RAM.
Note: There is a strong relationship between battery life and size of the MTU. Typically a smaller MTU = longer battery life but ultimately depends on how much data the application needs to send and how often.
Further questions:
- Is answer#1. and #2. also true for other BCM. e.g. BCM4329 ?
- In the BLUETOOTH SPECIFICATION Version 4.1 [Vol 3] page 494 chapter 3.4.2.1. (see English Specification | Adopted Documents)
it can be seen that:
"...The Client Rx MTU shall be greater than or equal to the default ATT_MTU. "
- In the BLUETOOTH SPECIFICATION Version 4.0 [Vol 3] page 479 chapter 3.2.8. it can be seen that:
"...ATT_MTU is defined as the maximum size of any packet sent between a client
and a server. A higher layer specification defines the default ATT_MTU value.
The client and server may optionally exchange the maximum size of packet
that can be received using the Exchange MTU Request and Response PDUs.
Both devices then use the minimum of these exchanged values for all further communication..."
So IMO: According to the BT spec, ATT_MTU value may be higher than 23.
Value of 158 can really be seen in BLE Transfer between two iOS 8 devices.
I am looking into this with the developers and will ask one of them for feedback.
What you are trying to accomplish appears to be doable per the developers. Unfortunately, we have never prototyped this feature and lack any tested examples we can provide as sample source.
/*
* Copyright 2014, Broadcom Corporation
* All Rights Reserved.
*
* This is UNPUBLISHED PROPRIETARY SOURCE CODE of Broadcom Corporation;
* the contents of this file may not be disclosed to third parties, copied
* or duplicated in any form, in whole or in part, without the prior
* written permission of Broadcom Corporation.
*/
/** @file
*
* Long Characteristic Sample
*
* This sample demonstrates how to read and write values to a characteristic value
* larger than 512 octets in length.
*
* Features demonstrated
* - reading long characteristic from the GATT database
* - writing long characteristic to the GATT database
* - reading value of the long characteristic over the air
* - processing of the value of the long characteristic received over the air
*
* To demonstrate the app, work through the following steps.
* 1. Plug the WICED eval board into your computer
* 2. Build and download the application (to the WICED board)
* 3. Using some client application discover vendor specific service and
* a single vendor specific characteristic of that service
* 4. Read value of the characteristic. It should be 160 zeroes.
* 5. Write a new value with a length of more than 23 bytes. (GATT procedures for
* prepare write and execute write should be used
* 6. Read value again to make sure that it has been written correctly
* 7. Push the application button on the board. During the interrupt processing
* all bytes of the characteristic value are increased by 1 and written back
* to the GATT database
* 8. Read value again to make sure that it has been written correctly
*
*/
#include "bleprofile.h"
#include "bleapp.h"
#include "gpiodriver.h"
#include "string.h"
#include "stdio.h"
#include "platform.h"
#include "long_characteristic_support.h"
#include "long_characteristic.h"
#include "thread_and_mem_mgmt.h"
#define LEL2CAP_CID_LE_ATT 0x4
#define LEATT_OPCODE_MASK 0x3f
#define LEL2CAP_MTU 23
#define LEL2CAP_ACL_PKT_BOUNDARY_FLAG_CONT 0x1 // this is allowed for LE-U
#define LEL2CAP_ACL_PKT_BOUNDARY_FLAG_START 0x2 // this is allowed for LE-U
/******************************************************
* Function Prototypes
******************************************************/
static void long_characteristic_create(void);
static void long_characteristic_connection_up( void );
static void long_characteristic_connection_down( void );
static void long_characteristic_advertisement_stopped( void );
static int long_characteristic_write_handler( LEGATTDB_ENTRY_HDR *p );
static void long_characteristic_interrupt_handler( UINT8 value );
#pragma pack(1)
// this is the general header for L2CAP.
typedef PACKED struct
{
UINT16 length;
UINT16 cid;
} LEL2CAP_HDR;
#pragma pack()
static void my_l2capHandler(LEL2CAP_HDR *l2capHdr);
/******************************************************
* Variables Definitions
******************************************************/
const UINT8 gatt_database[]= // Define GATT database
{
// ***** Primary service 'Generic Access'
//<Name>Generic Access</Name>
//<Uuid>1800</Uuid>
//Service handle: HDLS_GENERIC_ACCESS
//Service UUID: UUID_SERVICE_GAP
PRIMARY_SERVICE_UUID16 (HDLS_GENERIC_ACCESS, UUID_SERVICE_GAP),
//<Name>Device Name</Name>
//<Uuid>2A00</Uuid>
CHARACTERISTIC_UUID16 (HDLC_GENERIC_ACCESS_DEVICE_NAME,
HDLC_GENERIC_ACCESS_DEVICE_NAME_VALUE,
UUID_CHARACTERISTIC_DEVICE_NAME,
LEGATTDB_CHAR_PROP_READ,
LEGATTDB_PERM_READABLE,
16),
'l','o','n','g','_','c','h','a','r',0x00,0x00,0x00,0x00,0x00,0x00,0x00,
//<Name>Appearance</Name>
//<Uuid>2A01</Uuid>
CHARACTERISTIC_UUID16 (HDLC_GENERIC_ACCESS_APPEARANCE,
HDLC_GENERIC_ACCESS_APPEARANCE_VALUE,
UUID_CHARACTERISTIC_APPEARANCE,
LEGATTDB_CHAR_PROP_READ,
LEGATTDB_PERM_READABLE,
2),
BIT16_TO_8(APPEARANCE_GENERIC_TAG),
// ***** Primary service 'Generic Attribute'
//<Name>Generic Attribute</Name>
//<Uuid>1801</Uuid>
//Service handle: HDLS_GENERIC_ATTRIBUTE
//Service UUID: UUID_SERVICE_GATT
PRIMARY_SERVICE_UUID16 (HDLS_GENERIC_ATTRIBUTE, UUID_SERVICE_GATT),
// ***** Primary service 'long_characteristic'
//<Name>long_characteristic</Name>
//<Uuid>bf 90 21 8e c0 68 4c 00 84 01 2d ba 08 ab 32 88</Uuid>
//Service handle: HDLS_LONG_CHARACTERISTIC
//Service UUID: UUID_LONG_CHAR_SERVICE
PRIMARY_SERVICE_UUID128 (HDLS_LONG_CHARACTERISTIC, UUID_LONG_CHAR_SERVICE),
//<Name>long_characteristic</Name>
//<Uuid>34 5b e2 12 5e b1 45 03 b6 29 24 55 8a 11 1e 36</Uuid>
CHARACTERISTIC_UUID128_WRITABLE (HDLC_LONG_CHARACTERISTIC,
HDLC_LONG_CHARACTERISTIC_VALUE,
UUID_LONG_CHAR_CHAR,
LEGATTDB_CHAR_PROP_READ | LEGATTDB_CHAR_PROP_WRITE_NO_RESPONSE | LEGATTDB_CHAR_PROP_WRITE | LEGATTDB_CHAR_PROP_NOTIFY | LEGATTDB_CHAR_PROP_INDICATE,
LEGATTDB_PERM_READABLE | LEGATTDB_PERM_WRITE_CMD | LEGATTDB_PERM_WRITE_REQ | LEGATTDB_PERM_RELIABLE_WRITE | LEGATTDB_PERM_VARIABLE_LENGTH,
SIZE_LONG_CHARACTERISTIC_VALUE),
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
//<ClientConfiguration>
//<Notification>false</Notification>
//<Indication>false</Indication>
CHAR_DESCRIPTOR_UUID16_WRITABLE (HDLD_LONG_CHARACTERISTIC_LONG_CHARACTERISTIC_CLIENT_CONFIGURATION,
UUID_DESCRIPTOR_CLIENT_CHARACTERISTIC_CONFIGURATION,
LEGATTDB_PERM_READABLE | LEGATTDB_PERM_WRITE_CMD | LEGATTDB_PERM_WRITE_REQ | LEGATTDB_PERM_RELIABLE_WRITE | LEGATTDB_PERM_AUTH_WRITABLE,
2),
BIT16_TO_8 (CCC_NONE),
};
// Indication sent, waiting for ack
UINT8 long_characteristic_indication_sent = 0;
// current value of client configuration descriptor
UINT16 long_characteristic_client_configuration = 0;
// negotiated MTU, assume
#define LONG_CHARACTERISTIC_LOCAL_MTU 158
UINT16 long_characteristic_mtu;
// Length of the GATT database
const UINT16 gatt_database_len = sizeof(gatt_database);
// Following structure defines GPIO configuration used by the application
const BLE_PROFILE_GPIO_CFG long_characteristic_gpio_cfg =
{
{
GPIO_PIN_WP, // This need to be used to enable/disable NVRAM write protect
GPIO_PIN_BUTTON, -1, -1, -1,
-1, -1, -1, -1, -1, -1, -1, -1, -1, -1, -1 // Other GPIOs are not used
},
/*.gpio_flag =*/
{
GPIO_SETTINGS_WP,
GPIO_SETTINGS_BUTTON, 0, 0, 0,
0, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0
}
};
// Main vendor specific service
UINT8 long_characteristic_uuid_main_vsc_service[16] = {UUID_LONG_CHAR_SERVICE};
const BLE_PROFILE_CFG long_characteristic_cfg =
{
/*.fine_timer_interval =*/ 0, // ms
/*.default_adv =*/ 4, // HIGH_UNDIRECTED_DISCOVERABLE
/*.button_adv_toggle =*/ 0, // pairing button make adv toggle (if 1) or always on (if 0)
/*.high_undirect_adv_interval =*/ 32, // slots
/*.low_undirect_adv_interval =*/ 1024, // slots
/*.high_undirect_adv_duration =*/ 30, // seconds
/*.low_undirect_adv_duration =*/ 300, // seconds
/*.high_direct_adv_interval =*/ 0, // seconds
/*.low_direct_adv_interval =*/ 0, // seconds
/*.high_direct_adv_duration =*/ 0, // seconds
/*.low_direct_adv_duration =*/ 0, // seconds
/*.local_name =*/ "long_char", // [LOCAL_NAME_LEN_MAX];
/*.cod =*/ BIT16_TO_8(APPEARANCE_GENERIC_TAG),0x00, // [COD_LEN];
/*.ver =*/ "1.00", // [VERSION_LEN];
/*.encr_required =*/ 0, //(SECURITY_ENABLED | SECURITY_REQUEST), // data encrypted and device sends security request on every connection
/*.disc_required =*/ 0, // if 1, disconnection after confirmation
/*.test_enable =*/ 1, // TEST MODE is enabled when 1
/*.tx_power_level =*/ 0x04, // dbm
/*.con_idle_timeout =*/ 0, // second 0-> no timeout
/*.powersave_timeout =*/ 0, // second 0-> no timeout
/*.hdl =*/ {0x00, 0x00, 0x00, 0x00, 0x00}, // [HANDLE_NUM_MAX];
/*.serv =*/ {0x00, 0x00, 0x00, 0x00, 0x00},
/*.cha =*/ {0x00, 0x00, 0x00, 0x00, 0x00},
/*.findme_locator_enable =*/ 0, // if 1 Find me locator is enable
/*.findme_alert_level =*/ 0, // alert level of find me
/*.client_grouptype_enable =*/ 0, // if 1 grouptype read can be used
/*.linkloss_button_enable =*/ 0, // if 1 linkloss button is enable
/*.pathloss_check_interval =*/ 0, // second
/*.alert_interval =*/ 0, // interval of alert
/*.high_alert_num =*/ 0, // number of alert for each interval
/*.mild_alert_num =*/ 0, // number of alert for each interval
/*.status_led_enable =*/ 1, // if 1 status LED is enable
/*.status_led_interval =*/ 0, // second
/*.status_led_con_blink =*/ 0, // blink num of connection
/*.status_led_dir_adv_blink =*/ 0, // blink num of dir adv
/*.status_led_un_adv_blink =*/ 0, // blink num of undir adv
/*.led_on_ms =*/ 0, // led blink on duration in ms
/*.led_off_ms =*/ 0, // led blink off duration in ms
/*.buz_on_ms =*/ 100, // buzzer on duration in ms
/*.button_power_timeout =*/ 0, // seconds
/*.button_client_timeout =*/ 0, // seconds
/*.button_discover_timeout =*/ 0, // seconds
/*.button_filter_timeout =*/ 0, // seconds
#ifdef BLE_UART_LOOPBACK_TRACE
/*.button_uart_timeout =*/ 15, // seconds
#endif
};
// Following structure defines UART configuration
const BLE_PROFILE_PUART_CFG long_characteristic_puart_cfg =
{
/*.baudrate =*/ 115200,
/*.txpin =*/ PUARTDISABLE | GPIO_PIN_UART_TX,
/*.rxpin =*/ PUARTDISABLE | GPIO_PIN_UART_RX,
};
/******************************************************
* Function Definitions
******************************************************/
// Application initialization
APPLICATION_INIT()
{
// default number of prepare writes is 5, which is not enough for very long characteristics.
// Setting it to 15 will cover characteristics of up to 256 octets in length.
bleprofile_SetMaxQueuedWriteRequests(15);
bleapp_set_cfg((UINT8 *)gatt_database,
gatt_database_len,
(void *)&long_characteristic_cfg,
(void *)&long_characteristic_puart_cfg,
(void *)&long_characteristic_gpio_cfg,
long_characteristic_create);
}
// Create device
void long_characteristic_create(void)
{
extern UINT32 blecm_configFlag ;
blecm_configFlag |= BLECM_DBGUART_LOG | BLECM_DBGUART_LOG_L2CAP | BLECM_DBGUART_LOG_SMP;
ble_trace0("create()");
ble_trace0(bleprofile_p_cfg->ver);
// dump the database to debug uart.
legattdb_dumpDb();
bleprofile_Init(bleprofile_p_cfg);
bleprofile_GPIOInit(bleprofile_gpio_p_cfg);
// Initialized ROM code which will monitor the battery
blebat_Init();
// register the handler for the CID.
lel2cap_regConnLessHandler(LEL2CAP_CID_LE_ATT, my_l2capHandler);
// register connection up and connection down handler.
bleprofile_regAppEvtHandler(BLECM_APP_EVT_LINK_UP, long_characteristic_connection_up);
bleprofile_regAppEvtHandler(BLECM_APP_EVT_LINK_DOWN, long_characteristic_connection_down);
bleprofile_regAppEvtHandler(BLECM_APP_EVT_ADV_TIMEOUT, long_characteristic_advertisement_stopped);
// register to process client writes
legattdb_regWriteHandleCb((LEGATTDB_WRITE_CB)long_characteristic_write_handler);
// register interrupt handler
bleprofile_regIntCb((BLEPROFILE_SINGLE_PARAM_CB) long_characteristic_interrupt_handler);
// total length should be less than 31 bytes
BLE_ADV_FIELD adv[3];
BLE_ADV_FIELD scr[1];
// flags
adv[0].len = 1 + 1;
adv[0].val = ADV_FLAGS;
adv[0].data[0] = LE_LIMITED_DISCOVERABLE | BR_EDR_NOT_SUPPORTED;
adv[1].len = 16 + 1;
adv[1].val = ADV_SERVICE_UUID128_COMP;
memcpy(adv[1].data, &long_characteristic_uuid_main_vsc_service[0], 16);
// Tx power level
adv[2].len = TX_POWER_LEN+1;
adv[2].val = ADV_TX_POWER_LEVEL;
adv[2].data[0] = bleprofile_p_cfg->tx_power_level;
// name
scr[0].len = strlen(bleprofile_p_cfg->local_name) + 1;
scr[0].val = ADV_LOCAL_NAME_COMP;
memcpy(scr[0].data, bleprofile_p_cfg->local_name, scr[0].len - 1);
bleprofile_GenerateADVData(adv, 3);
bleprofile_GenerateScanRspData(scr, 1);
blecm_setTxPowerInADV(0);
bleprofile_Discoverable(HIGH_UNDIRECTED_DISCOVERABLE, NULL);
}
// Connection up callback function is called on every connection establishment
void long_characteristic_connection_up(void)
{
// until MTU has been exchanged, the only thing that is possible is 23 bytes
long_characteristic_mtu = LEL2CAP_MTU;
// Device supports a single connection, stop advertising
bleprofile_Discoverable(NO_DISCOVERABLE, NULL);
}
// Connection down callback
void long_characteristic_connection_down(void)
{
// If disconnection was caused by the peer, start low advertisements
bleprofile_Discoverable(HIGH_UNDIRECTED_DISCOVERABLE, NULL);
}
// Callback function indicates to the application that advertising has stopped.
// restart advertisement if needed
void long_characteristic_advertisement_stopped(void)
{
// Start low advertisements to keep device connectable
bleprofile_Discoverable(LOW_UNDIRECTED_DISCOVERABLE, NULL);
}
// Process write request or command from peer device
int long_characteristic_write_handler(LEGATTDB_ENTRY_HDR *p)
{
UINT8 writtenbyte;
UINT16 handle = legattdb_getHandle(p);
int len = legattdb_getAttrValueLen(p);
UINT8 *attrPtr = legattdb_getAttrValue(p);
BOOL changed;
ble_trace2("write_handler: handle %04x len:%d", handle, len);
if ((handle == HDLC_LONG_CHARACTERISTIC_VALUE) && (len <= 160))
{
// do not need to do anything. If we return 0, the value will be stored the GATT database
}
if ((len == 2) && (handle == HDLD_LONG_CHARACTERISTIC_LONG_CHARACTERISTIC_CLIENT_CONFIGURATION))
{
long_characteristic_client_configuration = attrPtr[0] + (attrPtr[1] << 8);
}
return 0;
}
// Three Interrupt inputs (Buttons) can be handled here.
// If the following value == 1, Button is pressed. Different than initial value.
// If the following value == 0, Button is depressed. Same as initial value.
// Button1 : value&0x01
// Button2 : (value&0x02)>>1
// Button3 : (value&0x04)>>2
void long_characteristic_interrupt_handler(UINT8 value)
{
BLEPROFILE_DB_PDU *db_pdu;
static UINT8 seqnum = 0;
ble_trace3("(INT)But1:%d But2:%d But3:%d\n", value&0x01, (value& 0x02) >> 1, (value & 0x04) >> 2);
void *p_mem = cfa_mm_Alloc(SIZE_LONG_CHARACTERISTIC_VALUE + 2);
seqnum++;
if (p_mem != 0)
{
db_pdu = (BLEPROFILE_DB_PDU *)p_mem;
db_pdu->len = SIZE_LONG_CHARACTERISTIC_VALUE;
if (bleprofile_ReadHandleData(HDLC_LONG_CHARACTERISTIC_VALUE, db_pdu, SIZE_LONG_CHARACTERISTIC_VALUE + 2) == 0)
{
ble_trace0("ReadHandleData success");
ble_tracen(db_pdu->pdu, db_pdu->len);
}
else
{
ble_trace0("ReadHandleData failed :-(");
cfa_mm_Free(p_mem);
return;
}
memset (db_pdu->pdu, seqnum, SIZE_LONG_CHARACTERISTIC_VALUE);
if (bleprofile_WriteHandleData(HDLC_LONG_CHARACTERISTIC_VALUE, db_pdu, SIZE_LONG_CHARACTERISTIC_VALUE + 2) == 0)
{
ble_trace0("WriteHandleData success");
}
else
{
ble_trace0("WriteHandleData failed");
}
cfa_mm_Free(p_mem);
}
else
{
ble_trace0("no mem");
}
}
// Process indication confirmation. if client service indication, each indication
// should be acknowledged before the next one can be sent.
void long_characteristic_indication_cfm(void)
{
}
/******************************************************************************
* Function: void lel2cap_sendConnectionLessPkt(int cid, UINT8 *pkt, int len )
*
* Abstract: This function will pass the data packet through connectionless
* l2cap channel. It does not do segmentation.
*
* Input/Output: Trivial
*
* Return: None
*
******************************************************************************/
void lel2cap_sendFragmentConnectionLessPkt(int cid, UINT8 *pkt, int len )
{
BOOL first_chunk = TRUE;
LEL2CAP_HDR *l2capPtr;
HCI_ACL_HDR *txBuffer;
int bytes_to_copy;
int offset = 0;
// The len is the packet above l2cap length. we need to add l2cap
// header and acl header to it.
while (len != 0)
{
txBuffer = (HCI_ACL_HDR*) cfa_hci_AllocateBLEACL(
LEL2CAP_MTU + 4 + sizeof(LEL2CAP_HDR), TRUE);
if (txBuffer == NULL)
{
ble_trace0("lel2cap Fail to allocate buffer");
break;
}
// Skip over HCI header, get to the l2cap.
l2capPtr = (LEL2CAP_HDR *)(txBuffer + 1);
// form the HCI header.
txBuffer->connectionHandleEtc = emconinfo_getConnHandle();
// copy the payload, reserve room for the l2cap header area.
if (first_chunk)
{
first_chunk = FALSE;
bytes_to_copy = (len <= LEL2CAP_MTU) ? len : LEL2CAP_MTU;
memcpy( (l2capPtr + 1), pkt, bytes_to_copy);
// put the l2cap connectionless packet header on it.
l2capPtr->cid = cid;
l2capPtr->length = len;
// Set the packet boundary flag to be 10.
// packet boundary flag are bit [13:12].
txBuffer->connectionHandleEtc |= (LEL2CAP_ACL_PKT_BOUNDARY_FLAG_START<<12);
txBuffer->length = bytes_to_copy + sizeof(LEL2CAP_HDR);
}
else
{
bytes_to_copy = len <= LEL2CAP_MTU + sizeof(LEL2CAP_HDR) ? len : LEL2CAP_MTU + sizeof(LEL2CAP_HDR);
memcpy( l2capPtr, pkt + offset, bytes_to_copy);
txBuffer->connectionHandleEtc |= (LEL2CAP_ACL_PKT_BOUNDARY_FLAG_CONT<<12);
txBuffer->length = bytes_to_copy;
}
len -= bytes_to_copy;
offset += bytes_to_copy;
ble_trace0("\rl2cap Tx:");
ble_tracen((UINT8 *) txBuffer, txBuffer->length + 4 );
cfa_hci_SendACLTx( txBuffer );
// we need to keep track of HCI buffer usage.
blecm_decAvailableTxBuffers();
// refresh the idle timer.
blecm_refreshConnIdletimer( );
}
}
void my_l2capHandler(LEL2CAP_HDR *l2capHdr)
{
LEATT_PDU_HDR *gattPtr = (LEATT_PDU_HDR*) (l2capHdr +1);
LEATT_PDU_MTU_EXCHANGE_REQ *p_mtu_exchange;
LEATT_PDU_READ_REQ_HDR *p_read_req;
LEATT_PDU_READ_RSP_HDR *p_read_rsp;
LEATT_PDU_READ_BLOB_REQ *p_read_blob_req;
LEATT_PDU_READ_BLOB_RSP_HDR *p_read_blob_rsp;
LEATT_PDU_PREPARE_WRITE_REQ_HDR *p_prepare_write_req;
BLEPROFILE_DB_PDU *db_pdu;
UINT8 *p_data;
void *p_mem;
UINT16 bytes_to_send;
LEATT_PDU_EXECUTE_WRITE_REQ_HDR *p_execute_write_req;
LEATT_PDU_EXECUTE_WRITE_RSP_HDR *p_execute_write_rsp;
int opcode = LEATT_OPCODE_MASK & gattPtr->attrCode ;
ble_trace2("l2cap len:%d gatt opcode:%d", l2capHdr->length, opcode);
if (opcode == LEATT_OPCODE_EXCHANGE_MTU_REQ)
{
p_mtu_exchange = (LEATT_PDU_MTU_EXCHANGE_REQ *)gattPtr;
ble_trace1("mtu req:%d", p_mtu_exchange->mtu);
long_characteristic_mtu = p_mtu_exchange->mtu < LONG_CHARACTERISTIC_LOCAL_MTU ? p_mtu_exchange->mtu : LONG_CHARACTERISTIC_LOCAL_MTU;
p_mtu_exchange->attrCode = LEATT_OPCODE_EXCHANGE_MTU_RSP;
p_mtu_exchange->mtu = long_characteristic_mtu;
lel2cap_sendConnectionLessPkt(LEL2CAP_CID_LE_ATT, p_mtu_exchange, l2capHdr->length);
return;
}
else if (opcode == LEATT_OPCODE_READ_REQ)
{
p_read_req = (LEATT_PDU_READ_REQ_HDR *)gattPtr;
ble_trace1("read req:%04x", p_read_req->attrHandle);
if (p_read_req->attrHandle == HDLC_LONG_CHARACTERISTIC_VALUE)
{
if ((p_mem = cfa_mm_Alloc(SIZE_LONG_CHARACTERISTIC_VALUE + 2)) == 0)
{
leatt_sendErrResponse(LEATT_ERR_CODE_INSUFFICIENT_RESOURCES, LEATT_OPCODE_READ_REQ, HDLC_LONG_CHARACTERISTIC_VALUE);
return;
}
db_pdu = (BLEPROFILE_DB_PDU *)p_mem;
db_pdu->len = SIZE_LONG_CHARACTERISTIC_VALUE;
bleprofile_ReadHandleData(HDLC_LONG_CHARACTERISTIC_VALUE, db_pdu, SIZE_LONG_CHARACTERISTIC_VALUE + 2);
bytes_to_send = db_pdu->len + sizeof (LEATT_PDU_READ_RSP_HDR) < long_characteristic_mtu ?
db_pdu->len + sizeof (LEATT_PDU_READ_RSP_HDR) : long_characteristic_mtu;
p_data = db_pdu->pdu - sizeof (LEATT_PDU_READ_RSP_HDR);
p_read_rsp = (LEATT_PDU_READ_RSP_HDR *)p_data;
p_read_rsp->attrCode = LEATT_OPCODE_READ_RSP;
lel2cap_sendFragmentConnectionLessPkt(LEL2CAP_CID_LE_ATT, p_data, bytes_to_send);
cfa_mm_Free(p_mem);
return;
}
}
else if (opcode == LEATT_OPCODE_READ_BLOB_REQ)
{
p_read_blob_req = (LEATT_PDU_READ_BLOB_REQ *)gattPtr;
ble_trace1("read blob:%04x", p_read_blob_req->attrHandle);
if (p_read_blob_req->attrHandle == HDLC_LONG_CHARACTERISTIC_VALUE)
{
if (p_read_blob_req->valueOffset > SIZE_LONG_CHARACTERISTIC_VALUE)
{
leatt_sendErrResponse(LEATT_ERR_CODE_INVALID_OFFSET, LEATT_OPCODE_READ_BLOB_REQ, HDLC_LONG_CHARACTERISTIC_VALUE);
return;
}
if ((p_mem = cfa_mm_Alloc(SIZE_LONG_CHARACTERISTIC_VALUE + 2)) == 0)
{
leatt_sendErrResponse(LEATT_ERR_CODE_INSUFFICIENT_RESOURCES, LEATT_OPCODE_READ_BLOB_REQ, HDLC_LONG_CHARACTERISTIC_VALUE);
return;
}
db_pdu = (BLEPROFILE_DB_PDU *)p_mem;
db_pdu->len = SIZE_LONG_CHARACTERISTIC_VALUE;
bleprofile_ReadHandleData(HDLC_LONG_CHARACTERISTIC_VALUE, db_pdu, SIZE_LONG_CHARACTERISTIC_VALUE + 2);
bytes_to_send = db_pdu->len + sizeof (LEATT_PDU_READ_BLOB_RSP_HDR) - p_read_blob_req->valueOffset < long_characteristic_mtu ?
db_pdu->len + sizeof (LEATT_PDU_READ_BLOB_RSP_HDR) - p_read_blob_req->valueOffset : long_characteristic_mtu;
p_data = db_pdu->pdu - sizeof (LEATT_PDU_READ_BLOB_RSP_HDR);
p_read_blob_rsp = (LEATT_PDU_READ_BLOB_RSP_HDR *)p_data;
p_read_blob_rsp->attrCode = LEATT_OPCODE_READ_BLOB_RSP;
lel2cap_sendFragmentConnectionLessPkt(LEL2CAP_CID_LE_ATT, p_data, bytes_to_send);
cfa_mm_Free(p_mem);
return;
}
}
else if (opcode == LEATT_OPCODE_PREPARE_WRITE_REQ)
{
p_prepare_write_req = (LEATT_PDU_PREPARE_WRITE_REQ_HDR *)gattPtr;
ble_trace1("prepare write:%04x", p_prepare_write_req->attrHandle);
if (p_prepare_write_req->attrHandle == HDLC_LONG_CHARACTERISTIC_VALUE)
{
if (p_prepare_write_req->valOffset + l2capHdr->length - sizeof (LEATT_PDU_PREPARE_WRITE_REQ_HDR) > SIZE_LONG_CHARACTERISTIC_VALUE)
{
leatt_sendErrResponse(LEATT_ERR_CODE_INVALID_OFFSET, LEATT_OPCODE_PREPARE_WRITE_REQ, HDLC_LONG_CHARACTERISTIC_VALUE);
return;
}
if ((p_mem = cfa_mm_Alloc(SIZE_LONG_CHARACTERISTIC_VALUE + 2)) == 0)
{
leatt_sendErrResponse(LEATT_ERR_CODE_INSUFFICIENT_RESOURCES, LEATT_OPCODE_PREPARE_WRITE_REQ, HDLC_LONG_CHARACTERISTIC_VALUE);
return;
}
db_pdu = (BLEPROFILE_DB_PDU *)p_mem;
db_pdu->len = SIZE_LONG_CHARACTERISTIC_VALUE;
bleprofile_ReadHandleData(HDLC_LONG_CHARACTERISTIC_VALUE, db_pdu, SIZE_LONG_CHARACTERISTIC_VALUE + 2);
memcpy(&db_pdu->pdu[p_prepare_write_req->valOffset], (UINT8 *)(l2capHdr + 1), l2capHdr->length - sizeof (LEATT_PDU_PREPARE_WRITE_REQ_HDR));
db_pdu->len = p_prepare_write_req->valOffset + l2capHdr->length - sizeof (LEATT_PDU_PREPARE_WRITE_REQ_HDR);
bleprofile_WriteHandleData(HDLC_LONG_CHARACTERISTIC_VALUE, db_pdu, db_pdu->len);
p_prepare_write_req->attrCode = LEATT_OPCODE_PREPARE_WRITE_RSP;
lel2cap_sendFragmentConnectionLessPkt(LEL2CAP_CID_LE_ATT, (UINT8 *)p_prepare_write_req, l2capHdr->length);
cfa_mm_Free(p_mem);
return;
}
}
else if (opcode == LEATT_OPCODE_EXECUTE_WRITE_REQ)
{
p_execute_write_req = (LEATT_PDU_EXECUTE_WRITE_REQ_HDR *)gattPtr;
if (p_execute_write_req->flag != 1)
{
ble_trace0("write cancel, not supported");
}
p_execute_write_req->attrCode = LEATT_OPCODE_EXECUTE_WRITE_RSP;
lel2cap_sendConnectionLessPkt(LEL2CAP_CID_LE_ATT, (UINT8 *)p_execute_write_req, sizeof(LEATT_PDU_EXECUTE_WRITE_RSP_HDR));
return;
}
leatt_l2capHandler(l2capHdr);
}
Attached is long_char application modified to have characteristic 208 bytes and MTU 158 bytes.
Please note that Win7 has a bug, so we did our testing with Win8.
It's still a good sample to show how this can be accomplished.
Note that there are a few execution paths that have not been implemented or tested.
How many of these long_characteristics with the 158 byte MTU can be 'read' during a single connection interval? If it is untested, no worries. . .I have a test system showing up shortly.