Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi all

1.How to control 20732S through UART?

2.How to add find me profile?

thanks

0 Likes
1 Solution

I'm not sure which board that is you are using.  I will ask someone from our team in Asia to respond.

nsankar boont roychang

The boards we normally support here on the forum are included here in this document: BCM2073X Product Portfolio (Module and Evaluation Board Overview)

View solution in original post

0 Likes
10 Replies
Anonymous
Not applicable
0 Likes
Anonymous
Not applicable

Hi J.T

I have seen these posts

but I am using 20732S(SPIL production module)

Have the same right 20736S?

My main problem now is how to control through UART 20732S

and

How to use putty(terminal tool)?

thanks

0 Likes
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

1. Specific to the 20732S, which is using the original firmware, you will want to consult the PUART example within the WICED™ Smart Hardware Interfaces document, along with the sample in the SDK: /WICED-Smart-SDK/Apps/uart_firmware_upgrade

In addition, SDK 2.2 introduced an application called puart_control which does this exact thing well, but it will not work on the 20732S.  Not sure if an ugrade is possible.

2.

There is no Find Me Profile.

Either proximity and proximity_client are what I think you need.

0 Likes
Anonymous
Not applicable

Hi

UART connector must use FTDI chip?

because

I use the  unable connection of the chip (silicon labs CP210X)

currently still looking for is what causes (Putty message can not be displayed)

thanks

0 Likes

The FTDI and Silicon Labs chips are USB to Serial converters.

The FTDI part is used with the TAG3 development board.

The Silicon Labs part is used with the WICED Sense Evaluation Board.

Neither is technically required within a production design (the PUART is a simple UART implementation)

However, many use FTDI Serial to USB cables to program the SIP modules in production from a PC.

0 Likes
Anonymous
Not applicable

Hi

Sorry!

Such as the following pictures

show "No tag detected"

What may be the reason?(usb cable driver)

thanks

boardcom.jpg

0 Likes

Please describe what board is being connected to your PC (TAG3, WICED Sense, Etc.) and with what cable (FTDI USB to Serial Cable, 1.8V or 3V version).

Not that if this is a custom design, the state if the HCI Uart line is critical.

This thread offers a tremendous amount of insight related to programming a custom design: Re: Programming the BCM20736S on a custom PCB

0 Likes
Anonymous
Not applicable

Hi

FTDI USB to Serial Cable is 3.3V version

How to confirm that EVB or TAG3 ?

the board is manufactured by SPIL modules

thanks

IMAG0573.jpg

0 Likes

I'm not sure which board that is you are using.  I will ask someone from our team in Asia to respond.

nsankar boont roychang

The boards we normally support here on the forum are included here in this document: BCM2073X Product Portfolio (Module and Evaluation Board Overview)

0 Likes
Anonymous
Not applicable

Hi

really appreciate your help!

I can only determine the chip is 20732

0 Likes