BCM20732S Stencil question

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi all, I'm trying to make an eagle part library for BCM20732S for the board I'm designing.

I'm looking at P9 of the BCM20732S datasheet where the layout of the pins is described for the PCB stencil.

I'm a bit confused about the positioning of pins "C" - are they centred on the centre of the chip? Judging from the position of pins "A" and "B", pins "C" are centred (0.25,0.25) mm from the centre of the chip and are 1.25mm apart from each other, but the drawing doesn't show this explicitly. Is this drawing available in any cad format, or is there even a part library?

I'm happy to share the eagle part library once I finish it.

Tim

0 Likes
1 Solution
Anonymous
Not applicable

Actually the correct information is on page 27 (fig 15), apologies

View solution in original post

0 Likes
1 Reply
Anonymous
Not applicable

Actually the correct information is on page 27 (fig 15), apologies

0 Likes