- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello All,
Having a problem with the SPI interface on the BCM20732S (and BCM20736S). We had this working previously with different IO on the BCM20732S (same chip) on a past project. The only activity we see now is a 25.5us low pulse on the SPI CS. Any ideas? TIA
Using these NEW pins (highlighted in yellow):
Logic Analyzer probe of the SPI signals. SPI Clock is always low. MISO is always low, MOSI is always high:
Older code & Schematic snippets (working):
Spi init-
// SPI:
#define CS1_PORT 1 // use P26 for SPI_CS1_LED1
#define CS1_PIN 10
#define CS2_PORT 0 // use P2 for SPI_CS2_LED2
#define CS2_PIN 2
#define SPEED 8000000 // Use 8M speed
#define CS_ASSERT 0 // CS is active low
#define CS_DEASSERT 1
void DW_Gateway_SpiInit(void)
{
// Use SPIFFY2 interface as master
spi2PortConfig.masterOrSlave = MASTER2_CONFIG;
// pull for MISO for master, MOSI/CLOCK/CS if slave mode
spi2PortConfig.pinPullConfig = INPUT_PIN_PULL_UP;
// Use P3 for CLK, P0 for MOSI and P1 for MISO
spi2PortConfig.spiGpioConfig = MASTER2_P03_CLK_P00_MOSI_P01_MISO;
// Initialize SPIFFY2 instance
spiffyd_init(SPIFFYD_2);
// Define this to the Port/Pin you want to use for CS. // Port = P#/16 and PIN = P# % 16
// Configure the CS pin and deassert it intially. If enabling output, you only need to configure once. Use gpio_setPinOutput to toggle value being o/p
gpio_configurePin(CS1_PORT, CS1_PIN, GPIO_OUTPUT_ENABLE | GPIO_INPUT_DISABLE, CS_DEASSERT);
gpio_configurePin(CS2_PORT, CS2_PIN, GPIO_OUTPUT_ENABLE | GPIO_INPUT_DISABLE, CS_DEASSERT);
// Configure the SPIFFY2 HW block
spiffyd_configure(SPIFFYD_2, SPEED, SPI_MSB_FIRST, SPI_SS_ACTIVE_LOW, SPI_MODE_0); // Originally SPI_MODE_3, but problems with Freq Synth Writes
// Deassert chip selects
gpio_setPinOutput(CS1_PORT, CS1_PIN, CS_DEASSERT);
gpio_setPinOutput(CS2_PORT, CS2_PIN, CS_DEASSERT);
}
Newer code & Schematic snippets (not working):
Spi init-
// SPI:
#define CS1_PORT 1 // use P26 for SPI_CS to accelerometer
#define CS1_PIN 10
#define CS2_PORT 0 // use P8 for SPI_USB_CSn to USB/uController
#define CS2_PIN 8
void Macnica_Mpression_SpiInit(void)
{
gpio_configurePin(0, 0, GPIO_OUTPUT_DISABLE | GPIO_INPUT_DISABLE, CS_DEASSERT);
gpio_configurePin(0, 1, GPIO_OUTPUT_DISABLE | GPIO_INPUT_DISABLE, CS_DEASSERT);
gpio_configurePin(0, 2, GPIO_OUTPUT_DISABLE | GPIO_INPUT_DISABLE, CS_DEASSERT);
gpio_setPinOutput(0, 0, CS_DEASSERT);
gpio_setPinOutput(0, 1, CS_DEASSERT);
gpio_setPinOutput(0, 2, CS_DEASSERT);
// Use SPIFFY2 interface as master
spi2PortConfig.masterOrSlave = MASTER2_CONFIG;
// pull for MISO for master, MOSI/CLOCK/CS if slave mode
spi2PortConfig.pinPullConfig = INPUT_PIN_PULL_UP;
// Use P3 for CLK, P0 for MOSI and P1 for MISO
spi2PortConfig.spiGpioConfig = MASTER2_P24_CLK_P27_MOSI_P25_MISO;
// Initialize SPIFFY2 instance
spiffyd_init(SPIFFYD_2);
// Define this to the Port/Pin you want to use for CS. // Port = P#/16 and PIN = P# % 16
// Configure the CS pin and deassert it intially. If enabling output, you only need to configure once. Use gpio_setPinOutput to toggle value being o/p
gpio_configurePin(CS1_PORT, CS1_PIN, GPIO_OUTPUT_ENABLE | GPIO_INPUT_DISABLE, CS_DEASSERT);
gpio_configurePin(CS2_PORT, CS2_PIN, GPIO_OUTPUT_ENABLE | GPIO_INPUT_DISABLE, CS_DEASSERT);
// Configure the SPIFFY2 HW block
spiffyd_configure(SPIFFYD_2, SPEED, SPI_MSB_FIRST, SPI_SS_ACTIVE_LOW, SPI_MODE_0);
// Deassert chip selects
gpio_setPinOutput(CS1_PORT, CS1_PIN, CS_DEASSERT);
gpio_setPinOutput(CS2_PORT, CS2_PIN, CS_DEASSERT);
}
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello Dkalva,
Yes that is the correct method to disable the PUART. If you use the SPI2 and PUART they have to both be on either the upper or lower PORTs. P0-P7 or P24-P39.
Regards,
Frank