- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The IIC and SPI (aka SPIFFY1) interfaces share Pin 16 (SCL/CLK) and Pin 15 (SDA/MOSI) of the 20732 device. Page 19 of 20732-DS104-RDS.pdf (dated 9/17/2013) states pullups are required on these open drain I/O pins.
Schematics showing the EEPROM based designs consistently remind us that pullup resistors are required on these pins.
However, some schematics showing the (SPI) Serial Flash based implementation (e.g. 920732EVAL_Q32_P3-HWUM100-RDS.pdf) do not show pullup resistors.
I *assume* the IIC or GPIO interface is the default multiplexer setting for these pins after RESET, in which case there could (?) be a window of opportunity for an input to float before the software has an opportunity to re-configure the mux to use the SPIFFY1 interface instead?
Are the resistors mandatory (?), recommended (?), or truly not needed when using a serial flash?
Solved! Go to Solution.
- Labels:
-
I2C
- Tags:
- 20732
- assume
- assumption
- based
- bc20732
- bcm20732
- bcm20732s
- bcm920732tag_q32
- board
- broadcom
- chip
- chip-level
- confirm
- correct
- current
- data
- datsheet
- developed
- directory
- distribution
- docschematics
- external
- externally
- forum
- implementations
- implimentation
- install
- internal
- internally
- level
- manufactures
- module
- needed
- note
- noted
- pins
- point
- pull-up
- pulled
- recommended
- representatives
- resistor
- resistors
- schematic
- status
- technical
- tool
- vddio
- version
- weak
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content