- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
We use a new flash MX25L6406E for our project.
When download it,it will fail,and in download.log:
BluetoolDownloadMinidriver failed!
If use recover mode to download it ,it fail too,and in download.log:
Download minidriver successfully had written 251 bytes to address 0x00201000
Download minidriver successfully had written 251 bytes to address 0x002010FB
Download minidriver successfully had written 251 bytes to address 0x002011F6
Download minidriver successfully had written 251 bytes to address 0x002012F1
Download minidriver successfully had written 251 bytes to address 0x002013EC
Download minidriver successfully had written 251 bytes to address 0x002014E7
Download minidriver successfully had written 251 bytes to address 0x002015E2
Download minidriver successfully had written 251 bytes to address 0x002016DD
Download minidriver successfully had written 251 bytes to address 0x002017D8
Download minidriver successfully had written 251 bytes to address 0x002018D3
Download minidriver successfully had written 251 bytes to address 0x002019CE
Download minidriver successfully had written 251 bytes to address 0x00201AC9
Download minidriver successfully had written 251 bytes to address 0x00201BC4
Download minidriver successfully had written 251 bytes to address 0x00201CBF
Download minidriver successfully had written 251 bytes to address 0x00201DBA
Download minidriver successfully had written 251 bytes to address 0x00201EB5
Download minidriver successfully had written 251 bytes to address 0x00201FB0
Download minidriver successfully had written 251 bytes to address 0x002020AB
Download minidriver successfully had written 251 bytes to address 0x002021A6
Download minidriver successfully had written 251 bytes to address 0x002022A1
Download minidriver successfully had written 251 bytes to address 0x0020239C
Download minidriver successfully had written 251 bytes to address 0x00202497
Download minidriver successfully had written 251 bytes to address 0x00202592
Download minidriver successfully had written 251 bytes to address 0x0020268D
Download minidriver successfully had written 251 bytes to address 0x00202788
Download minidriver successfully had written 251 bytes to address 0x00202883
Download minidriver successfully had written 251 bytes to address 0x0020297E
Download minidriver successfully had written 251 bytes to address 0x00202A79
Download minidriver successfully had written 251 bytes to address 0x00202B74
Download minidriver successfully had written 251 bytes to address 0x00202C6F
Download minidriver successfully had written 251 bytes to address 0x00202D6A
Download minidriver successfully had written 251 bytes to address 0x00202E65
Download minidriver successfully had written 251 bytes to address 0x00202F60
Download minidriver successfully had written 251 bytes to address 0x0020305B
Download minidriver successfully had written 251 bytes to address 0x00203156
Download minidriver successfully had written 251 bytes to address 0x00203251
Download minidriver successfully had written 251 bytes to address 0x0020334C
Download minidriver successfully had written 251 bytes to address 0x00203447
Download minidriver successfully had written 251 bytes to address 0x00203542
Download minidriver successfully had written 251 bytes to address 0x0020363D
Download minidriver successfully had written 251 bytes to address 0x00203738
Download minidriver successfully had written 251 bytes to address 0x00203833
Download minidriver successfully had written 251 bytes to address 0x0020392E
Download minidriver successfully had written 251 bytes to address 0x00203A29
Download minidriver successfully had written 251 bytes to address 0x00203B24
Download minidriver successfully had written 21 bytes to address 0x00203C1F
Download minidriver successfully had written 8 bytes to address 0x002043FC
Launch minidriver at 0x00201000 succeeded
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Executing -- erasing chip
Downloaded 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Verified 0 code bytes ( 0.0%) and 0 data bytes ( 0.0%). Current state: Terminated with error
Chip erase timeout (nLastProgressReportTime)
What's wrong with this issue? And how to resolve?
BTW, I use SDK 2.2.0.
Solved! Go to Solution.
- Labels:
-
FlashEEPROM
-
Manufacturing and Test
- Tags:
- sflash spi
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The issue have been solved.It's SPI and I2C confliting.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Are you using the tag3 or your own product board?
Can you describe how do you program your board? Tools? Did you use a USB-to-serial converter?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1.Are you using the tag3 or your own product board?
I use our own product board.
2.Can you describe how do you program your board? Tools? Did you use a USB-to-serial converter?
I use a PL2303 USB-to-serial wire for download.The download software is wiced SDK2.2.0.
I don't change with any code of hello_sensor.Just change the name to add "recover PLATFORM_NV=SFLASH UART=COM2" to download into board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Note that we have only tested the FTDI USB to Serial cable described in this thread: Programming the TAG2/TAG3 Board using command line tools
Several on the forum have tried other cables with little to no success. You will need to review the scematic of each to verify that your cable is identical to the FTDI model (or purchase the FTDI model) as the device is extremely particular with regards to interfacing to the HCI UART.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
But the cable I have verified with BCM2073xTAG board.Download is ok for EEPROM.
You mean flash HCI is not same with EEPROM?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Confused by the reference to this product for use with the TAG board: Products
Recall that the TAG boards do not require a USB to serial cable externally as they leverage an onboard USB to serial IC from FTDI to perform this function (standard USB cable is all that is needed). These external USB to Serial cables are really only needed to program custom boards that were designed without the FTDI IC for cost or size reasons.
Note that enabling the serial flash vs. the EEPROM on the TAG board is a little tricky as well.
First make sure you can get this working using the procedure here: TAG3 Serial Flash Configuration
In addition, I see that the MX25L6406E flash you are using is not one of the two versions we have tested on the TAG3 board (both PNs are included in the blog above), so this could also be a driver issue as well.
Not sure at this point. Bringing up a custom board for the first time is often challenging from the perspective of getting the HCI UART to respond properly, so normally we ask customers to use the TAG3 board as a reference when debugging their own board.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The issue have been solved.It's SPI and I2C confliting.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thanks for updating the thread.