Sensors Forum Discussions
Browse the Community
CO₂ sensor
In this forum you can post your questions, comments and feedback about the XENSIV™ PAS CO₂ sensor, a small yet highly accurate CO₂ sensor based on photoacoustic spectroscopy (PAS) technology. This sensor is ideal for integration into smart home appliances, consumer devices and HVAC systems. Here you can also find the links to the latest board pages, GitHub, documents and FAQs.
3D Hall (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ 3D Hall sensors, a sensor family (TLx493D) which is using a hall-based technology in order to detect the strength of a magnetic field in all three dimensions, i.e. x-, y- and z-axis. This family fits into industrial and consumer applications such as control elements and joysticks. Furthermore, it is the ideal fit for low-power automotive applications like indicators and gear shifters. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Switches (Magnetic sensors)
In this forum you can post your questions, comments and feedback about the XENSIV™ Magnetic Switch sensors, a sensor family which is using e.g. a hall-based technology in order to detect the strength of a magnetic field in one dimension. Our switches can be found in a variety of consumer, industry and automotive applications like conventional block commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Radar sensor
In this forum you can post your questions, comments and feedback about Infineon's XENSIV™ radar sensors. Designed to support a wide range of industrial, consumer and automotive applications, Infineon’s millimeter wave (mmWave) radar portfolio offers both FMCW and Doppler radar sensors supporting 24GHz, 60GHz, 77/79GHz. Here you can also find the links to the latest board pages, GitHub, documents, tools and FAQs.
Angle (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Angle sensors. This sensor family is based on integrated Magneto Resistive (ixMR) technologies (e.g. GMR, TMR) in order to detect the orientation of an applied magnetic field by measuring sine and cosine angle components with monolithically integrated magneto resistive elements. Our Angle sensors can be found in a variety of consumer, industry and automotive applications like motor commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Current (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Current sensors, a sensor family which is using a hall-based technology in order to sense accurate and stable the current. Our Current sensors can be found in a variety of consumer, industry and automotive applications like traction inverters, industrial drives, photovoltaic inverters or battery disconnect systems. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
MEMS microphones
In this forum you can post your questions, comments and feedback about Infineon’s XENSIV™ MEMS microphones. Our high performance microphones can be used in a variety of application such as earbuds, headphones, smartphones or laptops for high quality audio pickup.
Pressure Sensors
Our XENSIV™ family of digital absolute barometric pressure sensors gives designers the best choice when it comes to mobile and wearable devices. Highlights include small form factors to facilitate system integration, highest precision and relative accuracy over a wide temperature range, fast read-out speeds via the serial I2C/SPI interface, and low power consumption to ensure longer battery lifetimes. All of our air sensing solutions have a FIFO buffer that can store the last 32 measurements. Since the host processor can remain in sleep mode for a longer period between readouts, the FIFO buffer can reduce system power consumption further.
Speed (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Speed sensors. This sensor family is based on integrated Magneto Resistive (ixMR) or hall-based technologies in order to determine linear and rotational speed. Our Speed sensors can be used with ferromagnetic gear tooth wheels or encoders to measure speed and position and they are essential components for the function of safety and powertrain applications like rotating shafts. Here you can also find the links to the latest board pages, documents and FAQs.
Featured Discussions
I have a Sense2GOL development kit. But I can't download the Radar Sense2GoL from the Developer Center. Is there any solution?Thanks for your kindness.
Show Lesshow can i get access to the Distance2Go IDC package
Hi all,
I'm using the DEMO BGT60LTR11AIP board. The welding point of TD,PD,VIN,GND on the board were broken so I cannot weld it and read data with arduino uno. I have a Radar MCU 7 base board, which supports reading data of the radar shield and send data to PC with Radar GUI. Is there any way that I can read motion status without Radar GUI? I mean, is there any way I can get the data from the MCU 7 base board and send it through I2C/SPI/Uart or any other communication protocol to an Arduino or STM32 or even PSoC from infineon?
Show LessDear Sir,
I am studying Infineon 2T4R radar. regarding to the function of ADC tracking setting . May I know any effect for ADC by setting a difference Duration? thanks.
Show LessHi Everyone
Questions about the Rawdata application:
1, Currently, we are measuring the distance to the wall of the room. I got the waveforms below, but the waveforms for Rx1, Rx2 and Rx3 are far apart.
Could you help me what are the possible causes?
2. I want to measure the size of the room.Is there a way to measure using the Demo BGT60 TR13C?
Is it possible to roughly measure the size of a 10mx4m, 8mx6m room?
Questions about Segmentation & Seamless Tracking:
When two people are detected, the detected person may appear or disappear on the display screen, causing false detection.
Thanks
Yang
The current Fusion Radar GUI is for evaluation purposes, but are there any plans to improve it in the future?
can you tell us how to make range or doppler spectrogram using bgt60tr13c demo board.
https://www.mdpi.com/1424-8220/22/4/1519 like as shown in this paper. in this paper spectrogram is shown by using bgt60tr13c sensor
Show LessHi, I try to use BGT60TR13C to get raw data.and I get raw.bin and raw.txt files.According to help in radar fusion GUI.I know which part is the data.but I don't understand that what's the specific meaning of each data.May I get some suggestions about how to learn about the meaning of them?And what's the difference between them?
Show Less
HI,
I bought BGT60TR13C before.But when I connected the board with PC.In the Fusion GUI It has showed'no deviced detected'.I go to Device and select Flash Firmware.but I can't select device there.What should I do for it?
Show LessI used sense2Gol pulse radar to detect vibration but the results was not good is position 2go suitable to detect machine vibration or not. if no what type of radar is recommend to measure machine vibration.
Show Less