Sensors Forum Discussions
Browse the Community
CO₂ sensor
In this forum you can post your questions, comments and feedback about the XENSIV™ PAS CO₂ sensor, a small yet highly accurate CO₂ sensor based on photoacoustic spectroscopy (PAS) technology. This sensor is ideal for integration into smart home appliances, consumer devices and HVAC systems. Here you can also find the links to the latest board pages, GitHub, documents and FAQs.
3D Hall (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ 3D Hall sensors, a sensor family (TLx493D) which is using a hall-based technology in order to detect the strength of a magnetic field in all three dimensions, i.e. x-, y- and z-axis. This family fits into industrial and consumer applications such as control elements and joysticks. Furthermore, it is the ideal fit for low-power automotive applications like indicators and gear shifters. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Switches (Magnetic sensors)
In this forum you can post your questions, comments and feedback about the XENSIV™ Magnetic Switch sensors, a sensor family which is using e.g. a hall-based technology in order to detect the strength of a magnetic field in one dimension. Our switches can be found in a variety of consumer, industry and automotive applications like conventional block commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Radar sensor
In this forum you can post your questions, comments and feedback about Infineon's XENSIV™ radar sensors. Designed to support a wide range of industrial, consumer and automotive applications, Infineon’s millimeter wave (mmWave) radar portfolio offers both FMCW and Doppler radar sensors supporting 24GHz, 60GHz, 77/79GHz. Here you can also find the links to the latest board pages, GitHub, documents, tools and FAQs.
Angle (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Angle sensors. This sensor family is based on integrated Magneto Resistive (ixMR) technologies (e.g. GMR, TMR) in order to detect the orientation of an applied magnetic field by measuring sine and cosine angle components with monolithically integrated magneto resistive elements. Our Angle sensors can be found in a variety of consumer, industry and automotive applications like motor commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Current (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Current sensors, a sensor family which is using a hall-based technology in order to sense accurate and stable the current. Our Current sensors can be found in a variety of consumer, industry and automotive applications like traction inverters, industrial drives, photovoltaic inverters or battery disconnect systems. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
MEMS microphones
In this forum you can post your questions, comments and feedback about Infineon’s XENSIV™ MEMS microphones. Our high performance microphones can be used in a variety of application such as earbuds, headphones, smartphones or laptops for high quality audio pickup.
Pressure Sensors
Our XENSIV™ family of digital absolute barometric pressure sensors gives designers the best choice when it comes to mobile and wearable devices. Highlights include small form factors to facilitate system integration, highest precision and relative accuracy over a wide temperature range, fast read-out speeds via the serial I2C/SPI interface, and low power consumption to ensure longer battery lifetimes. All of our air sensing solutions have a FIFO buffer that can store the last 32 measurements. Since the host processor can remain in sleep mode for a longer period between readouts, the FIFO buffer can reduce system power consumption further.
Speed (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Speed sensors. This sensor family is based on integrated Magneto Resistive (ixMR) or hall-based technologies in order to determine linear and rotational speed. Our Speed sensors can be used with ferromagnetic gear tooth wheels or encoders to measure speed and position and they are essential components for the function of safety and powertrain applications like rotating shafts. Here you can also find the links to the latest board pages, documents and FAQs.
Featured Discussions
in the driver sensor-xensiv-dps3xx-master.zip (downloaded from https://github.com/Infineon/sensor-xensiv-dps3xx), there are two files with license texts (LICENSE & EULA).
Which of the two license text is the current one? Where can I request this information?
Thank you very much
Thomas
the original driver writes values to undocumented registers 0x0E, 0x0F & 0x62 (neither in the datasheet for the DPS368 nor DPS310).
See function _xensiv_dps3xx_correct_temperature in xensiv_dps3xx.c (below)
Can anyone tell me anything about this function?
Thank you very much
Thomas
static cy_rslt_t _xensiv_dps3xx_correct_temperature(xensiv_dps3xx_t* dev)
{
uint8_t write_data = 0xA5;
cy_rslt_t rc = _xensiv_dps3xx_reg_write(dev, 0x0E, &write_data, 1);
if (rc == CY_RSLT_SUCCESS)
{
write_data = 0x96;
rc = _xensiv_dps3xx_reg_write(dev, 0x0F, &write_data, 1);
}
if (rc == CY_RSLT_SUCCESS)
{
write_data = 0x02;
rc = _xensiv_dps3xx_reg_write(dev, 0x62, &write_data, 1);
}
if (rc == CY_RSLT_SUCCESS)
{
write_data = 0x00;
rc = _xensiv_dps3xx_reg_write(dev, 0x0E, &write_data, 1);
}
if (rc == CY_RSLT_SUCCESS)
{
write_data = 0x00;
rc = _xensiv_dps3xx_reg_write(dev, 0x0F, &write_data, 1);
}
return rc;
}
Show Less
Hello, when using the DEMO BGT60tr13c evaluation version for radar sensor evaluation, I encountered a problem where the Radar Fusion GUI interface was unable to display data
Phenomenon description:
1. Radar Fusion GUI can detect sensors
2. No data is displayed after entering the interface
3. The DEMO board is always flashing green
I want to ask what is usually the cause of this
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E9%9B%B7%E8%BE%BE%E4%BC%A0%E6%84%9F%E5%99%A8/DEMO-BGT60TR13C%E8%AF%84%E4%BC%B0%E7%89%88%E6%97%A0%E6%B3%95%E9%87%87%E9%9B%86%E6%95%B0%E6%8D%AE/td-p/635786
Show LessPlz give steps to compile this
D:\IFX_D2GL-HW-SW_V1.0.0\Firmware_Software\Communication Library\ComLib_C_Interface\examples\D2GL_basics
I am trying to compile this to get raw data but some errors are coming , I included library also but I don't know why.
thank you
Show LessI have extracted the raw data but do not know how to analyze them. So where i can see the Protocol of raw data
Problem description:OSError: /usr/..libradar_sdk.so: cannot open shared object file: No such file or directory (PS:full context in the end)
Problem generated from: I try to config this radar to collect data by running python script on a Raspberry Pi 4B, but this error came out, I tried solutions all failed including:
1.add working path or lib path folder to ~/.bashrc or LD_LIBRARY_PATH or /etc/profile or /etc/ld.so.conf; even just copy the lib file to PATH like /usr/lib etc; meanwhlie I am pretty sure this .so file is in right path and it does exists. And the error is always the same: No such file or directory.
2.change newer verison raspberry pi operating system; use the libradar_sdk.so in linux_raspi(32bit) in official sdk and cmd info says error ELF32bit meaning the .so file was not correponding to the OS bits.
3.change libradar_sdk.so to libsdk_avian.so, use the latest sdk's counterparts(linux_x64)
4.I previously used the same python scripts on windows 10, and it can work very well even can work in win11 on raspberry4B. The only difference is in Avian.py it depends on libradar_sdk.dll instead of libradar_sdk.so. And as the problem mentioned before, it just can not find this .so file.
Here's my develop situation:
Radar device:BGT60ATR24C
radar_sdk version:3.3.0 (latest 3.5.1)
firstly pip installed: ifxAvian-3.3.0-py3-none-any.whl
related sdk python scripts: main.py(just init_radar and get_frame very simple codes) Avian.py Common.py
the OS version: linux raspberry pi 5.10.63 aarch64(python 3.9.2 built-in)
FULL Cmd Error description:
Traceback (most recent call last):
File "/home/pi/Desktop/PPG/ifxAvian/data_collect_V31.py", line 31, in <module>
from ifxAvian import Avian
File "/usr/local/lib/python3.9/dist-packages/ifxAvian/Avian.py", line 101, in <module>
class Device():
File "/usr/local/lib/python3.9/dist-packages/ifxAvian/Avian.py", line 136, in Device
@handle_errors(dll())
File "/usr/local/lib/python3.9/dist-packages/ifxAvian/Common.py", line 53, in inner
cache[func] = func(*args, **kwargs)
File "/usr/local/lib/python3.9/dist-packages/ifxAvian/Avian.py", line 55, in dll
lib = load_library("radar_sdk")
File "/usr/local/lib/python3.9/dist-packages/ifxAvian/Common.py", line 289, in load_library
dll = CDLL(find_library(libname))
File "/usr/lib/python3.9/ctypes/__init__.py", line 374, in __init__
self._handle = _dlopen(self._name, mode)
OSError: /usr/local/lib/python3.9/dist-packages/ifxAvian/libradar_sdk.so: cannot open shared object file: No such file or directory------------------
(program exited with code: 1)
Press return to continue
Environment description:
- STM32G0B1RET6 (64MHz bus) I2C1, 400kHz fast mode, configured for DMA communication, calls and configuration functions are all HAL libraries
- There are 3 TLV493D-A2BW sensors on the I2C1 bus. The 3 PMOS controls the VDD and 3.3 V connections respectively (the PMOS switch test is valid)
- The I2C1 bus SCL and SDA have 1.2kΩ pull-up resistors. The pull-up 3.3V is always present, and SCL and SDA do not have matching resistors to connect to the terminals
- The INT pins of the three TLV493D-A2BW sensors are each connected to the MCU's IO (input mode)
The hardware connection has been checked and there are no problems
Problem:
At the time of testing, the initial state was only one of the PMOS enabled to power up a TLV493D-A2BW. It felt like there was no response to ACK. After sending a written command for the first time, it returned HAL_BUSY
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/3D-Hall-%E7%A3%81%E6%80%A7%E4%BC%A0%E6%84%9F%E5%99%A8/TLV493D-A2BW-I2C%E9%80%9A%E4%BF%A1%E9%97%AE%E9%A2%98/td-p/634583
Show LessCan someone kindly explain in steps how can i extract raw data on MATLAB using Position2Go Board to plot the range doppler graph?
I have Distance2GoL XENSIV™ 24 GHz low-power radar shield BGT24LTR11
In Radar GUI I am getting output and also converting it to .txt file while recording.
but how to get data directly from the serial port.
I am trying to take data without using radar GUI instead I need data directly from the Serial port
and another question is :
can I use this Distance2GoL XENSIV™ 24 GHz low-power radar shield BGT24LTR11 with Arduino IDE
Show Less