Sensors Forum Discussions
Browse the Community
CO₂ sensor
In this forum you can post your questions, comments and feedback about the XENSIV™ PAS CO₂ sensor, a small yet highly accurate CO₂ sensor based on photoacoustic spectroscopy (PAS) technology. This sensor is ideal for integration into smart home appliances, consumer devices and HVAC systems. Here you can also find the links to the latest board pages, GitHub, documents and FAQs.
3D Hall (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ 3D Hall sensors, a sensor family (TLx493D) which is using a hall-based technology in order to detect the strength of a magnetic field in all three dimensions, i.e. x-, y- and z-axis. This family fits into industrial and consumer applications such as control elements and joysticks. Furthermore, it is the ideal fit for low-power automotive applications like indicators and gear shifters. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Switches (Magnetic sensors)
In this forum you can post your questions, comments and feedback about the XENSIV™ Magnetic Switch sensors, a sensor family which is using e.g. a hall-based technology in order to detect the strength of a magnetic field in one dimension. Our switches can be found in a variety of consumer, industry and automotive applications like conventional block commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Radar sensor
In this forum you can post your questions, comments and feedback about Infineon's XENSIV™ radar sensors. Designed to support a wide range of industrial, consumer and automotive applications, Infineon’s millimeter wave (mmWave) radar portfolio offers both FMCW and Doppler radar sensors supporting 24GHz, 60GHz, 77/79GHz. Here you can also find the links to the latest board pages, GitHub, documents, tools and FAQs.
Angle (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Angle sensors. This sensor family is based on integrated Magneto Resistive (ixMR) technologies (e.g. GMR, TMR) in order to detect the orientation of an applied magnetic field by measuring sine and cosine angle components with monolithically integrated magneto resistive elements. Our Angle sensors can be found in a variety of consumer, industry and automotive applications like motor commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Current (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Current sensors, a sensor family which is using a hall-based technology in order to sense accurate and stable the current. Our Current sensors can be found in a variety of consumer, industry and automotive applications like traction inverters, industrial drives, photovoltaic inverters or battery disconnect systems. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
MEMS microphones
In this forum you can post your questions, comments and feedback about Infineon’s XENSIV™ MEMS microphones. Our high performance microphones can be used in a variety of application such as earbuds, headphones, smartphones or laptops for high quality audio pickup.
Pressure Sensors
Our XENSIV™ family of digital absolute barometric pressure sensors gives designers the best choice when it comes to mobile and wearable devices. Highlights include small form factors to facilitate system integration, highest precision and relative accuracy over a wide temperature range, fast read-out speeds via the serial I2C/SPI interface, and low power consumption to ensure longer battery lifetimes. All of our air sensing solutions have a FIFO buffer that can store the last 32 measurements. Since the host processor can remain in sleep mode for a longer period between readouts, the FIFO buffer can reduce system power consumption further.
Speed (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Speed sensors. This sensor family is based on integrated Magneto Resistive (ixMR) or hall-based technologies in order to determine linear and rotational speed. Our Speed sensors can be used with ferromagnetic gear tooth wheels or encoders to measure speed and position and they are essential components for the function of safety and powertrain applications like rotating shafts. Here you can also find the links to the latest board pages, documents and FAQs.
Featured Discussions
Hi
I am developing a radar module using BGT60TR13C+ STM32F730.
Since the library provided by Infineon cannot be used directly on the STM32 chip, we are developing a method of writing/reading information by directly accessing the registers provided in the manual.
I would like to ask a question as I have found some problems in proceeding with this method.
1) Is BGT60TR13C operated at default settings when external power is connected?
2) If there is no default setting, which register should be set to operate TX, ADC, etc. of BGT60TR13C?
3) What settings value are needed to drive BGT60TR13C for basic operation?
4) Is there a register full manual for setting and obtaining information?
5) Is there a way to apply/port the code provided by Infineon to the STM32 chip?
Thanks for your time
Regards
Oneman
Show LessHi all,
After reflow soldering sensor DSP368 to PCB, i want to add protect holder to PCB, but i need to preheat glue to add the holder. But the glue Heat Cure Time @ 150ºC ,30minutes => Is The sensor DPS368 OK after Heat cure ?
Thanks,
Show LessBGT24ATR11 相关的参考设计,目前准备使用此款芯片做雷达液位计
Hi,
I have some question regarding the BGT60LTR11AIP (+Shield + MCU7 radar baseboard):
When using Radar Fusion GUI_1.5.4 to detect sensor BGR60LTR11AIP, the LEDs on the sensor and development board can light up normally and change colors when objects are moving. However, the device cannot be found in the software Radar Fusion GUI_1.5.4. I want to manually update the firmware, but there is no response from the device or firmware version drop-down box in the Decision ->Flash Firmware dialog box. I have reviewed the solutions on the forum regarding BGR60LTR11AIP No Decided, but I have not found where to download the "Radar BGT60LTR11AIP" software and the file "InitializeBGTxxx. bat", and where should I download this file.
Radar Fusion Gui Version: v3.5.4
Thanks for your time,
Regards,
xiao
Show LessAre there available instructions or guidance on connecting the BGT60TR13C development kit to a jetson orin nano? Or a way to compile the sdk for the jetson? Following the "Building SDK from source code" in the RFS SDK Documentation in the radar_sdk didn't work for compile or install using python wheel.
Show LessTLE5012B The E1000 reads and writes the MODE3 register, and after I write the angle value in, occasionally the value read out is 0X8091, not the value I wrote in.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/%E8%A7%92%E5%BA%A6-%E7%A3%81%E6%80%A7%E4%BC%A0%E6%84%9F%E5%99%A8/TLE5012B-E1000%E8%AF%BB%E5%86%99%E5%AF%84%E5%AD%98%E5%99%A8/td-p/740382
Show LessDear Sir,
I would like to define the angle versus SIN (N) Sin(P) Voltage table. (0deg~120deg)
does Infineon have the table for reference, thanks.
Show LessDear Team,
my customer develop the traction inverter based on hybridepack 1200V SiC board.
below are support needs could you kindly comment below?
1.Can magnetic sensor TLE5309D replace the resolver on EV traction inverter application? What kind of position sensor can use in traction inverter and meet ASIL-C requirement?
2.Can energy recovery share same group of SiC modules? How it work?
3.The gaol of input voltage ripple below 2%, how can I select the DC-link capacitor capacity in ?uF
Regards,
Bard
Show LessHello: The IM72D128 chip's receiving hole, can it resist salt spray corrosion, thank you.
smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/MEMS%E9%BA%A6%E5%85%8B%E9%A3%8E/IM72D128%E7%8E%AF%E5%A2%83%E9%80%82%E5%BA%94%E6%80%A7%E9%97%AE%E9%A2%98/td-p/739370
Show LessHi,
I am using BGT60TR13C radar development kit on the Jetson Orin NX but all the provided libraries such as motionangle is not compatible when building code.
Is there any version of the radar_sdk for linux-aarch64 which I can use?
Thank you,
Best regards
Show Less