Sensors Forum Discussions
Browse the Community
CO₂ sensor
In this forum you can post your questions, comments and feedback about the XENSIV™ PAS CO₂ sensor, a small yet highly accurate CO₂ sensor based on photoacoustic spectroscopy (PAS) technology. This sensor is ideal for integration into smart home appliances, consumer devices and HVAC systems. Here you can also find the links to the latest board pages, GitHub, documents and FAQs.
3D Hall (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ 3D Hall sensors, a sensor family (TLx493D) which is using a hall-based technology in order to detect the strength of a magnetic field in all three dimensions, i.e. x-, y- and z-axis. This family fits into industrial and consumer applications such as control elements and joysticks. Furthermore, it is the ideal fit for low-power automotive applications like indicators and gear shifters. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Switches (Magnetic sensors)
In this forum you can post your questions, comments and feedback about the XENSIV™ Magnetic Switch sensors, a sensor family which is using e.g. a hall-based technology in order to detect the strength of a magnetic field in one dimension. Our switches can be found in a variety of consumer, industry and automotive applications like conventional block commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Radar sensor
In this forum you can post your questions, comments and feedback about Infineon's XENSIV™ radar sensors. Designed to support a wide range of industrial, consumer and automotive applications, Infineon’s millimeter wave (mmWave) radar portfolio offers both FMCW and Doppler radar sensors supporting 24GHz, 60GHz, 77/79GHz. Here you can also find the links to the latest board pages, GitHub, documents, tools and FAQs.
Angle (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Angle sensors. This sensor family is based on integrated Magneto Resistive (ixMR) technologies (e.g. GMR, TMR) in order to detect the orientation of an applied magnetic field by measuring sine and cosine angle components with monolithically integrated magneto resistive elements. Our Angle sensors can be found in a variety of consumer, industry and automotive applications like motor commutation in brushless drives (BLDC). Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
Current (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Current sensors, a sensor family which is using a hall-based technology in order to sense accurate and stable the current. Our Current sensors can be found in a variety of consumer, industry and automotive applications like traction inverters, industrial drives, photovoltaic inverters or battery disconnect systems. Here you can also find the links to the latest board pages, GitHub, documents, simulation tools and FAQs.
MEMS microphones
In this forum you can post your questions, comments and feedback about Infineon’s XENSIV™ MEMS microphones. Our high performance microphones can be used in a variety of application such as earbuds, headphones, smartphones or laptops for high quality audio pickup.
Pressure Sensors
Our XENSIV™ family of digital absolute barometric pressure sensors gives designers the best choice when it comes to mobile and wearable devices. Highlights include small form factors to facilitate system integration, highest precision and relative accuracy over a wide temperature range, fast read-out speeds via the serial I2C/SPI interface, and low power consumption to ensure longer battery lifetimes. All of our air sensing solutions have a FIFO buffer that can store the last 32 measurements. Since the host processor can remain in sleep mode for a longer period between readouts, the FIFO buffer can reduce system power consumption further.
Speed (Magnetic sensor)
In this forum you can post your questions, comments and feedback about the XENSIV™ Speed sensors. This sensor family is based on integrated Magneto Resistive (ixMR) or hall-based technologies in order to determine linear and rotational speed. Our Speed sensors can be used with ferromagnetic gear tooth wheels or encoders to measure speed and position and they are essential components for the function of safety and powertrain applications like rotating shafts. Here you can also find the links to the latest board pages, documents and FAQs.
Featured Discussions
Hi,
I am using a DEMO BGT60TR13C with #MCU7 Baseboard and the Python3 ifxAvian package and am trying to understand the raw data coming from the sensor after acquiring a frame:
from ifxAvian import Avian
with Avian.Device() as device:
config = Avian.DeviceConfig(
sample_rate_Hz=1_000_000,
rx_mask=1,
tx_mask=1,
if_gain_dB=33,
tx_power_level=31,
start_frequency_Hz=60e9,
end_frequency_Hz=61.5e9,
num_chirps_per_frame=128,
num_samples_per_chirp=64,
chirp_repetition_time_s=0.0005,
frame_repetition_time_s=0.25,
mimo_mode="off",
)
device.set_config(config)
f = device.get_next_frame()
print(f.shape)
print(f)
# (1, 128, 64)
# [[[0.45470086 0.41855922 0.4058608 ... 0.4859585 0.4893773 0.46984127]
# [0.45274726 0.41807082 0.4068376 ... 0.4869353 0.4893773 0.46984127]
# [0.45177045 0.41807082 0.4063492 ... 0.4859585 0.4888889 0.46886447]
# ...
# [0.45347986 0.41855922 0.4056166 ... 0.4888889 0.4903541 0.46837607]
# [0.45250306 0.41807082 0.4043956 ... 0.4884005 0.4908425 0.46837607]
# [0.45372406 0.41855922 0.4058608 ... 0.4884005 0.4901099 0.46788767]]]
I understand that the shape of the array is determined by (rx_antenna_count, num_chirps_per_frame, num_samples_per_chirp).
However I don't understand the individual cell values.
What do the numbers represent? Do they have a unit?
Thanks,
Jannik
Show Less
Hi all,
I'm using TLI4971-A505T5-U-E0001 to measure current of H bridge DC motor. I want to use Aout in Analog output mode. But when motor start, sometime Aout jump in to Communication mode, that makes analog reading wrong.
Can you give me the troubleshooting?
Thanks!
Show Less
Dear support,
I have got a couple of questions regarding the magnetic operating conditions of the device.
The IC will be used in a configuration with back-biasing.
The following operating conditions are stated in the datasheet of TLE4953C:
- Pre-induction: +/- 500 mT
My understanding ist, that the dynamic range is maximum +/- 500 mT on all three channels (L, R, C) and for me as an integrator I have to ensure that this limit is not exceeded, even at the minimum possible air gap? Basically the flux density has always to be below +/- 500 mT for all three hall elements? Is this understanding correct? - Pre-induction offset between outer probes: +/- 20 mT
Suppose the dB = L-R signal is non-symmetrical. The positive peak is 42 mT and the negative peak is 0 mT. The peak-to-peak value would be within the specification, but there would be an offset of 21 mT present. Does this limit refer to (max(dB)-min(dB))/2<20 mT? If my understanding is correct, I would not maintain the allowed operating range? - Pre-induction offset between mean of outer probes and center probe: +/- 20 mT
Basically same question as point 2. I calculate based on this equation dBdir = (L+R)/2-C the differential directional signal and check (max(dBdir)-min(dBdir))/2<20 mT? Is this again the correct approach? I attached some simulation results for a non-symmetrical Bdir case (upper plot raw flux densities, then dB and dBdir). - Differential: +/- 120 mT
Does this value refer to the positive and negative peak of the dB = L-R signal? - Note: Limit threshold speed 0Hz ≤ f ≤ 2500Hz +1.5 mT. The stated condition is 50% missing pulses. Is there as well a flux density limit for which let's say 99.99966 % of all pulses are detected. I used guard banding by using dB >= 4 mT as the allowed lower limit for the simulation, but I am not sure what the expectation for the missing pulses would be.
- Note: Limit differential direction signal 0Hz ≤ f ≤ 1100Hz +0.73 mT. The stated condition is: "just one pulse missing out of 100". Does that mean, there will be no directional pulse width shown on the output for this single pulse or the entire pulse is missing?
Thank you for your support.
Regards
Show Less
Hi
I am running
MCU V2.2 03/2020
Shield V2.0
RadarBaseboardMCU7_v2512.bin
SDK v3.4.0
RadarFusionGuide v3.3.0
I try using Matlab MatlabWrapperConnectOnly.m
in the example files and get the error code "no compatible device found (IFX_ERROR_NO_DEVICE)"
I looked around here and read posts about version issues compatible to the SDK. I think my hard/firmware is up to date,
I just uploaded the newest firmware
Any idea what could be the issue?
Thanks
WW
Show Less
Hello. The issue I inquired about last time has been successfully resolved, thanks to your previous advice.
I have one more question I'd like to ask. / (using sensors: TLE493D-W2B6 A0, A1)
When a magnet is placed near the sensor, the values are consistently received. However, when the magnet is not near the sensor, I believe values close to 0 should be measured.
But, values close to 0x00 and 0xff irregularly appear when the magnet is not near the sensor.
I don't understand why 0xff values are coming in. Is there a reason for such extreme differences in values to periodically occur when there is no magnetic presence near the sensor?
Or are there certain initial settings that need to be done to prevent this? Currently, I believe I can handle this through exception handling, but I'm curious, so I wanted to ask.
TLE493D-W2B6 A0 TLE493D-W2B6 A1
Show LessI am using the Arduino IDE's Cartesiar sample program, but it cannot effectively detect the position. I don't know where the setting is wrong. The execution result is as follows:
Show Less
Hello,
I have KIT_CSK_BGT60TR13C and I want to test the sensor for presence detection. There are some parameters to set, shown in the following tables:
I've understood that hight sensitivity could be good for detection micromovements, max_range is the limit in terms of meters for the detection and the thresholds allow to detect the presence or not.
Moreover with setting the mode you could see only micromovements, only macromovements or both.
1.Do you have any experience with this component?
2.Could you suggest me an example of setting for detection face micromovements?
3. Is there a report after the test (with all the information that I have used)?
4.Do you know if on Modus Toolbox and for KIT_CSK_BGT60TR13C is available this :
Thanks a lot for the support.
Best regards
Show Less
Hello,
we are planning to use the upcoming BGT60UTR11AIP in a new development project. Is there any information regarding countries that do not allow the deployment of 60GHz radar sensors or just allow certain frequency bands/ranges? This seems to be the case for 120GHz radars if i am informed correctly... I have also heard of countries that require radar sensors of certain frequencies to be registered. Regarding this is there anything to keep an eye on with this new chip?
Thanks.
Show Less Regarding the BGT24LTR11N16,
please let me know if the VCO output can oscillate when the input range of V_TUNE is 0V to 3.3V(Vcc).
Alternatively, please tell me the input voltage range of V_TUNE for BGT24LTR11N16.
In fact, when I applied 0 to 3.3 (VCC) to V_tune in the environment of -30℃ to 75℃ and observed the BGT24LTR11N16TX output with the spectrum analyzer, I was able to observe the oscillation output at any temperature.
On the other hand,
In the datasheet of BGT24LTR11N16,
at the section 2.4 TX Section, it is stated that "Tuning voltage to cover VCO frequency range" is 0.7V to 2.5V.
Another specification item "VCO frequency range" was 24.05 to 24.25GHz.
As an interpretation of the above specification,
I interpreted "Tuning voltage to cover VCO frequency range" as the voltage range specification to cover the "VCO frequency range" specification.
Is this interpretation correct?
In addition,
For my application,
There is no problem with lower TX output level.
There is no problem due to the temperature characteristics of the oscillation frequency, and it is a good use as long as the oscillation output is produced.
I don't have the sufficient information of the VCO internal circuit of BGT24LTR11N16,
but it is a BiCMOS MMIC, and is estimated to be an LC Voltage-Controlled Oscillator using a Variable Capacitance Diode.
If so, V-tune would be able to oscillate in the range of 0 to 3.3V (VCC), and the experimental results would be understandable.
Please support me regarding the above.