Browse the Community
OPTIGA™ Trust
High-end easy to use security solutions that provide an anchor of trust for your application, connecting IoT devices to the cloud, giving billons of device its own unique identity, pre-personalized turnkey solutions, zero-touch onboarding, high performance, ... We did not meet your expectations? Let us know!
OPTIGA™ TPM
OPTIGA™ TPM (Trusted Platform Module) offers a broad portfolio of standardized security controllers to protect the integrity and authenticity of embedded devices and systems. With a secured key store and support for a variety of encryption algorithms, OPTIGA™ TPM security chips provide robust protection for critical data and processes through their rich functionality. OPTIGA™ TPM security controllers are ideal for platforms running both Windows and Linux and its derivatives (SLB 9645 product versions for Chrome OS available). Based on Trusted Computing Group (TCG) standards, they support the TPM 1.2 or the latest innovative TPM 2.0 standard.
Recent discussions
Hi,
I am trying to interface SLB 9670VQ2.0 via SPI BUS and after configuring kernel to enable the required module, The device is going into time out mode. I also found a kernel patch which corresponds the problem of timeout but the patch is not currently integrated into the main line kernel.
https://lore.kernel.org/lkml/1229fbc4-0abd-376e-a9d7-ccdd6d56c2ae@gmx.de/t/
My question is,
If I spare a GPIO pin as a reset pin and assigned it to SLB 9670VQ2.0 then it will be enough for the SLB 9670VQ2.0 to come out of timeout phase or do i also need an implementation at the Linux kernel driver level to toggle the reset pin?
Regards
Ata
Show LessHi
I'm working on secure boot on TI omapl138 soc using TPM1.2 slb9645, I am able to detect TPM chip through I2C, But i didn't get any data sheet or technical reference module to know how TPM 1.2 works and register/memory addresses, To develop further can you please provide detailed documents of TPM 1.2 slb9645.
Thanks & regards
Yashwanth T L
Show LessHello All,
I'm trying to bringup TPM2.0-SLB9670VQ2.0 in "uboot2016" for IPQ8072 qualcomm chipset.
Would be great if some one pls share some docs/references or pointers.
thanks in advance..
Gourav Jain
Show LessHi Team,
Does Infineon have a TPM module which is FIPS 140-3 compliant or certified? I currently use SLB 9670VQ2.0 which is FIPS 140-2 certified and would like to move to FIPS 140-3.
Thanks and Regards,
Shahasan Noushad
Show Less
Hello, everyone, I bought an evaluation board iridium 9645 ( IRIDIUM9645TPMI2CTOBO1), with an SLB9645 TPM 1.2, but I can't find any datasheet to plug this board on a raspberry pi 3B (40 pins header). Could you provide the datasheet? If there is no datasheet, could you tell me what is the interest of the two jumpers, the 28 pins header, the 6 pins headers? The 26 pins header for raspberry? Where should I plug it on the header of my raspberry pi 3B, and in what way should I plug it?
Regards,
David
Show LessHi Infineon Team,
I'm trying to interface TI omapl138 soc with TPM1.2 slb9645 through Driver module (DM)_I2C, But facing problem with integration via U-boot not able to detect TPM chip on I2C bus. I'm looking for a U-boot driver/source code to interface TPM1.2 slb9645, Presently I am using U-Boot 2018.01.
Thanks & regards,
Yashwanth T L
Show LessCan you provide link to get detailed datasheet of SLJ52ACA150A1VQFN32XUMA1 including part number details and technical details like single pin interface to FPGA.
We are interfacing SLJ52ACA150A1 with FPGA LFE5UM-45F (lattice) using single wire for DATA I/O, RST and CLK pins. Need any example schematic. Specifically we need pull-up value required on DATA pin (if required) and any other similar interface details.
Show LessWhat is the difference between VQFN-32-20 and VQFN-32-13? what 13 and 20 represents
Hi
Good day.
We have programming requirements for SLB9665 and SLB9670, and we are evaluating to implement TPM programming/provisioning to our programming systems. We have HSM and CA server, and we need the more detail information about LPC/SPI protocol and programming flow to implement. We have tried to find the source code from github, but it seems based on the OS to execute the IC provisioning.
May i know any documents about the detail (protocol and flow and command..) for third party?
Thank you.
Jack
Show Less