Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

SRAM

Anonymous
Not applicable

Hi,

   

AN6017, table 1: "Burst of 2 QDR II+/DDR II+ support 333 MHz and Burst of 4 QDR II+/DDR II+ support 550 MHz as highest frequency."

   

Is this a relevant restriction?

0 Likes
3 Replies
PriteshM_61
Employee
25 solutions authored 10 solutions authored 5 solutions authored
Employee

 Hi,

   

 

   

I am not sure if I have understood your question. Could you please elborate the same!

0 Likes
Anonymous
Not applicable

According to the AN6017 the maximum frequency of burst of 2 DDR II+ device is 333 MHz. But it is false, isn't it? For example, CY7C1168KV18 support 550 MHz.

0 Likes
Bob_Marlowe
Level 10
50 questions asked 10 questions asked 1000 solutions authored
Level 10

When you look at the datasheet of the CY7C1168KV18 you provided, you will see under "Ordering Information" that the device comes in different speed versions, from 400 MHz up to 550MHz.

   

 

   

Bob

0 Likes