Announcements

Community will be in read-only mode on 25th Sep for 10 hours. Click here for more details

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

SRAM Forum Discussions

Sort by:
rkm151
SRAM
Hello,   I'd like the direct technical contact for discussing CY62138FV30LL‐45ZXI.  I would like to discuss getting or collecting lot data for the sta... Show More
MAO
SRAM
The device here lists 1.65 V-2.2 V and 4.5 V-5.5 V, but not 2.2 V-3.6 V. If I want to run the device at 3 V, should I use the 5 V value as a reference... Show More
MAO
SRAM

CY62187G30-55BAXI Please let me know when you will start mass production of this product.

H512369
SRAM

Can you please share BSDL file for part numbers CY14B101LA-SP25XI and CY14B101LA-SZ25XI.

 

bala1943
SRAM
Comparison between the two as seen from the Logic Block Diagrams & Pin configurations as shared here in  gives one to understand , there is No differe... Show More
Harshitha
SRAM
CY7C2663KV18 NC Pins some of the NC Pins can I connect to GND and VDDQIn my design Iam using CY7C2663KV18 QDR-II part.For NC Pins connection, in datas... Show More
MAO
SRAM
  (1) In the RAM ARRAY section, 1M x 16/2M x 8 is shown, and depending on the input status of the control signal, either of these configurations can b... Show More
MAO
SRAM
Are there any time restrictions, etc. for BHE/BLE with respect to address signals? For example, Liontech's SRAM LY62L409716A(https://protect2.fireeye.com/v1/url?k=31323334-501d0a38-31314cae-454441504e31-b458843b1000309f&q=1&e=e607cbae-0409-4a20-a0c6-d6eae17bbeb4&u=http%3A%2F%2Fwww.lyontek.com.tw%2Fpdf%2Flp%2FLY62L409716A-1.2.pdf%29%25E3%2581%25A7%25E3%2581%25AF%25E3%2580%2581... Show More
bala1943
SRAM
Need a clarification for CY62157EV30LL-45ZSXI (Supposed to be 90nm Process Product ) received with Mark Die Revision AB33 which is from UMC Fab site 1... Show More
NaMo_1534561
SRAM
Hello, The customer is considering reducing the power consumption of equipment that is in standby mode for a long period of time.The power supply to S... Show More