SRAM Forum Discussions
Hi, the DDR2+ SRAM parts are supposed to have ODT on the DATA lines... but I don't see it in the ibis model. I see it on the BWS and K/K* though.
Example from ddr2pb2l25_cy21xx.ibs (You can see where it says what the driving output impedance is, but the input impedance is unknown):
[Model Selector] DATAIO
|
DATAIO50_TT_1.5 DATAIO models (50ohms) at TT conditions - 1.5V I/O
DATAIO50_FF_1.5 DATAIO models (50ohms) at FF conditions - 1.5V I/O
DATAIO50_TSF_1.5 DATAIO models (50ohms) at Typ Slow Fast conditions- 1.5V I/O
DATAIO30_TT_1.5 DATAIO models (30ohms) at TT conditions - 1.5V I/O
DATAIO30_FF_1.5 DATAIO models (30ohms) at FF conditions - 1.5V I/O
DATAIO30_TSF_1.5 DATAIO models (30ohms) at Typ Slow Fast conditions- 1.5V I/O
DATAIO40_TT_1.5 DATAIO models (40ohms) at TT conditions - 1.5V I/O
DATAIO40_FF_1.5 DATAIO models (40ohms) at FF conditions - 1.5V I/O
DATAIO40_TSF_1.5 DATAIO models (40ohms) at Typ Slow Fast conditions- 1.5V I/O
DATAIO60_TT_1.5 DATAIO models (60ohms) at TT conditions - 1.5V I/O
DATAIO60_FF_1.5 DATAIO models (60ohms) at FF conditions - 1.5V I/O
DATAIO60_TSF_1.5 DATAIO models (60ohms) at Typ Slow Fast conditions- 1.5V I/O
DATAIO70_TT_1.5 DATAIO models (70ohms) at TT conditions - 1.5V I/O
DATAIO70_FF_1.5 DATAIO models (70ohms) at FF conditions - 1.5V I/O
Thank you.
Show LessDid you know that some of the Cypress MoBL SRAM's have a Byte Power Down feature, wherein, if the Byte Enables are disabled together, the chip would seamlessly transition into standby mode? This helps in significant power savings in power-critical applications. Please see the Cypress MoBL SRAM datasheets for more information?
Show LessDid you know that Cypress MoBL SRAM's are very popular for their use in BBSRAM (Battery Backed SRAM) designs? Please see Application note http://www.cypress.com/?rID=12710 that discusses some Design considerations for such applications.
Show LessAt what frequency do you recommend that we need to use the ODT feature?
Does Cypress have any plan to include ECC in future memory products?
LVTTL is a JEDEC standard that references the input signal to ground. The output switching range is 0.4 to 2.4V for 3.3V LVTTL and 0.4 to 2.2V for 2.5V LVTTL .
HSTL is a technology-independent interface standard for digital ICs that calibrates the input signal to a reference voltage rather than to ground. This calibration enables a smaller I/O swing and improves performance. HSTL was developed for voltage-scalable and technology-independent I/O structures. The nominal logic-switching range is 0.65 to 0.85V for 1.5V HSTL, resulting in faster outputs with reduced power-dissipation and signal-integrity issues.
For more details refer to the article below:
http://www.edn.com/article/476349-Exploring_memory_interface_options.php
Show LessIs JTAG feature offered in TQFP packages for Sync/NOBL SRAMs?
Did you know that Cypress products are available for sale in Wafer and Die form? These are typically assembled by vendors with other devices (in similar die form) into a Multi-Chip module (MCM), which helps in reducing board space.
Please contact www.cypress.com/support with your requirements or for more details.
Thanks,
-Anuj
Show Less