SRAM Forum Discussions
text.format{('custom.tabs.no.results')}
Please tell me about θjb or Ψjb of CY7C1041G30-10ZSXI made by Infineon as it was not mentioned in the datasheet.
Hello,
Do you know if there is SEE testing data available for the CY7C185 SRAM?
-Chris
There is no mention of 3V for Rev. R in the English version of this datasheet.
The CY62167GE30-45ZXIT datasheet has a description.
Is it some kind of mistake? Please let me know if there is a reason.
Show Less
Hello,
I'd like the direct technical contact for discussing CY62138FV30LL‐45ZXI. I would like to discuss getting or collecting lot data for the standby current for this part at 25C.
Show Less
The device here lists 1.65 V-2.2 V and 4.5 V-5.5 V, but not 2.2 V-3.6 V. If I want to run the device at 3 V, should I use the 5 V value as a reference?
Show LessIn the config.v file i set the define to FM25CL64B.
When I try to compile the model with ncsim, the compiler tells me that he's expecting a keyword like 'module', 'macromodule' or 'primitive' at line 381. This is where the parameters for the choosen part start.
Since there are only defines and parameters in this file the compiler output doesn't make much sense to me.
Ideas anybody?
Show LessHello
We are looking for top marking:
CY7C1061GE30-10BV1XIT
CY62187G30-55BAXI Please let me know when you will start mass production of this product.
Can you please share BSDL file for part numbers CY14B101LA-SP25XI and CY14B101LA-SZ25XI.
Comparison between the two as seen from the Logic Block Diagrams & Pin configurations as shared here in gives one to understand , there is No difference between CY7C1041GN & CY7C1041G .
NC Pins in both CY7C1041G & CY7C1041GN are Not Connected Internally to the Die.
CY7C1041G is supposed to be a part with ECC, while CY7C1041GN is identified as No ECC as for the PCN . Confusing indeed!!!!
Sharing extract of PCN155107 Last Updated: Oct 31, 2017, Issue Date: December 20, 2015, Effectivity Date: December 20, 2015
4Mb FAST and Micropower (MoBL®) Asynchronous SRAM Products: Technology Transition from 250-, 180-, 130-
and 90-nanometer to 65-nanometer Technology shared for ready reference provides the details of Process migration.
|
|
||||
Item |
Marketing Part Number |
Last Time Buy Date |
Last Time Ship Date |
Replacement Part Number with ECC (65nm) |
Replacement Part Number without ECC (65nm) |
13 |
CY7C1041DV33-10BVXI |
6-Jul-16 |
2-Jan-17 |
CY7C1041G30-10BVXI |
CY7C1041GN30-10BVXI |
14 |
CY7C1041DV33-10BVXIT |
6-Jul-16 |
2-Jan-17 |
CY7C1041G30-10BVXIT |
CY7C1041GN30-10BVXIT |