SRAM Forum Discussions
Hi,
I used CY7C1339G-133AXC in the circuit, but it is obsolete now, do you have a replacement for it , which is Pin to Pin and has the same frequency ?
Thank you.
Show LessHi,
My project requires to interface a DDR II+ SRAM with an Altera Arria10 device acting as a buffer memory. Arria10 datasheet states that it supports QDR SRAM IP only but QDR SRAM is out of my consideration due to my application do not require to write and read at the same time and furthermore I am out of IOs.
Seems like I have to create my own IP. Is anyone successfully doing this?
Thanks.
Regards,
Soo Cheng
Show LessDPRAM POWER DISSIPATION AND THERMAL ANALYSIS DETAILS
LIKE TJ,TC,THETA JC,THETA JA,THETA JB
just want to know the absolute value of dpram junction temperature
help us
I am interfacing QorIQ Processor with SRAM memory (CY62167G18-55ZXI). I am unable to know how to interface BLE#(Byte Low Enable) and BHE#(Byte High Enable) signals present on SRAM to the processor.
CY62167G18-55ZXI |
Dear,
The datasheet of a pipelined SRAM (for example part CY7C1382KV33) states in the "Single Read Accesses" paragraph on page 8, that Consecutive read cycles are supported. One single read cycle has a lantency of 2 Clk cycles.
Does this mean you can do a read cycle every 2 Clk cycles, or can you initiate a read cycle every Clk cycle?
Thanks and best regards,
Toma
Show LessWe are using STK12C68-5C55M @ high temperatures 150 deg C. I need relation between access times and temperature. What is teh max deviation @150 deg C. I could not find Temperature vs access time graph anywhere in cypress website/ datasheet.
Show LessWe are Using CY62157V . we need Configruation setting for LPC4088 Controller.we are using folliwing configruation setting which corruts data in SRAM.:
typedef struct {
uint8_t ChipSelect; /*!< Chip select */
uint32_t Config; /*!< Configuration value */
int32_t WaitWen; /*!< Write Enable Wait */
int32_t WaitOen; /*!< Output Enable Wait */
int32_t WaitRd; /*!< Read Wait */
int32_t WaitPage; /*!< Page Access Wait */
int32_t WaitWr; /*!< Write Wait */
int32_t WaitTurn; /*!< Turn around wait */
} IP_EMC_STATIC_CONFIG_T;
STATIC const IP_EMC_STATIC_CONFIG_T CY62157EV30_config = {
1,
EMC_STATIC_CONFIG_MEM_WIDTH_16 |
EMC_STATIC_CONFIG_CS_POL_ACTIVE_LOW |
EMC_STATIC_CONFIG_BLS_HIGH /* |
EMC_CONFIG_BUFFER_ENABLE*/,
EMC_NANOSECOND(0),
EMC_NANOSECOND(35),
EMC_NANOSECOND(70),
EMC_NANOSECOND(70),
EMC_NANOSECOND(45),
EMC_CLOCK(4)
};
please send perfect Configuation setting.
Show LessGood day, I use 2 CY62126ESL, for the organization of 32-bit mode.
When reading from the memory cells of both chips simultaneously (32-bit mode), when the number of units in the data exceeds 70%, there is an effect of Latch up. There is a current surge up to 12A. Is this a normal mode of operation? How to overcome such a release?
Добрый день, я использую 2 CY62126ESL, для организации 32 -битного режима.
При чтении из ячеек памяти обеих микросхем одновременно (32-битный режим), когда количество единиц в данных превышает 70%, наблюдается эффект Latch up. Наблюдается бросок тока до 12А. Является ли это нормальным режимом работы? Как побороть такой выброс?
Show Less