Announcements

Community going into read-only mode on 25 Sep. Click here for more details

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

SRAM Forum Discussions

Sort by:
MAO
SRAM

Please tell me about θjb or Ψjb of CY7C1041G30-10ZSXI made by Infineon as it was not mentioned in the datasheet.

chris-
SRAM

Hello,

Do you know if there is SEE testing data available for the CY7C185 SRAM?

-Chris

rkm151
SRAM
Hello,   Can this memory be ordered as lot sorted for the standby current?  Can you provide the manufacturing distribution for the standby current? Show More
rkm151
SRAM
Hello,   I'd like the direct technical contact for discussing CY62138FV30LL‐45ZXI.  I would like to discuss getting or collecting lot data for the sta... Show More
MAO
SRAM
The device here lists 1.65 V-2.2 V and 4.5 V-5.5 V, but not 2.2 V-3.6 V. If I want to run the device at 3 V, should I use the 5 V value as a reference... Show More
Anonymous
SRAM
In the config.v file i set the define to FM25CL64B.    When I try to compile the model with ncsim, the compiler tells me that he's expecting a keyword... Show More
maroz1
SRAM

Hello

We are looking for top marking:

CY7C1061GE30-10BV1XIT

 

MAO
SRAM

CY62187G30-55BAXI Please let me know when you will start mass production of this product.

H512369
SRAM

Can you please share BSDL file for part numbers CY14B101LA-SP25XI and CY14B101LA-SZ25XI.

 

bala1943
SRAM
Comparison between the two as seen from the Logic Block Diagrams & Pin configurations as shared here in  gives one to understand , there is No differe... Show More