World's first 64Mbit 3V Asynchronous SRAM

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Cypress packs 64Mbit memory in SRAM chips that are sized 8.0 mm x 9.5 mm. To get a comparable estimate of the size, the 1 dollar coin has a diameter of 26.5mm. That is, the dollar coin covers an area equivalent to 7 such chips. Talk about value for money!

These chips are designed to operate at a cycle time of 12ns. What is the timescale equivalent to? Well, the human heart pumps blood 72 times every minute. In that one minute, the Cypress chip can support 5 billion read / write operations! One can only marvel at such technological prowess.

The chips have been built in 90nm CMOS technology. That is, a single transistor could be as tiny as 90 nm in length. What is the dimensional equivalent?  The human hair is roughly that thick, irrespective of the shampoo / conditioner that we use!. Imagine a switch (or a transistor!) that could be only as wide as a single hair strand!

These chips are guaranteed for high performance and cater to niche markets including storage servers, switches and routers, testing equipment, high-end security systems and military systems

And in what packages do these "dynamites" come in? They are available in RoHS-compliant 48-BGA packages with the smallest footprint.

The I/O configurations supported are both 16-bit and 8-bit, with a power supply of 3V.

A high resolution pic @ http://www.cypress.com/go/pr/3264asyncphoto
The press release covering the launch @ http://www.cypress.com/?rID=43301
The datasheets @ http://www.cypress.com/?rID=49137    

 

0 Likes
1 Reply
Anonymous
Not applicable

wow!

   

64Mbit  SRAM,

   

it must  be a  hard  work
!

0 Likes