- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Is there any recommendation or example for decoupling capacitor on CYF0018V of
Vcc1, Vcc2 and Vccio?
I will apply 25MHz clock into WCLK and RCLK.
Regards,
Koike
Solved! Go to Solution.
- Labels:
-
SYNC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
I've got perfect answer from Tech Support, so I forward this mail for anyone in the future.
Hi Koike-san,
Greetings!
Here are the answers to your questions:
Question: JTAG pins: I'm thinking killing the function of JTAG. How should I take care of JTAG input pins?
Solution: If you are not using the JTAG functionality, then the pins shall have the following:
1. TRST: Connect to GND through a Pull-Down resistance of 1Kohm to ensure the test access port is held in the reset mode.
2. TMS: Connect to GND
3. TDI: Connect to GND
4. TCK: Connect to GND
5. TDO: Can be left Floating
Question: VCC2- connect to 1.5V. Special care has to be taken for this supply to ensue these power pins are as noise free as possible. I understood "Special care has to be taken", but how should I design circuit, exactly? Some example would be appreciated.
Solution: Vcc2(1.5V), capacitor of 10uF bulk close to the voltage supply end and a .01uF de-coupling close to the device pin is to be placed. Since Vref is a biasing voltage generated from the Vcc2, hence there will be negligible current consumption and a decoupling capacitor of 0.1uF is required to be placed close to the device.
Question: Vref - Use 10uF and 0.1uF de-coupling capacitors. Place .1uF de-coupling close to the pin. If common supply used, have a common 10uF and individual 0.1uF decoupling capacitors. I thought resistive divided circuit was good enough but now I'm wondering. Any recommendations for Vref?
Solution: “If common supply used, have a common 10uF and individual 0.1uF decoupling capacitors”, we meant Vref is generated from Vcc2 using the resistive divider network, then 10uF bulk close to the Vcc2 voltage supply end & decoupling capacitor of 0.1uF close to the device for Vcc2 & Vref (since Vref is a biasing voltage generated from the Vcc2, there will be negligible current consumption & a decoupling capacitor of 0.1uF close to the device) to be placed.
Question: Pin U6- DNU -Connect a weak pull down. Pulling down to Vss directly (or open) is not allowed?
Solution: We are sorry. As per the datasheet, this pin should be tied to VSS preferably or can be left floating to ensure normal operation.
Thanks for contacting Cypress Tech Support. Feel free to contact us if you have any further query on this.
Regards,
Asha