Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

SRAM Forum Discussions

Anonymous
Not applicable

Hi all,

I want to know the differences between "CY7C1061G30-10BVJXI" and "CY7C1061G30-10BV1XI" (J or 1) ?

Are all below ordering codes drop in replacement for CY7C1061G30-10BVJXI ?

CY7C1061G30-10BV1XI

CY7C1061GE30-10BV1XI

CY7C1061GE30-10BVJXI

Thank's in advance,

Best Regards

Niklas

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi Niklas,

If a J is present in the MPN then it will be a dual chip select IC. If 1 is present in the MPN it will be a single chip select IC. If 1 and J both are missing then by default it will be a dual chip select IC. If your application does not use the second chip select functionality then you can use it as a replacement as the functionality is the same.

Thanks and Regards,

Pradipta.

View solution in original post

0 Likes
1 Reply
PradiptaB_11
Moderator
Moderator
Moderator
500 replies posted 250 solutions authored 250 replies posted

Hi Niklas,

If a J is present in the MPN then it will be a dual chip select IC. If 1 is present in the MPN it will be a single chip select IC. If 1 and J both are missing then by default it will be a dual chip select IC. If your application does not use the second chip select functionality then you can use it as a replacement as the functionality is the same.

Thanks and Regards,

Pradipta.

0 Likes