Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

himc_284346
Level 3
Level 3
Welcome! 10 replies posted 5 replies posted

Hi

   

I'm using the part CY62157EV30LL-45ZXI in 1Mx8bits mode. I understand that I understand BHE, BLE and I/O8 to I/O14 pins are not used (NC). But I also noticed that ISB2 and ICCDR specifications are valid only when /BHE and /BLE signals are tied to CMOS levels. So while operating in 1Mx8bit mode, will the ISB2 and ICCDR specifications be met?

   

Regards,

   

HiZ

1 Solution
himam_31
Employee
Employee
50 likes received 25 likes received 10 likes received

 When Part is in 1M X8bit mode using BYTE# pin,BHE#, BLE#, IO0 - IO14 can be left floating.

   

ISB2 and ICCDR will be met in this condition for X8 Mode

View solution in original post

0 Likes
1 Reply
himam_31
Employee
Employee
50 likes received 25 likes received 10 likes received

 When Part is in 1M X8bit mode using BYTE# pin,BHE#, BLE#, IO0 - IO14 can be left floating.

   

ISB2 and ICCDR will be met in this condition for X8 Mode

0 Likes