C2HCD Tool is released to help you convert WICED Bluetooth firmware/RAM_patch format from c to hcd.
WICED Studio provides an official script tool to help developers convert WICED Bluetooth firmware/RAM_patch format from hcd to c. The script tool is named hcd2c.pl and is located at <wiced_sdk>\43xxx_Wi-Fi\libraries\drivers\bluetooth\firmware\tools.
However, in some conditions, developers might want to revert the firmware format from c to hcd. C2HCD Tool can help in this case.
Refer to this page for usage and source.
Note: C2HCD Tool is not an Infineon product. Use this tool at your own risk. Report issues to the author only.
Scope and purpose
This document describes the Infineon Wi-Fi onboarding service that allows your device to transfer Wi-Fi credentials over a Bluetooth® LE link. It only describes the custom Bluetooth® LE GATT service and its behavior. The actual implementation is up to the user.
This document is primarily intended for anyone who want to use Infineon Wi-Fi onboarding service to onboard Wi-Fi using Bluetooth® LE.
Infineon provides the industry’s broadest portfolio of Wi-Fi and Wi-Fi + Bluetooth combo devices. Our global Wireless Module Partner Ecosystem enables development of IoT applications with our Wi-Fi and Bluetooth connectivity on time, on budget, and with minimized risk.
Download the PDF below to access our Wi-Fi Bluetooth Partner Modules Selector Guide and explore the different wireless modules available from our partners to enable connectivity in your next IoT design.
AnyCloud libraries help you rapidly develop Wi-Fi and Bluetooth applications using connectivity combo devices, such as CYW4343W, CYW4373 and CYW43012, with the PSoC 6 MCU.
With the ModusToolbox AnyCloud collection of software libraries, you can rapidly develop Wi-Fi and Bluetooth applications on PSoC 6 MCU devices. This document describes all the libraries and versions included with AnyCloud 1.3.
AnyCloud 1.3 adds the 202011.00 version of Amazon’s AWS IoT Device SDK for Embedded C with updated implementations of the HTTP Client and MQTT protocols. The AnyCloud OTA library has also been re-worked to support the new HTTP client as well as and MQTT-based image downloads.
New MQTT Library with Quality-of-Service 2 (QoS 2)The AWS IoT Device SDK for Embedded C includes an update to the MQTT protocol, adding QoS2 support, which guarantees that a message is delivered once and once only.
Enhanced Wi-Fi / Bluetooth Coexistence (Smart CoEx)Coexistence refers to the ability of Infineon combo devices to reliably and efficiently share the wireless bandwidth, enabling simultaneous Wi-Fi and Bluetooth Low Energy connections through a single antenna. Smart CoEx extends that feature with an API to control the combo device behavior at run-time, giving the developer unrivalled control over application performance.
Wi-Fi and Bluetooth LE Manufacturing and Certification TestsThis is a set of applications, provided in source form, that enable manufacturing and certification tests to get your product to market quickly.