Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Using AP(softAP) and STA(client) simultaneously

Using AP(softAP) and STA(client) simultaneously

GregG_16
Employee
Employee
50 sign-ins 25 sign-ins 25 comments on KBA

Using AP(softAP) and STA(client) simultaneously

 

Several people have asked about using the WICED module as a SoftAP (AP) and a Client (STA) at the same time.

In this Blog, we will demonstrate this with the Console test App.

First, compile, download and run the Console Test App:

This can be done with the following "Make Target" test.console-BCM943362WCD4 download run

ap1.JPG

 

Next assure via the Serial port console window that the Console app is running

For more information on this Serial Port Communication to WICED Module

Using AP and STA simul..JPG

Typing 'help'  will scroll a long list of commands.

 

> help

Console Commands:

     help [<command> [<example_num>]]

         - Print help message or command example.

     loop <times> [ <semicolon_separated_commands_list> ]

         - Loops the commands inside [ ] for specified number of times

     antenna <0|1|3>

         - Antenna selection. 3 = Auto

     get_noise

         - Get PHY noise after successful TX

     get_ap_info

         - Get AP information

     get_access_category_parameters_sta

         - Get access category parameters for STA

     get_associated_sta_list

         - Get list of associated clients

     get_counters

         - Get counters

     get_country

         - Get country.

     get_rate

         - Get current rate.

     get_data_rate

         - Get data rate.

     get_mac_addr

         - Get the device MAC address.

     get_pmk <key>

         - Get PMK

     get_random

         - Get a random number.

     get_rssi

         - Get the received signal strength of the AP (client mode only).

     get_soft_ap_credentials

         - Get SoftAP credentials

     get_tx_power

         - Gets the tx power in dBm.

     join <ssid> <open|wep|wpa_aes|wpa_tkip|wpa2|wpa2_tkip> [key] [ip netmask gateway]

         - Join an AP. DHCP assumed if no IP address provided

     join_specific <ssid> <bssid> <channel> <open|wep|wpa_aes|wpa_tkip|wpa2|wpa2_tkip> [key] [ip netmask gateway]

         - Join specified AP. DHCP assumed if no IP address provided

     leave

         - Leave an AP.

     scan

         - Scan all enabled channels and print a list of APs found.

     set_legacy_rate <1|2|5.5|6|9|11|12|18|24|36|48|54>

         - Set legacy (CCK/OFDM) rate on PHY

     set_mcs_rate <MCS Index> <Override MCS only>

         - Set MCS rate on PHY

     disable_11n

         - Disable 11n mode operation

     enable_11n

         - Enable 11n mode operation

     set_data_rate <1|2|5.5|6|9|11|12|18|24|36|48|54>

         - Set data rate.

     set_ip <ip> <netmask> <gateway>

         - Set a static IP.

     set_listen_interval <listen interval> <time unit>

         - Set listen interval in time unit 0 = Beacon Intervals. 1 = DTIM Intervals

     wifi_powersave <mode> [delay]

         - Enable/disable Wi-Fi powersave mode. 0 = disable. 1 = PS Poll. 2 = Wait [delay] ms before entering powersave

     set_tx_power <0-31>

         - Set the tx power in dBm.

     start_ap <ssid> <open|wpa2|wpa2_aes> <key> <channel> <wps>

         - Start AP mode.

     status

         - Print status of the Wi-Fi and network interfaces.

     stop_ap

         - Stop AP mode.

     test_ap <ssid> <open|wpa2|wpa2_aes> <key> <channel> <wps> <iterations>

         - Test AP mode.

     test_join <ssid> <open|wep|wpa_aes|wpa_tkip|wpa2|wpa2_tkip> [key] [ip netmask gateway] <iterations>

         - Test joining an AP. DHCP assumed if no IP address provided

     test_join_specific <ssid> <bssid> <channel> <open|wep|wpa_aes|wpa_tkip|wpa2|wpa2_tkip> [key] [ip netmask gateway] <iterations>

         - Test joining an AP. DHCP assumed if no IP address provided

     test_cred <ssid> <bssid> <channel> <open|wep|wpa_aes|wpa_tkip|wpa2|wpa2_tkip> [key]

         - Test joining an AP

     ping <destination> [-i <interval in ms>] [-n <number>] [-l <length>]

         - Pings the specified IP or Host.

     force_alignment

         - Force aligned memory accesses

     join_wps <pbc|pin> [pin] [<ip> <netmask> <gateway>]

         - Join an AP using WPS

     join_wps_specific [pin] [<ip> <netmask> <gateway>]

         - Join a specific WLAN using WPS PIN mode

     scan_wps

         - Scan for APs supporting WPS

     start_registrar <pbc|pin> [pin]

         - Start the WPS Registrar

     stop_registrar

         - Stop the WPS Registrar

     p2p_connect <pin|pbc> [8 digit PIN]

         - Connect to an existing Group Owner or negotiate to form a group

     p2p_client_test <SSID> <8 digit PIN> [Iterations]

         - Test P2P client connection to existing group owner

     p2p_discovery_disable

         - Disable P2P discovery mode

     p2p_discovery_enable

         - Enable P2P discovery mode

     p2p_discovery_test [iterations]

         - Test enable/disable of P2P discovery mode

     p2p_go_start <p|n> [<ssid_suffix> <key> <operating channel>]

         - Start P2P (p)ersistent or (n)on-persistent group

     p2p_go_stop

         - Stop P2P group owner

     p2p_go_test <p|n> [iterations]

         - Test start/stop of (p)ersistent or (n)on-persistent group

     p2p_go_client_test_mode <enable=1|disable=0> <pin value>

         - Allow test client to join using PIN value

     p2p_leave

         - Disassociate from P2P group owner

     p2p_negotiation_test <8 digit PIN> [Iterations]

         - Test P2P negotiation handshake

     p2p_peer_list

         - Print P2P peer list

     p2p_registrar_start <pin|pbc> [8 digit PIN]

         - Start P2P group owner's WPS registrar

     p2p_registrar_stop

         - Stop P2P group owner's WPS registrar

     p2p_set_go_intent <intent value>

          - Set P2P group owner intent (0..15 where 15 = must be GO)

     p2p_set_go_pbc_mode_support <0|1>

          - Set P2P group owner support for PBC mode (1 = allow, 0 = disallow)

     p2p_set_listen_channel <channel>

         - Set listen channel (1, 6 or 11)

     p2p_set_operating_channel <channel>

         - Set operating channel (1..11)

     iperf

         - Run iperf --help for usage.

     iperf_test

         - iperf_test [iterations] iperf command

     malloc_info

         - Print memory allocation information

     thread_list

         - [ThreadX only] Lists the current running threads

     thread_kill <thread id>

         - [ThreadX only] Kills the specified running thread

     thread_spawn [priority] <cmds>

         - [ThreadX only] Spawns a new thread for the specified command. Optionally run at a specific priority.

     reboot

         - Reboot the device

     mcu_powersave <0|1>

         - Enable/disable MCU powersave

     traffic_stream_ipv4 [-c <destination ip>] [-p <port>] [-u (for udp)] [-l <length>] [-d <duration in seconds>] [-r <rate (pps)>] [-S <type of service>] [-i <interface>]

         - Start a traffic stream.

>

 

 

In this demo we will use the following commands:

 

status

     - Print status of the Wi-Fi and network interfaces.

 

scan

     - Scan all enabled channels and print a list of APs found.

 

start_ap <ssid> <open|wpa2|wpa2_aes> <key> <channel> <wps>

     - Start AP mode.

 

stop_ap

     - Stop AP mode.

 

join <ssid> <open|wep|wpa_aes|wpa_tkip|wpa2|wpa2_tkip> [key] [ip netmask gateway]

    - Join an AP. DHCP assumed if no IP address provided

 

leave

- Leave an AP.

 

 

First let's check the "status"

> status
WICED Version  : 3.1.2
Platform              : BCM943362WCD4
MAC Address     : 44:39:C4:31:14:83

STA Interface     : Down
AP Interface       : Down
P2P Interface     : Down

 

You can see from the output that the STA and AP interfaces are both down.

 

Next we can join an existing network:

 

Type 'scan' to see who is available:

> scan

Waiting for scan results...

  # Type  BSSID                      RSSI  Rate Chan Security    SSID

----------------------------------------------------------------------------------------------

  0 Infra 00:16:01:A1:98:38     -68    144.4     1    Open              Nidal-Out

  1 Infra 00:90:4C:10:E2:20    -57     216.7    1    Open              BSD-Android-Test

  2 Infra B8:BE:BF:15:AF:B2  -38     144.4    1    WPA2 AES    BRCMWiFi

  3 Infra B8:BE:BF:15:AF:B1  -38     144.4    1    WPA2 AES    brcmwpa

  4 Infra 04:A1:51:38:63:AD    -65     216.7   1    WPA2 AES    NETGEAR24-BT

  5 Infra B8:BE:BF:15:AF:B0   -36     54.0     1    WPA2 AES    BRCMGUEST

 

End of scan results

 

Next we will join an AP, in this example "BRCMGUEST"

> join BRCMGUEST wpa2 <passphrase>

Joining : BRCMGUEST

Successfully joined : BRCMGUEST

Obtaining IPv4 address via DHCP

Setting IPv6 link-local address

IPv4 network ready IP: 10.16.101.9

 

Now check the status:

> status
WICED Version  : 3.1.2
Platform              : BCM943362WCD4
MAC Address     : 44:39:C4:31:14:83

STA Interface
   MAC Address : 44:39:C4:31:14:83
   SSID               : BRCMGUEST
   IP Addr           : 10.16.101.9
   Gateway         : 10.16.96.1
   Netmask         : 255.255.248.0
AP Interface      : Down
P2P Interface    : Down

 

You can see we have successfully joined the network and received an IP address via the DHCP server.

 

Next we start an AP:

If you type start_ap you will see the correct syntax:

> start_ap

Usage: start_ap <ssid> <open|wpa2|wpa2_aes> <key> <channel> <wps>

 

Let's start an AP with the SSID 'gangi' with WPA2 security and a passphrase of '12345678' on Channel 1

PLEASE NOTE: The AP and STATION need to be on the same channel!  In this case it is 2.4GHz Channel 1.

> start_ap gangi wpa2 12345678 1
Setting IPv6 link-local address
IPv4 network ready IP: 192.168.0.1

 

Look at the Status again:

> status

WICED Version  : 3.1.2

Platform              : BCM943362WCD4

MAC Address     : 44:39:C4:31:14:83

STA Interface
   MAC Address  : 44:39:C4:31:14:83
   SSID                : BRCMGUEST
   IP Addr            : 10.16.101.9
   Gateway          : 10.16.96.1
   Netmask          : 255.255.248.0
AP Interface
   MAC Address  : 44:39:C4:31:14:83
   SSID                : gangi
   IP Addr            : 192.168.0.1
   Gateway          : 192.168.0.1
   Netmask          : 255.255.255.0
P2P Interface     : Down

 

Now you can see we have a AP interface and a STA Interface simultaneously running.

 

 

You can easily stop the soft AP using 'stop_ap' and leave the AP using the 'leave' command

> stop_ap
> status
WICED Version  : 3.1.2
Platform              : BCM943362WCD4
MAC Address     : 44:39:C4:31:14:83

STA Interface
   MAC Address  : 44:39:C4:31:14:83
   SSID                : BRCMGUEST
   IP Addr            : 10.16.101.9
   Gateway          : 10.16.96.1
   Netmask          : 255.255.248.0
AP Interface      : Down
P2P Interface     : Down

 

 

> leave
> status
WICED Version  : 3.1.2
Platform              : BCM943362WCD4
MAC Address     : 44:39:C4:31:14:83

STA Interface    : Down
AP Interface       : Down
P2P Interface     : Down

 

 

Enjoy. Hope this helps!

 

Please direct questions and comments to:

seyhan and gangi

3094 Views
Comments
Anonymous
Not applicable

very useful, thanks! !!!