Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

TCP stream API

TCP stream API

lock attach
Attachments are accessible only for community members.
PriyaM_16
Moderator
Moderator
Moderator
25 solutions authored 10 solutions authored 5 solutions authored

TCP stream API

WICED provides multiple APIs to implement a TCP connection. This blog discusses the TCP stream_read/write APIs which are more convenient for receiving/sending a large chunk of data.

The usual flow of sending TCP packets is: packet creation-> write data into packet-> set the end of the data portion-> send the packet -> delete the packet.

This method of sending TCP packets turns out to be cumbersome for large chunk of data as one has to go back and forth between packet creation and deletion. The TCP stream APIs provide a better way to stream successive data without worrying about the packet boundaries. The TCP stream APIs takes care of creating the packet and sending it unless the entire buffer is sent. The following diagram gives a simple overview of differences between existing APIs and stream APIs:

pastedImage_7.png

Please refer the wiced_tcpip.h file in 43xxx_Wi-Fi\include dir for description of the provided TCP APIs. Some of the stream APIs are listed below:

wiced_result_t wiced_tcp_stream_init( wiced_tcp_stream_t* tcp_stream, wiced_tcp_socket_t* socket );

wiced_result_t wiced_tcp_stream_write( wiced_tcp_stream_t* tcp_stream, const void* data, uint32_t data_length );

wiced_result_t wiced_tcp_stream_write_resource( wiced_tcp_stream_t* tcp_stream, const resource_hnd_t* res_id );

wiced_result_t wiced_tcp_stream_read( wiced_tcp_stream_t* tcp_stream, void* buffer, uint16_t buffer_length, uint32_t timeout );

wiced_result_t wiced_tcp_stream_read_with_count( wiced_tcp_stream_t* tcp_stream, void* buffer, uint16_t buffer_length, uint32_t timeout, uint32_t* read_count );

wiced_result_t wiced_tcp_stream_flush( wiced_tcp_stream_t* tcp_stream );

Please find attached the tcp_client application modified to use the wiced_tcp_stream_write() API.

Attachments
1415 Views
Contributors