Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Supplicant in Linux

Supplicant in Linux

PrasanthR_06
Employee
First like received First like given Welcome!
Employee

Supplicant in Linux

The objective of this post is to install wpa_supplicant on the ARM target running Linux.

Introduction

wpa_supplicant is a WPA Supplicant for Linux, BSD, Mac OS X, and Windows with support for WPA and WPA2 (IEEE 802.11i / RSN). It is suitable for both desktop/laptop computers and embedded systems. Supplicant is the IEEE 802.1X/WPA component that is used in the client stations. It implements key negotiation with a WPA Authenticator and it controls the roaming and IEEE 802.11 authentication/association of the wlan driver.

wpa_supplicant is designed to be a "daemon" program that runs in the background and acts as the backend component controlling the wireless connection. wpa_supplicant supports separate front-end programs and a text-based front-end (wpa_cli) and a GUI (wpa_gui) are included with wpa_supplicant. wpa_supplicant uses a flexible build configuration that can be used to select which features shall be included and that allows to generate minimal code size binary.

Refer to WPA_Supplicant page for more information on the features supported. Also, refer to the attached developer's document on Supplicant and Hostapd which might be a helpful reference.

Dependencies

The following dependent libraries need to be installed on the target in order to run HostApd.

  • Libnl
  • OpenSSL

The installation steps for Libnl and OpenSSL is same as written for Hostapd. Check this blog to setup the dependencies before proceeding to the following section.

Install wpa_supplicant sources

Host commands

   1. Download the wpa_supplicant open-source package. Extract the file and go to root folder of the package.

$ wget http://hostap.epitest.fi/releases/wpa_supplicant-2.6.tar.gz

$ tar -xzf wpa_supplicant-2.6.tar.gz

$ cd wpa_supplicant-2.6/wpa_supplicant

   2. Copy the existing "defconfig" file to ".config". Edit the .config as shown below.

$ cp defconfig .config

$ vi .config

Now edit .config and make sure to set the following:

CONFIG_DRIVER_NL80211=y

CFLAGS += -I/usr/include/libnl3

CONFIG_LIBNL32=y

   3. Export the "pkgconfig" location.

       $ export PKG_CONFIG_PATH=/usr/arm-linux-gnueabi/lib/pkgconfig

   4. Cross-compile the sources and install the binaries to destination folder.

$ make CC=arm-linux-gnueabi-gcc

$ make install DESTDIR=<target_rootfs>

Start the WPA_Supplicant

  • wpa_supplicant runs as a daemon and requires a configuration file. Create a file called /etc/wpa_supplicant.conf with the following contents:

Secured networkOpen network

ctrl_interface=/var/run/wpa_supplicant

ctrl_interface_group=0

update_config=1

ap_scan=1

network={

ssid="MySSID"

key_mgmt=WPA-PSK

proto=RSN

pairwise=CCMP TKIP

psk="MyPassPhrase"

}

ctrl_interface=/var/run/wpa_supplicant

ctrl_interface_group=0

update_config=1

ap_scan=1

network={

        ssid="MySSID"

        key_mgmt=NONE

}

$ lsmod

Module                  Size  Used by

brcmfmac              209662  0

brcmutil                8504  1 brcmfmac

cfg80211              236740  1 brcmfmac

compat                  2028  2 brcmfmac,cfg80211

  • Start the supplicant to run in background. Basically the below command takes driver(nl80211), interface(wlan0), configuration file(/etc/wpa_supplicant).

$ wpa_supplicant -Dnl80211 -iwlan0 -c/etc/wpa_supplicant.conf -B

Attachments
Comments
Anonymous
Not applicable

Any reason to stick to the 2.2 version of wpa_supplicant, which is from 2014?

PrasanthR_06
Employee
First like received First like given Welcome!
Employee

You can also take the latest version of wpa_supplicant and follow the steps.

PrasanthR_06
Employee
First like received First like given Welcome!
Employee

Updated the blog taking latest version.

Contributors