- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Supplicant in Linux
The objective of this post is to install wpa_supplicant on the ARM target running Linux.
Introduction
wpa_supplicant is a WPA Supplicant for Linux, BSD, Mac OS X, and Windows with support for WPA and WPA2 (IEEE 802.11i / RSN). It is suitable for both desktop/laptop computers and embedded systems. Supplicant is the IEEE 802.1X/WPA component that is used in the client stations. It implements key negotiation with a WPA Authenticator and it controls the roaming and IEEE 802.11 authentication/association of the wlan driver.
wpa_supplicant is designed to be a "daemon" program that runs in the background and acts as the backend component controlling the wireless connection. wpa_supplicant supports separate front-end programs and a text-based front-end (wpa_cli) and a GUI (wpa_gui) are included with wpa_supplicant. wpa_supplicant uses a flexible build configuration that can be used to select which features shall be included and that allows to generate minimal code size binary.
Refer to WPA_Supplicant page for more information on the features supported. Also, refer to the attached developer's document on Supplicant and Hostapd which might be a helpful reference.
Dependencies
The following dependent libraries need to be installed on the target in order to run HostApd.
- Libnl
- OpenSSL
The installation steps for Libnl and OpenSSL is same as written for Hostapd. Check this blog to setup the dependencies before proceeding to the following section.
Install wpa_supplicant sources
Host commands
1. Download the wpa_supplicant open-source package. Extract the file and go to root folder of the package.
$ wget http://hostap.epitest.fi/releases/wpa_supplicant-2.6.tar.gz
$ tar -xzf wpa_supplicant-2.6.tar.gz
$ cd wpa_supplicant-2.6/wpa_supplicant
2. Copy the existing "defconfig" file to ".config". Edit the .config as shown below.
$ cp defconfig .config
$ vi .config
Now edit .config and make sure to set the following:
CONFIG_DRIVER_NL80211=y
CFLAGS += -I/usr/include/libnl3
CONFIG_LIBNL32=y
3. Export the "pkgconfig" location.
$ export PKG_CONFIG_PATH=/usr/arm-linux-gnueabi/lib/pkgconfig
4. Cross-compile the sources and install the binaries to destination folder.
$ make CC=arm-linux-gnueabi-gcc
$ make install DESTDIR=<target_rootfs>
Start the WPA_Supplicant
wpa_supplicant runs as a daemon and requires a configuration file. Create a file called /etc/wpa_supplicant.conf with the following contents:
Secured network | Open network |
---|---|
ctrl_interface=/var/run/wpa_supplicant ctrl_interface_group=0 update_config=1 ap_scan=1 network={ ssid="MySSID" key_mgmt=WPA-PSK proto=RSN pairwise=CCMP TKIP psk="MyPassPhrase" } | ctrl_interface=/var/run/wpa_supplicant ctrl_interface_group=0 update_config=1 ap_scan=1 network={ ssid="MySSID" key_mgmt=NONE } |
- Make sure the following kernel drivers are installed before starting the supplicant. Follow the Getting started on Linux Driver Backporting - FMAC blog to bringup the target with necessary drivers.
$ lsmod
Module Size Used by
brcmfmac 209662 0
brcmutil 8504 1 brcmfmac
cfg80211 236740 1 brcmfmac
compat 2028 2 brcmfmac,cfg80211
- Start the supplicant to run in background. Basically the below command takes driver(nl80211), interface(wlan0), configuration file(/etc/wpa_supplicant).
$ wpa_supplicant -Dnl80211 -iwlan0 -c/etc/wpa_supplicant.conf -B
- Subscribe to RSS Feed
- Mark Article as New
- Mark Article as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Any reason to stick to the 2.2 version of wpa_supplicant, which is from 2014?

- Subscribe to RSS Feed
- Mark Article as New
- Mark Article as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
You can also take the latest version of wpa_supplicant and follow the steps.

- Subscribe to RSS Feed
- Mark Article as New
- Mark Article as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Updated the blog taking latest version.