Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Programming the TAG2/TAG3 Board using command line tools

lock attach
Attachments are accessible only for community members.

Programming the TAG2/TAG3 Board using command line tools

Anonymous
Not applicable

Programming the 20732S MODULE USING 2073xTAG Board v. 1.0

 

Revision Change Decription Date
1.3

TTL-232RG-VREG3V3-WE - defined correct cable with 3V Output

Removed SPIL, Added NEW Loader file and LOTS of corrections

04/03/15
1.4

Corrections to Switch settings, correct Loader zip files for TAG2, TAG3

04/10/15

1.5 Example for command line programming of Serial FLASH 01/18/16
1.6    

 

Section 1: Overview

Introduction

 

This application note describes two recommended procedures of programming the Broadcom  BCM2073xTAG board.

 

Programming the TAG2 (BCM20732 device)

The programming procedure utilizes the Broadcom WICED-Smart-SDK-1.1.0-IDE-Installer that may be downloaded from our Broadcom WICED Community site - WICED-Smart-SDK-1.1.0-IDE-Installer

 

Programming the TAG3 (BCM20737 device)

The programming procedure utilizes the Broadcom WICED-Smart-SDK-2.2.0-IDE-Installer that may be downloaded from our Broadcom WICED Community site - WICED-Smart-SDK-2.2-IDE-Installer (Windows)

 

 

The production environment rarely allows for the compete SDK at the programming station and Broadcom has enabled

programmability utilizing a command line utility loader program that may be downloaded from the attachment below.

 

The following sections describe the BCM2073xTAG programming procedure:

 

Section 1: “Overview,” lists the links for the SDK.


Section 2: “BCM20732TAG Setup: Component/Switch Locations,” contains the setup.


Section 3: “BCM2073xTAG Setup: Component/Switch Locations,” contains the setup.


Section 4: “USB Connection to the PC,” describes the USB enumeration preparation process.


Section 5: “Setup for Command Line Programming.

 

Section 6: "Command Line Programming Procedure using the Loader.exe,” describes the Command Line Tool.


Section 7: “Hex File and BD_ADDR Configurations in Development and Mass Production", describes engineering development of BD_ADDR and Final Configuration for Mass Production.

 

 


Section 2: BCM20732TAG Setup:

Component/Switch Locations BCM20732/BCM2073x TAG Board Configuration

 

Procedure:

1.  BCM20732TAG - Locate the SW2 and SW3 Pins on the Board

 

Figure 1: BCM20732 TAG2 Switches and Buttons

Fig_1_BCM20732TAG Switches and Buttons.png


2.  BCM20732TAG - Place the SW2 and SW3 to the UP Positions as shown:

 

Figure 2: BCM20732 TAG2 SW2 and SW3 Up Positions
Fig_2_BCM20732TAG SW2 and SW3 Up Positions.png


3.  BCM20732TAG - All Dip switches should be in the ON(Up) Position as shown below:

 

Figure 4: BCM20732 TAG2 4 Pin Switch Settings

pastedImage_13.png
4.  BCM2073xTAG - Place the Dip Switch positions 2 and 4 to the OFF(Down) Position as shown:

 

 

 


Section 3: BCM2073xTAG Setup: Component/Switch Locations

BCM2073xTAG Board Configuration

 

Procedure
1.  Locate the SW3 and SW3 Pins on the BCM20737TAG Board


Figure 6: BCM20737TAG Switches and Buttons

 

BCM2073xTAG Switches and Buttons.png


2.  Place the SW2 to UP Position and SW3 to the DOWN Position as shown:

 

Figure 7: BCM20737TAG SW2 Up and SW3 Down Positions

BCM20732TAG SW2 Up and SW3 Down Positions.jpg

3.  Locate the Dip Switch on the TAG Board

 

Figure 8: BCM20737TAG Dip Switch

BCM2073xTAG Dip Switch.png


4.  Place the Dip Switch positions should be in the ON(Up) Position as shown below:

 

Figure 9: BCM2073xTAG3 4 Pin Switch Settings

 

pastedImage_17.png

 

 

 

 

Section 4: USB Enumeration Connection to the PC
USB Enumeration of the BCM2073xTAG Board

 

The BCM2073xTAG board must be enumerated by the Programing PC.  The FTDI chip on the TAG Board will enumerate the device on the Device Manager under the Ports Section as shown below:

 

Figure 10: Sample COM Port before 20732TAG USB Insertion

 

Sample COM Port before 20732TAG USB Insertion.jpg

Procedure
1.  Open up the Device Manager in the Control Panel as shown above.

 

2.  Insert the USB Cable (Connected to the USB Port on the BCM2073xTAG board) to enumerate the Device Driver for the FTDI chip on the Board.


a.  The BCM20732TAG board uses the FTDI TTL-232RG-VREG3V3-WE USB to Serial Cable - you MUST get the 3V output.

 

(http://www.ftdichip.com/Products/Cables/USBTTLSerial.htm)

 

 

Figure 11: Correct FTDI Cable

pastedImage_0.png


b.  This enables the programming of the BCM2073x devices without the need for a JTAG Interface


c.  Note that Serial Wire Debug (SWD) debug/trace messages can also be output through the HCI UART port that’s onboard.


d.  The SWD pins are muxed with HCI UART and are used in such a manner that the hardware and firmware can auto-detect the presence of SWD or the HCI host


e.  This means that HCI based download (programming) and SWD (debugging) are mutually exclusive of one another.


3.  In order to use the onboard UART header and a TTL-232RG-VREG3V3-WE USB to Serial cable to program your custom board, you would need to do the following:

a.  With the BCM20732S board powered down, connect the TTL-232RG-VREG3V3-WE USB to Serial Cable to your PC (USB) then to the UART header on your board: RXD, TXD, VBAT and GND respectively.

b. Power your board up while making sure that RXD is held high during power up. Note that by default this pin is pulled low through an internal 10k ohm resistor

c. Program the board using the Broadcom IDE just as you would if a BCM20732S Tag board were connected.


4.  As an example, the BCM2073xTAG board has been enumerated as COM16 as shown below:


Figure 12: Sample COM AFTER 2073xTAG USB Insertion – COM16 Enumerated

 

Sample COM AFTER 2073xTAG USB Insertion – COM16 Enumerated.jpg


If you’re not familiar with the installation of the drivers for your TAG board, refer to the WICED Smart™ Quick Start Guide found in the ~Docs folder of the SDK.

 

Section 5: Programming

 

 

Section 5.1: Software Programming Setup

 

Broadcom BCM20732x devices are be programmed using either the SDK Developer’s Tools or by using a command line tool called loader.exe.

 

The Loader directory of files to download can be found as an attachment at the bottom of this BLOG.

 

The SDK combined with the BCM2073xTAG Board provide the developer a convenient methodology for programming the BCM2073x or BCM2073xS Modules discussed below or for the developer’s Pre-Production Board.

 

To prepare the Production Board for Mass Production programming, the Loader command line tools provide a convenient process to automate the programming at a contract manufacturing facility or at a distribution programming center.

 

You will also need the ChipLoad.exe file attached at the bottom of this BLOG.

 

Section 5.2 System Programming Tools Setup:

 

The programming ecosystem of the BCM2073x/BCM2073xS devices involves the use of executable files both compile and produce necessary files for use in programming the modules.

 

The first file needed is the cgs.exe file to enable the board address (BD_ADDR) programming at the time of production.

 

The cgs.exe file is included in the SDK Directory (WICED\WICED-Smart-SDK-x.x.x\WICED-Smart-SDK\Tools\CGS\Win32) as shown below but can also be extracted from the loader.zip file located on the WICED SMART Community Forums download page located at the bottom of this BLOG.

 

Figure 13: Location of cgs.exe

 

Location of cgs exe.png

The second file needed is the chipload.exe file to download the programming file to the programmer at the time of production.

 

The Chipload.exe file is included in the SDK Directory (WICED\WICED-Smart-SDK-x.x.x\WICED-Smart-SDK\Tools\ChipLoad\Win32) as shown below but can also be extracted from the loader.zip file located on the WICED SMART Community Forums download page located at the bottom of this BLOG.

 

Figure 14: Location of ChipLoad.exe

Location of ChipLoad exe.png


The cgs file can also be edited in the SDK Build window as shown below:


The third file needing editing for programming is the EEPROM file BCM2073xAx.cgs file.  The cgs file is located in the SDK Directory (WICED\WICED-Smart-SDK-x.x.x/build/hello_sensor-BCM*_Q32-rom-ram-Wiced-release/A_*-hello_sensor-rom-ram-spar.cgs as shown below.

 

This is the file uses to program the EEPROM with the customer application.


Figure 15: Location of 20737_EEPROM.cgs file

pastedImage_0.png

 


The fourth file needing editing for programming is the EEPROM file 2073x_EEPROM.btp file.

 

The btp file is located in the SDK Directory (WICED\WICED-Smart-SDK-x.x.x\WICED-Smart-SDK\Platforms\BCM2073xTAG_Q32) as shown below.

 

This is the file uses to program the EEPROM with the customer application.

 

Figure 16: Location of 2073x_EEPROM.btp file

Location of 2073x_EEPROM btp file.png

 

Section 6: Command Line Programming Procedure using the Loader.exe

Using the Loader Software Command Line Tools

 

The Loader Software tool utilizes a Command Line Tool to call the appropriate programming files to program the same BD_ADDR programming as the SDK Tool Chain, but in used in the volume programming environment.

 

Programming Procedure using Cygwin utility

 

The Cygwin Utility can be found at: http://www.cygwin.com/install.html  is used to execute the Loader commands and accesses the appropriate configuration files used in the programming procedure.

NOTE: Cygwin is a 32GB file that takes time to download and install

 

Below is an example of using Cygwin to execute the Loader command line utilities.


Please observe the highlighted files described previously:


Figure 17: Contents of Loader.zip file at bottom of BLOG

 

pastedImage_22.png

Figure 18: Cygwin BCM2073x File Location

 

pastedImage_43.png

 

 

NOTE: You need to move the files highlighted above into the cygwin\home\<your name>\ directory under Cygwin.

 


Section 6.1 Converting cgs file to hex file

 

The following procedure converts the cgs file to a hex file:


1.  Using Cygwin Tools installed above, type the following command:


a.  ./cgs.exe -I <output_file_name.hex> –A 0xFF000000 –B <btp_file.btp> -D <file.hdf>

Note: -D refers to a different directory


b.  Example below:

./cgs.exe –I output.hex –A 0xFF000000 –B 20732_TAG32_EEPROM.btp –D . A_20732A0-bleprox_mod-rom-ram-spar.cgs


3.  Definitions of parameters:


a.  output_file_name.hex – will be the converted hex file.
b.  btp_file.btp – btp file for the 2073x_TAG board.
c.  input_file.cgs – built cgs file for the application from  the SDK
d.  0xFF000000 – base address for the EEPROM
e.  File.hdf - directories for hdf file

 

Results of the successful command execution:


Figure 19: Converting cgs file to hex file success

Converting cgs file to hex file success.jpg

Section 6.2 Downloading the hex file

The following procedure downloads the hex file:


1.  Run chipload.exe using the following command:


a.  ./Chipload.exe –BLUETOOLMODE –PORT COM16 –BAUDRATE 115200nfc –MINIDRIVER <minidriver.hex> -CONFIG <output_file_name.hex> -BTP <btp_file.btp> -NODLMINIDRIVER
b.  Example Below:

./chipload.exe –BLUETOOLMODE –BAUDRATE 115200nfc –PORT COM16 –MINIDRIVER uart_64bytes_DISABLE_EEPROM_WP_PIN1.hex –CONFIG output.hex –NODLMINIDRIVER –BTP 20732_TAG32_EEPROM.btp


3.  Definitions of parameters:


a.  COM16 – connected port as connected thru enumeration
b.  btp_file.btp – btp file for the TAG Board
c.  Output_file_name.hex – converted hex file.
d.  btp_file.btp – btp file for the TAG

e.  minidriver - Loads the Hex file into EEPROM or SFLASH image.

     - The MiniDriver uses P1 as the Write Protect Pin

     - If you use a different pin for Write Protect, then the MiniDriver will NOT work.

     - MiniDriver is specific to the P1 Write Protect Pin because it is driven LOW before Writing begins.

 

f.   Chipload.exe - Runs the MiniDriver and does the CheckSum

     - Chipload loads the image and does the CRC

     - If it returns "0", it PASSES

     - If it returns "1", it will PRINT the errors that were encountered

Results of the successful command execution:

 

Figure 20: Hex File Command Success

 

 

Hex File Command Success.jpg

Results of the successful hex file download execution:


Figure 21: Download is completed successfully

pastedImage_6.png

 

Notes:

The key to programming procedure is to know the state of the device:

1.  If device has never been programmed OR device is in recovery mode:
    - Add –NODLMINIDRIVER to chipload.exe

2.  If device has been successfully programmed before AND it is not in recovery mode:
    - Do *not* add –NODLMINIDRIVER to chipload.exe

3.  If in doubt, always use recovery mode.

 

The following example shows the command line for programming Serial FLASH:

 

jtate@LTSDO-JTATE /cygdrive/c/cygwin/home/jtate

$ ./chipload.exe -BLUETOOLMODE -PORT COM100 -BAUDRATE 115200nfc -MINIDRIVER uart_64bytes_DISABLE_EEPROM_WP_PIN1.hex -CONFIG output.hex -BTP 20737_SFLASH.btp

Download minidriver successfully had written 251 bytes to address 0x0020AF00

Download minidriver successfully had written 251 bytes to address 0x0020AFFB

Download minidriver successfully had written 251 bytes to address 0x0020B0F6

Download minidriver successfully had written 251 bytes to address 0x0020B1F1

Download minidriver successfully had written 251 bytes to address 0x0020B2EC

Download minidriver successfully had written 251 bytes to address 0x0020B3E7

Download minidriver successfully had written 251 bytes to address 0x0020B4E2

Download minidriver successfully had written 251 bytes to address 0x0020B5DD

Download minidriver successfully had written 251 bytes to address 0x0020B6D8

Download minidriver successfully had written 251 bytes to address 0x0020B7D3

Download minidriver successfully had written 251 bytes to address 0x0020B8CE

Download minidriver successfully had written 251 bytes to address 0x0020B9C9

Download minidriver successfully had written 251 bytes to address 0x0020BAC4

Download minidriver successfully had written 251 bytes to address 0x0020BBBF

Download minidriver successfully had written 251 bytes to address 0x0020BCBA

Download minidriver successfully had written 251 bytes to address 0x0020BDB5

........

Download config successfully had verified 167 bytes at address 0xFF004B58:  78 25 30 38 58 2C 20 55 47 20 6C 65 6E 67 74 68 3A 20 30 78 25 30 38 58 00 0D 75 70 67 72 61 64 65 20 63 6F 6D 70 6C 65 74 65 2C 20 70 65 72 66 6F 72 6D 20 72 65 73 65 74 00 49 6E 76 61 6C 69 64 61 74 65 64 20 4F 6C 64 20 53 53 2E 00 0A 4C 00 BC 9E 20 00 0A 48 0B 49 08 B5 88 42 02 D0 0A 4A 35 F6 4C FE 00 22 09 49 09 48 35 F6 8D FE 09 4A 09 4B 22 F0 0F 02 1A 60 BD E8 08 40 FE F7 B4 BB 60 9A 20 00 60 9A 20 00 00 00 00 00 5C 04 00 00 60 9A 20 00 DC 9E 20 00 50 0F 20 00 0B 04 00 BD 9E 20 00 FE 00 00
Chip reset to address 0x00000000 succeeded
Downloaded 0 code bytes ( 0.0%) and 18279 data bytes (100.0%). Verified 0 code bytes ( 0.0%) and 18279 data bytes (100.0%).   Current state: Completed successfully

A total of 2 contiguous memory areas were filled:
[FF000000..FF000027] DATA (40 bytes)
[FF0004C0..FF004BFE] DATA (18239 bytes)

 

Section 6.3 Hex File and BD_ADDR and Descriptions in Development

 

 

The WICED SMART SDK build process allows the programming of the BD_ADDR.

Below are the following steps:

 

1.  The SDK is able to program some of the BD_ADDR bytes with random values or

2.  The user can edit Platforms/BCM920736ATAG_Q32/20732_EEPROM.btp file and set DLConfigBD_ADDRBase to the desired value.

3.  To use random address set DLConfigBD_ADDRBase = "20736A0*****" where every “*” will be replaced with a random value.

 

Section 6.4 SDK 2.0 HDF File Changes

 

The WICED SMART SDK 2.2 .hdf file is now in binary form.

 

 

Figure 22: Binary Form of .hdf file

Binary_hdf.PNG

 

 

Section 7 Hex File and BD_ADDR Configurations in Development and Mass Production

 

BCM2073x Design: Using the BCM20736 in SDK 2.2 from the Platforms Directory

 

Figure 23: Binary Form of .hdf file

Arvind_Platform_Specific_Support_Files.png

 

Ex: DLConfigBD_ADDRBase = “20736A1*****”

 

1.  Previously in SDK 1.1 this was the same Random Address on all computers.
2.  Now, in SDK 2.2 it is random per computer that you use.
3.  If you have 2 computers, it will generate 2 different Random addresses.
4.  Everyone in your development team downloads on different computers, everyone will get different addresses.
5.  However, in Development, the same bluetooth address when you reload the application.
6.  Programing multiple boards on the same computer you will get the same address.
7.  In the BUILD target say Device BD_ADDR = BD_ADDR or
8.  Device BD_ADDR = Random and Make will generate a random number.
9.  Each “*” is a random nibble – so you can place the “*” in the middle and have *1234.
10. Example:

      a. Programming 4 devices on the same PC.

11.  BD_ADDR goes into a file that the application does not have access.
12.  It is loaded into a completely different sector
13.  We can include it in one of the build targets to show users the option is there.

 

 

Figure 24: BT_DEVICE_ADDRESS in the Makefile

ARvind_MakeFile_BT_DEVICE_ADDRESS.png


14.  You want your board to have a specific BD_ADDR:

           a.  You can modify the Make Target:

           b.  For instance in i2c_temperature_sensor-BCM920736TAG_Q32 download:

 

Figure 25: _i2c_temperature_sensor selected

Arvind_Specific_Board_Address.png

 

           c.  You can assign 6 bytes in Hex to the Target Name:

 

Figure 26: 6 Bytes assigned to Target Name

Arvind_6_Bytes_In_Target_Name.png

 

           e.  Here we did BT_DEVICE_ADDRESS=20736A112345

           f.  This is in the Quick Start Guide on the Make Target

           g.  Or you can put BT_DEVICE_ADDRESS=random

           h.  This will be random every time we do a build.

           i.  So this may be a good option for the user INSTEAD of the cgs.exe

           j.  The *.btp file parameters that you can change:

               - ConfigDSLocation – Dynamic Section – This is where the code and the Config is stored
               - DLConfigVSLocation =  is where your Link Keys are stored
               - We need 1K for at least 5 devices paired at the same time – Takes up 600 bytes.  And this is all in EPROM Layout

 

Section 7.1 Hex File and BD_ADDR and Descriptions in Production

 

1. The WICED SMART SDK build process produces 2 hex files.

2. What is downloaded in the factory during mass production is the factory <app_name>-<platform>-rom-ram-Wiced-release.hex

3. This is the factory image and includes the BD_ADDR.

4. The SDK and will program some of the BD_ADDR bytes with random values or

5. The user can edit Platforms/BCM920732ATAG_Q32/20732_EEPROM.btp file and set DLConfigBD_ADDRBase to the desired value.

6. To use random address set DLConfigBD_ADDRBase = "20732A0*****" where every “*” will be replaced with a random value.

 

NOTES:

1.  ChipLoad.exe loads the hex file into EEPROM or SFLASH depending on your configuration.

2.  Once you generate the .hex file, you know were the BD_ADDR is going to be: Byte 21 offset

3.  Jump to 21 Byte location and then generate the next 6 Bytes for the BD_ADDR and then you are done!

 


Please feel free to add comments and questions and I will update appropriately.

 

Thank you,

 

JT

Attachments
6038 Views
Comments
Anonymous
Not applicable

Hi,

So I wrote my firmware using sdk 2.0.1

Should I buy BCM20732S or BCM20736S because in other posts people said I can't use sdk2 for 732S designs. But here it looks like I can.

Anonymous
Not applicable

If you wrote your firmware using SDK 2.0.1, it's only programmed into 20736S or 20737S module.

For 20732S module, you should use SDK 1.1.0.

Anonymous
Not applicable
As a follow up, where can I buy bcm20736s because Avnet didn't list them.
MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

Couple of things.

1.

Source code generated for the BCM20732S should work fine on the BCM20736/37S once compiled under the SDK 2.X environment. Precompiled firmware cannot be exchanged between the two as previously noted.

2.

I checked and Avnet has stock on the 20736S: bcm20736S Wireless and GPS Modules RF Modules Misc Parts - Avnet Express

In addition, both Macnica Americas (Macnica) and TecStar (their parent company) in Japan should hold stock as well: TecStar

PhGi_2174146
Level 3
Level 3
First like received First like given

My development kit did not come with a wiring harness.  Any idea where I can get one that fits, or does anyone at least have the manufacturer & model # for the connector so I can order some sockets?

VikramR_26
Employee
Employee
25 sign-ins 10 sign-ins 10 comments on KBA

Manufacturer & model # for the connector

Contact: Maureen Supple

M Supple <msupple@devainc.com>

ph # 714-368-1717

Part Number # 4 pos cable assy

Its a double ended and you can have it cut to have two cables.



Anonymous
Not applicable

hi JT,

I have successfully downloaded the FW to 20736 board using chipload .

and i want to use chipload.exe to download the 20738 FW, is it possible ?

how can I remove the verify process ,only write .because the 20738 do not support verify when download FW by bluetool .when i use chipload.exe download the FW to 20738 chip ,it failed on the verify step .1.png

MichaelF_56
Moderator
Moderator
Moderator
250 sign-ins 25 comments on blog 10 comments on blog

The BCM20738 (Keyboard and Mouse specific device) and Bluetool (internal Broadcom test tool) are not supported here within the Community. Please ask the people at Broadcom that enabled these for you to define the correct support path, which is most likely our internal CSP system.

nsankar boont