- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
PSoC 6 MCU with FreeRTOS!
FreeRTOS is a class of RTOS that is designed to be small enough to run on a microcontroller - although its use is not limited to microcontroller applications. It provides the core real time scheduling functionality, inter-task communication, timing and synchronization primitives only. This means it is more accurately described as a real time kernel, or real time executive. Additional functionality, such as a command console interface, or networking stacks, can then be included with add-on components.
Cypress’ PSoC 6 MCUs is supporting FreeRTOS and designers can develop PSoC 6 MCU systems for IoT applications.
See it in a PSoC 6 project here, FreeRTOS for PSoC 6 MCUs.
Also, check out code examples and articles based on FreeRTOS.
Lastly, if you have any feedback, comments, or questions, feel free to leave them here, we appreciate the discussions!
-
Anonymous