cancel
Showing results for 
Search instead for 
Did you mean: 

Resource Library

PSOC 4 Flash Em_EEPROM stuck issue when Reading & Writing and solution

GuoXiangH_21
Employee

PSOC 4 Flash Em_EEPROM stuck issue when Reading & Writing and solution

Symptoms

           

GuoXiangH_21_0-1628588489364.pngGuoXiangH_21_1-1628588489367.png

 

Diagnosis

          Customer use PSOC 4 CY8C4147AZI-S455 to design Remote controller, implement Segment LCD+ Capsense+ System control function, use Flash Em_EEPROM (version: V2.2) component to store system parameter, and the remote controller was used in hotel room, and when room ID card insert in power supply booth ,the AC power on ,and indoor aircon & remote controller start work, when remove the ID card ,the ac power down, indoor aircon & remote controller stop work

                       They feedback the remote controller can’t start up and no display after several working months.

                       We read the bad remote controller, and found the code section are the same, and EEPROM data are different from each other           

 

GuoXiangH_21_2-1628588542637.png

 

 

        We re-program the bad remote controller, and it can run well again

Solution

 

                   We checked KBA227502 & KBA227530, and modified cy_em_eeprom.c the following code

 

Cy_Em_EEPROM_Read() 

 

    if((CY_EM_EEPROM_SUCCESS == ret) && (0u != seqNum))

    {

       numRowReads = (context->numberOfRows <= seqNum) ? (context->numberOfRows) : (seqNum);

       numRowReads--;

                for(i = (seqNum - numRowReads); i <= seqNum; i++)

       {

          startRowAddr = GetRowAddrBySeqNum(i, context);

                       if (0u != startRowAddr)

          {

    ...

 

         

       if((CY_EM_EEPROM_SUCCESS == ret) && (0u != seqNum))

   {

       numRowReads = (context->numberOfRows <= seqNum) ? (context->numberOfRows) : (seqNum);

                for(i = 0; i < numRowReads; i++)

       {

         startRowAddr = GetRowAddrBySeqNum(seqNum - ((numRowReads - 1) - i), context);

                    if (0u != startRowAddr)

         {

           ...

 

 

CheckCrcAndCopy() 

 

if(CY_EM_EEPROM_SUCCESS == ret)

{

   (void)memcpy((void *)(dstAddr), (void *)(writeRamBuffer + rowOffset), numBytes);

}

 

 

if(CY_EM_EEPROM_SUCCESS == ret)

{

    (void)memcpy((void *)(dstAddr), (void *)((uint32_t)writeRamBuffer + rowOffset), numBytes);

}

 

 

Cy_Em_EEPROM_Write()

/* Write the data to the specified flash row */

ret = WriteRow(emEepromRowAddr, writeRamBuffer, context);

tmpRowAddr = emEepromRowAddr;

 

/* Calculate the checksum of a data header if redundant copy is disabled */

if(0u == context->redundantCopy)

{

writeRamBuffer[CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET_U32] = (uint32_t) CalcChecksum((uint8_t *) &writeRamBuffer[0], CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET);

}

/* Write the data to the specified flash row */

ret = WriteRow(emEepromRowAddr, writeRamBuffer, context);

tmpRowAddr = emEepromRowAddr;

 

 

 

 

Cy_Em_EEPROM_Erase()

if(0u != context->redundantCopy)

{

writeRamBuffer[CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET_U32] = (uint32_t)

CalcChecksum((uint8_t *) &writeRamBuffer[CY_EM_EEPROM_EEPROM_DATA_OFFSET_U32],

CY_EM_EEPROM_EEPROM_DATA_LEN);

}

 

if(0u != context->redundantCopy)

{

writeRamBuffer[CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET_U32] = (uint32_t)

CalcChecksum((uint8_t *) &writeRamBuffer[CY_EM_EEPROM_EEPROM_DATA_OFFSET_U32],

CY_EM_EEPROM_EEPROM_DATA_LEN);

}

else

{ /* Calculate the checksum of a data header if redundant copy is disabled */

writeRamBuffer[CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET_U32] = (uint32_t)

CalcChecksum((uint8_t *) &writeRamBuffer[0],

CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET);

}

 

 

 

FindLastWrittenRow()

/* Some record in EEPROM was found. Store found sequence

* number and row address.

*/

prevSeqNum = seqNum;

*lastWrRowPtr = emEepromAddr;

 

if((*(uint32_t *)(emEepromAddr + CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET)) ==((uint32_t) CalcChecksum((uint8_t *)emEepromAddr, CY_EM_EEPROM_HEADER_CHECKSUM_OFFSET)))

{

/* Some record in EEPROM was found. Store found sequence number and row address. */

 

prevSeqNum = seqNum;

*lastWrRowPtr = emEepromAddr;

}

 

 

 

But we still found Cy_Em_EEPROM_Write()  following issue

 

for(; i <= seqNum; i++)

{

    ……

}

 

When  seqNum=0xFFFFFFFF ,the for loop will loop forever ,and no chance jump out

 

So we need to add some special deal before it

 

if(seqNum >= (0xFFFFFFF0))

{

    seqNum=1;

}

 

Cy_Em_EEPROM_Write()

        for(wrCnt = 0u; wrCnt < numWrites; wrCnt++)

        {

            uint32 skipOperation = 0u;

            /* Get the sequence number of the last written row */

            uint32 seqNum = CY_EM_EEPROM_GET_SEQ_NUM(emEepromRowAddr);

           

 

            /* Get the address of the row to be written. The "emEepromRowAddr" may be

            * updated with the proper address (if wear leveling is used). The

            * "emEepromRowRdAddr" will point to the row address from which the historic

            * data will be read into the RAM buffer.

            */

            GetNextRowToWrite(seqNum, &emEepromRowAddr, &emEepromRowRdAddr, context);

        for(wrCnt = 0u; wrCnt < numWrites; wrCnt++)

        {

            uint32 skipOperation = 0u;

            /* Get the sequence number of the last written row */

            uint32 seqNum = CY_EM_EEPROM_GET_SEQ_NUM(emEepromRowAddr);

           

            if(seqNum >= (0xFFFFFFF0))

            {

                  seqNum=1;

            }

 

            /* Get the address of the row to be written. The "emEepromRowAddr" may be

            * updated with the proper address (if wear leveling is used). The

            * "emEepromRowRdAddr" will point to the row address from which the historic

            * data will be read into the RAM buffer.

            */

            GetNextRowToWrite(seqNum, &emEepromRowAddr, &emEepromRowRdAddr, context);

 

 

We have modified cy_em_eeprom.c ,and download the attached file

Please update it as the following path:

 

C:\Program Files (x86)\Cypress\PSoC Creator\4.X\PSoC Creator\psoc\content\CyComponentLibrary\CyComponentLibrary.cylib\Em_EEPROM_Dynamic_v2_X\API

GuoXiangH_21_3-1628588602243.png

 

 

 

 

 

0 Likes
Version history
Revision #:
2 of 2
Last update:
‎Aug 19, 2021 07:06 PM
Updated by: