Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Interfacing STM32Fx-Discovery with WICED using JTAG Debugger

Interfacing STM32Fx-Discovery with WICED using JTAG Debugger

SeyhanA_31
Employee
100 likes received 50 likes received 25 likes received
Employee

Interfacing STM32Fx-Discovery with WICED using JTAG Debugger

WICED SDK could be connected to the STM32Fx-Discovery board (in this case STM32F4-Discovery board is used) with JTAG debugger.

Connect the JTAG debugger to the STM32F4-Discovery board using the following connections.

ScreenHunter_105 Jan. 02 22.49.jpg

To build an application and run it on the target STM32F4-Discovery board add the following to the Make Target built command:

     For Olimex:     JTAG=Olimex_ARM-USB-TINY-H

     For Segger:     JTAG=jlink

     <WicedApplication>-<YourPlatform> JTAG=Olimex_ARM-USB-TINY-H download run

For sample interface of interfacing SN8000 WiFi module to the STM32F4-Discovery board please check out this link SN8000 WiFi Module with STM Discovery Board.

0 Likes
Contributors