cancel
Showing results for 
Search instead for 
Did you mean: 

Resource Library

I2C Infrared Contactless Temperature Sensor Interface

SeyhanA_31
Employee

I2C Infrared Contactless Temperature Sensor Interface

This snippet application interfaces the Infrared contact-less temperature sensor (TMP007) module from Adafruit (https://www.adafruit.com/products/2023) using WICED SDK.

- The snippet application sets up the I2C device interface and probes the device.

- Then all register values are read and pushed to the serial terminal interface.

- To show writing to the I2C device, object high temperature alarm register is updated with a given value then the same register is register back.

- Every 1 second period, I2C device die and object temperature values are read from corresponding registers and printed on the serial terminal.

For BCM943362WCD4 evaluation platform update the platform.c and platform.h files for I2C device.

Update the .../platforms/BCM943362WCD4/platform.c file by adding the following changes to the file:

const platform_i2c_t platform_i2c_peripherals[] =

{

    [WICED_I2C_1] =

    {

        .port                    = I2C1,

        .pin_scl                 = &platform_gpio_pins[WICED_GPIO_11],

        .pin_sda                 = &platform_gpio_pins[WICED_GPIO_12],

        .peripheral_clock_reg    = RCC_APB1Periph_I2C1,

        .tx_dma                  = DMA1,

        .tx_dma_peripheral_clock = RCC_AHB1Periph_DMA1,

        .tx_dma_stream           = DMA1_Stream7,

        .rx_dma_stream           = DMA1_Stream0,

        .tx_dma_stream_id        = 7,

        .rx_dma_stream_id        = 0,

        .tx_dma_channel          = DMA_Channel_1,

        .rx_dma_channel          = DMA_Channel_1,

        .gpio_af                 = GPIO_AF_I2C1

    }

};

For platforms/BCM943362WCD4/platform.h file add the WICED_I2C_1 to the wiced_i2c_t as below:

typedef enum

{

    WICED_I2C_1,

    WICED_I2C_MAX,

    WICED_I2C_32BIT = 0x7FFFFFFF,

} wiced_i2c_t;

The platform files for BCM943362WCD4 are attached.

NOTE: On BCM943362WCD4 evaluation board, two 4.7K pull up resistors are needs on each of the SCL and SDA connections.

For BCM943341WCD1, the I2C device of WICED_I2C_1 is already defined in the platform files. Since the SCL and SDA pull resistors are already populated on the BCM943341WCD1 evaluation board, no hardware related modifications are needed.

Your application specific platform files can be updated as above to interface the chosen I2C device to the WICED SDK 3.x platforms.

1. To run the test, connect the I2C device to the evaluation board as following:

Connection setup for I2C device to STM32F4xx based WICED evaluation board

I2C-Device   BCM943341WCD1 J7 Header

      -                    J7-27

     +                    J7-28

     SDA               J7-26

     SCL               J7-25

Connection setup for I2C device to STM32F2xx based WICED evaluation board

I2C-Device   BCM943362WCD4 J7 Header

     -                         J7-2

     +                        J7-1

     SDA                   J7-7

     SCL                   J7-6

2. Unzip and copy the attached files to the WICED SDK-3.x version.

For I2C Temp application snippet:

     Copy the content of the i2c_temp.7z source to .../apps/snip/i2c_temp

For BCM943362WCD4:

     Copy the content of the BCM943362WCD4.7z source to .../platforms/BCM943362WCD4

For BCM943341WCD1:

     Default platform files could be used.

3. To build, download and run the application below

For STM32F4xx MCU BCM943341WCD1:

     snip.i2c_temp-BCM943341WCD1 download run

For STM32F2xx MCU BCM943362WCD4:

     snip.i2c_temp-BCM943362WCD4 download run

Picture of setup:

IMG_0966.JPG

Serial terminal log:

13:15:39.028: Starting WICED v3.3.DEVELOPMENT

13:15:39.028: Platform BCM943341WCD1 initialised

13:15:39.028: Started ThreadX v5.6

13:15:39.028: Initialising NetX_Duo v5.7_sp2

13:15:39.028: Creating Packet pools

13:15:39.028: WWD SDIO interface initialised

13:15:39.348: WLAN MAC Address : 6C:AD:F8:F0:E8:F1

13:15:39.364: WLAN Firmware    : wl0: Nov 25 2015 14:01:39 version 6.49.2 (r602357) FWID 01-1302682f

13:15:39.364: I2C LED Interface Application.

13:15:39.396: Probe successful on address 64!

13:15:39.396: Manufacturer ID: 0x5449

13:15:39.396: Device ID: 0x0078

13:15:39.396: Voltage: -27.6562 uV

13:15:39.396: Die Temp: 25.22C

13:15:39.396: Object Temp: 25.12C

13:15:39.412: Alarms(L/H): Die -256.00C / 255.50C, Object -256.00C / 198.50C

13:15:39.412: Write: 6340 Read: 6340

13:15:39.412: Write: 198.50C Read: 198.50C

13:15:39.412: Die Temp: 25.22C (78.39F) - Object Temp: 25.12C (77.22F)

13:15:39.428: Die Temp: 25.19C (78.34F) - Object Temp: 25.19C (77.34F)

13:15:40.420: Die Temp: 25.19C (78.34F) - Object Temp: 25.34C (77.62F)

13:15:41.428: Die Temp: 25.19C (78.34F) - Object Temp: 26.38C (79.47F)

13:15:42.436: Die Temp: 25.19C (78.34F) - Object Temp: 28.12C (82.62F)

13:15:43.444: Die Temp: 25.19C (78.34F) - Object Temp: 30.03C (86.06F)

13:15:44.451: Die Temp: 25.22C (78.39F) - Object Temp: 32.50C (90.50F)

13:15:45.459: Die Temp: 25.22C (78.39F) - Object Temp: 34.25C (93.65F)

13:15:46.451: Die Temp: 25.22C (78.39F) - Object Temp: 33.12C (91.62F)

13:15:47.460: Die Temp: 25.22C (78.39F) - Object Temp: 32.47C (90.44F)

13:15:48.468: Die Temp: 25.22C (78.39F) - Object Temp: 33.06C (91.51F)

13:15:49.476: Die Temp: 25.22C (78.39F) - Object Temp: 33.91C (93.03F)

13:15:50.484: Die Temp: 25.22C (78.39F) - Object Temp: 34.59C (94.27F)

13:15:51.476: Die Temp: 25.22C (78.39F) - Object Temp: 34.97C (94.94F)

13:15:52.484: Die Temp: 25.25C (78.45F) - Object Temp: 35.38C (95.68F)

13:15:53.492: Die Temp: 25.25C (78.45F) - Object Temp: 35.06C (95.11F)

13:15:54.500: Die Temp: 25.25C (78.45F) - Object Temp: 33.53C (92.36F)

13:15:55.507: Die Temp: 25.22C (78.39F) - Object Temp: 32.19C (89.94F)

13:15:56.515: Die Temp: 25.22C (78.39F) - Object Temp: 30.94C (87.69F)

13:15:57.508: Die Temp: 25.22C (78.39F) - Object Temp: 31.34C (88.42F)

13:15:58.516: Die Temp: 25.28C (78.51F) - Object Temp: 34.59C (94.27F)

13:15:59.524: Die Temp: 25.34C (78.62F) - Object Temp: 38.72C (101.69F)

13:16:00.532: Die Temp: 25.38C (78.68F) - Object Temp: 41.81C (107.26F)

13:16:01.540: Die Temp: 25.44C (78.79F) - Object Temp: 44.59C (112.27F)

13:16:02.532: Die Temp: 25.50C (78.90F) - Object Temp: 47.03C (116.66F)

13:16:03.540: Die Temp: 25.53C (78.96F) - Object Temp: 48.81C (119.86F)

13:16:04.548: Die Temp: 25.59C (79.07F) - Object Temp: 49.91C (121.83F)

13:16:05.556: Die Temp: 25.62C (79.12F) - Object Temp: 50.91C (123.63F)

13:16:06.563: Die Temp: 25.66C (79.18F) - Object Temp: 51.44C (124.59F)

13:16:07.557: Die Temp: 25.72C (79.29F) - Object Temp: 52.41C (126.33F)

13:16:08.564: Die Temp: 25.75C (79.35F) - Object Temp: 52.94C (127.29F)

13:16:09.572: Die Temp: 25.81C (79.46F) - Object Temp: 54.03C (129.26F)

13:16:10.580: Die Temp: 25.88C (79.58F) - Object Temp: 54.62C (130.32F)

13:16:11.588: Die Temp: 25.91C (79.63F) - Object Temp: 55.19C (131.34F)

13:16:12.596: Die Temp: 25.94C (79.69F) - Object Temp: 55.84C (132.52F)

13:16:13.588: Die Temp: 26.00C (79.80F) - Object Temp: 56.59C (133.87F)

13:16:14.596: Die Temp: 26.06C (79.91F) - Object Temp: 57.34C (135.22F)

13:16:15.604: Die Temp: 26.09C (79.97F) - Object Temp: 58.06C (136.51F)

13:16:16.612: Die Temp: 26.16C (80.08F) - Object Temp: 58.78C (137.81F)

13:16:17.621: Die Temp: 26.22C (80.19F) - Object Temp: 59.47C (139.04F)

13:16:18.613: Die Temp: 26.28C (80.31F) - Object Temp: 60.03C (140.06F)

13:16:19.620: Die Temp: 26.34C (80.42F) - Object Temp: 60.38C (140.68F)

13:16:20.628: Die Temp: 26.41C (80.53F) - Object Temp: 60.84C (141.52F)

13:16:21.636: Die Temp: 26.50C (80.70F) - Object Temp: 60.62C (141.12F)

13:16:22.644: Die Temp: 26.59C (80.87F) - Object Temp: 60.34C (140.62F)

13:16:23.653: Die Temp: 26.69C (81.04F) - Object Temp: 60.22C (140.39F)

13:16:24.644: Die Temp: 26.75C (81.15F) - Object Temp: 60.56C (141.01F)

13:16:25.652: Die Temp: 26.81C (81.26F) - Object Temp: 58.62C (137.53F)

13:16:26.660: Die Temp: 26.78C (81.21F) - Object Temp: 53.47C (128.24F)

13:16:27.669: Die Temp: 26.78C (81.21F) - Object Temp: 48.19C (118.74F)

13:16:28.677: Die Temp: 26.81C (81.26F) - Object Temp: 44.44C (111.99F)

13:16:29.669: Die Temp: 26.81C (81.26F) - Object Temp: 41.47C (106.64F)

13:16:30.677: Die Temp: 26.81C (81.26F) - Object Temp: 39.09C (102.37F)

13:16:31.684: Die Temp: 26.84C (81.32F) - Object Temp: 37.34C (99.22F)

13:16:32.692: Die Temp: 26.84C (81.32F) - Object Temp: 36.00C (96.80F)

13:16:33.700: Die Temp: 26.84C (81.32F) - Object Temp: 34.84C (94.72F)

13:16:34.692: Die Temp: 26.84C (81.32F) - Object Temp: 34.00C (93.20F)

13:16:35.700: Die Temp: 26.84C (81.32F) - Object Temp: 33.25C (91.85F)

13:16:36.708: Die Temp: 26.84C (81.32F) - Object Temp: 32.84C (91.12F)

13:16:37.717: Die Temp: 26.84C (81.32F) - Object Temp: 32.59C (90.67F)

Attachments
Version history
Revision #:
1 of 1
Last update:
‎Mar 28, 2016 12:36 PM
Updated by:
 
Contributors