Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Hardware connections for USB evaluation on CYW943907AEVAL1F

Hardware connections for USB evaluation on CYW943907AEVAL1F

AndrewY_86
Employee
Employee
25 sign-ins 25 replies posted 10 replies posted

To evaluate USB operation on the CYW943907AEVAL1F, the following hardware modification / connections need to be made:

  1. USB Bootstrapping
  2. Power Distribution IC
  3. USB Type A Connector
  4. USB Host/Device Select

 

1. USB Bootstrapping


GPIO_9 is a bootstrapping option to choose between HSIC PHY and USB PHY. Pull this pin up with a 4.7k resistor to enable USB PHY and power cycle the board for the bootstrapping to take effect.

USB/HSIC Sel : 0 = HSIC PHY

                          1 = USB PHY

 

2. Power Distribution IC


When operating as a USB host, it is recommended to use a power distribution IC to control power delivery to the USB device. The USB driver will not function if the power distribution IC is not present.

Wire up an external power distribution IC and make the necessary changes in the platform.h file. A possible option for the power distribution IC is the TPS2051BDBVR, example application circuit pictured below.

In platforms/CYW943907AEVAL1F/platform.h, change

#define WICED_USB_HOST_OVERCURRENT      (WICED_GPIO_NONE) /* No GPIO available, must use controller */

#define WICED_USB_HOST_POWER_ENABLE     (WICED_GPIO_NONE) /* No GPIO available, must use controller */

to

#define WICED_USB_HOST_OVERCURRENT      (WICED_GPIO_1)

#define WICED_USB_HOST_POWER_ENABLE     (WICED_GPIO_2)

pastedImage_0.png

For evaluation purposes, we can bypass the power distribution IC requirement. Doing so will increase the risk of damage to the eval board and the USB device. Proceed with this option only if you accept the risks.

Pull WICED_USB_HOST_POWER_ENABLE pin low through a 10k resistor (based on the pin defined in platform.h)

Pull WICED_USB_HOST_OVERCURRENT pin high through a 4.7k resistor (based on the pin defined in platform.h)

Modify platform.h as mentioned above

pastedImage_0.png

 

3. USB Type A Connector


Device Mode


Option 1 - Using the on-board Micro USB receptacle:

Rework R26 and R56, move both resistors from position A-C to position B-C

pastedImage_0.png

Note: This disconnects the Micro USB receptacle from the FTDI IC, you will not be able download or view UART traces through the USB port until the resistors are moved back to the A-C position. You can still download to the CYW943907 via JTAG and view UART traces using an external UART-USB adapter.

Visit OpenOCD -WICED for instructions on how to download via JTAG

Option 2 - Using a modified USB cable:

Connect a USB cable to the DN/DP signals on the WICED header (J6.43 and J6.44)

Connect USB VCC to VIN_EXT (J9.8) and USB GND to any available ground (J9.6)

Note: This option may affect USB signal integrity

pastedImage_0.png

Host Mode


Option 1 - Using the on-board Micro USB receptacle:

The micro USB receptacle on the CYW943907AEVAL1F eval kit is of type Micro-B. This is sufficient if the CYW943907 is acting as a device, but not as a host.

Replace J5 with a Micro USB Type AB receptacle

Rework R26 and R56, move both resistors from position A-C to position B-C (Same as Device Mode Option 1)

Populate R66 with a 0R resistor. The R66 pads can be found on the underside of the eval board, near the uSD card socket

Use a Micro-A male to Type A receptacle adapter such as USB OTG Cable - Female A to Micro A - 4" - CAB-11604 - SparkFun Electronics​ (Using a Micro-A plug should properly pull USB2_HOST_DEV_SEL high)

If using a power distribution IC, connect the VCC from the USB cable to the 5V output of the IC. Otherwise connect VCC from the USB cable to VIN_EXT (J9.6)

Provide 5V to the DC barrel jack (J8). Make sure the DC power supply is center positive.

Option 2 - Using a modified USB cable:

Connect a USB cable to the DN/DP signals on the WICED header (J6.43 and J6.44)

If using a power distribution IC, connect the VCC from the USB cable to the 5V output of the IC. Otherwise connect VCC from the USB cable to VIN_EXT (J9.6)

Connect USB GND to any available ground (J9.6)

Provide 5V to the DC barrel jack (J8). Make sure the DC power supply is center positive.

Note: This option may affect USB signal integrity

pastedImage_2.png

4. USB  Host/Device Select


The CYW943907 will operate in 'Host' mode or 'Device' mode depending on the state of USB2_HOST_DEV_SEL.

When operating in 'Host' mode, ensure that USB2_HOST_DEV_SEL is pulled low. If using Option 1 for 'Host' mode, manually setting USB2_HOST_DEV_SEL is not necessary when using a proper adapter.

When operating in 'Device' mode, ensure that USB2_HOST_DEV_SEL is pulled high.

USB2_HOST_DEV_SEL Can be found on J6.21

Examples

Examples of USB Host and Device mode applications are available in WICED-Studio 6.1 under snip/usbx_usb_device and snip/usbx_usb_host

1897 Views