Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

CYW20706 SFLASH Layout

CYW20706 SFLASH Layout

Owen_Zhang123
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 250 sign-ins

Introduction

The SFLASH of CYW20706 is divided into the following section based on different purpose and function. There are three types of section:

SS (Static Section), static section used internally by chip firmware. It contains configuration records that don’t change after factory programming.

VS (Volatile Section), volatile section used by the application and the stack to store data. It may be modified frequently.

DS (Data Section), data section used to store application’s executable binary image built from source codes.

 

Section Layout Configuration (WICED SDK 6.2.1 for Example)

 

  1. Flash Layout for non-OTA application

 

The default section layout configuration for non-OTA application is in BTP file. Its path is WICED-Studio-6.2.1.2\20706-A2_Bluetooth\platforms\CYW920706WCDEVAL\CYW920706WCDEVAL_SFLASH.btp.

Owen_Zhang123_0-1637631256548.png

 

SS

VS

DS

UNUSED

4KByte @ 0x0000

4KByte @ 0x1000

500KByte@0x3000

 

The information can also be seen in the generated HEX file. The HEX file follows the intel HEX format:  https://developer.arm.com/documentation/ka003292/1-0

 

:02000004FF00FB

:280000000108006999994204204EB1FD0400FFFFFFFF4006007766556A7020020A000030000000100000001004

:F93000000AFB0000020D009DF8380021463A4600F07CFA044696F88000AAF7CFBA000000F022FC034C044E08B18BF749B98BF73FB90000F850210080D620000248006800F6FD608BF

 

As shown above, the address offset is 0xFF00. There are two parts in the application image: SS section and DS section. The SS section starts from 0x0000. The DS section starts from 0x3000. They are same with the configuration in the BTP file.

 

  1. Flash Layout for OTA Application

 

If the application supports OTA Firmware Upgrade. It will need one more SS section to back up the original configuration, VS section to store customer data and DS section to store the download OTA image.

The flash layout configuration can be found in the file C:\Users\zhxh\Documents\WICED-Studio-6.2.1.2\20706-A2_Bluetooth\libraries\fw_upgrade_lib\fw_upgrade.c as follows:

Owen_Zhang123_1-1637631290743.png

 

We can get the following section layout from the configuration:

 

SS1

SS2

VS1

VS2

DS1

DS2

4KByte@0x00000

4KByte@0x1000

4KByte@0x2000

4KByte@0x3000

248KByte@0x4000

248KByte@0x42000

0 Likes
856 Views