Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AIROC™ Bluetooth SDK Installation Notes

AIROC™ Bluetooth SDK Installation Notes

SaraLeslie
Community Manager
Community Manager
Community Manager
250 sign-ins 100 sign-ins 50 likes received

AIROC™ Bluetooth® SDK

The AIROC™ Bluetooth® SDK is targeted for the CYW20706, CYW20719B2, CYW20721B2, CYW20735B1, CYW20736, CYW30739, CYW20835, CYW20819, CYW20820, CYW89820, CYW43012 Wi-Fi/Bluetooth® combo (for embedded Bluetooth® development only), and CYW5557x Wi-Fi/Bluetooth® combo (for embedded Bluetooth development only). ModusToolbox 2.4 with the AIROC™ Bluetooth® SDK 3.2 provides a complete development environment to allow you to quickly create Bluetooth enabled IoT solutions like audio devices, beacons and trackers, hid devices, smart watches, medical devices, and home automation platforms.

 

The AIROC™ Bluetooth® SDK includes:

  • Bluetooth® firmware
  • Platform and board support packages
  • Utilities including BTSpy trace, Manufacturing Bluetooth® test tool, Client Control, and Mesh Client control
  • Peer apps for OTA and Mesh
  • A rich set of connectivity APIs that allow for simplified programming of Bluetooth® LE/Bluetooth® connectivity
  • Various sample applications that serve as examples of how to utilize the Bluetooth® LE/Bluetooth® APIs
  • More complex code examples  that utilize various APIs and middleware to create a more complete solution

 

Notes for Installing AIROC Bluetooth® SDK 3.2 with ModusToolbox 2.4:

  • Note:  If a previous version of AIROC™ Bluetooth® SDK3.x was installed and needs to be preserved, you will need to create a new workspace project in order to pull in Bluetooth® SDK 3.2 and avoid overwriting previous versions.
  • Within the IDE, click the “New Application” link in the Quick Panel
    • Alternatively, you can select File -> New -> ModusToolbox IDE Application
  • This will launch the Project Creator.  In Project Creator, click on "AIROC™ Bluetooth BSPs"
  • Next, select the evaluation board you are using with AIROC™ Bluetooth SDK
  • Now you will select a template application.
  • Click Create.
  • Click Close.
0 Likes
2058 Views
Comments
Owen_Zhang123
Moderator
Moderator
Moderator
5 questions asked 500 solutions authored 250 sign-ins

Is there a offline package for the BTSDK2.8? When will it be ready?