Browse the Community
RF Transistors
Looking to design a low noise amplifier. Be it in sub GHz frequencies or higher frequencies up to 12 GHz. We have got you covered ! Infineon Technologies offers one of the widest portfolio of radio frequency transistors which offer exceptionally low NF, high gain, and high linearity at low power consumption levels. The transistors could be used in automotive applications (car antenna) , GNSS, Wireless infrastructure , mobile communication infrastructure , consumer appliances such as LCD TV, set-top boxes, industrial electronics such as automation, lighting , and the list goes on. Along with providing a wide portfolio, our products offer outstanding quality and reliability , assuring long term supply while still having an attractive price.
Antenna tuners
With the fast adoption of 5G technology, more antennas need to cover even more frequency bands within limited space. This can potentially affect antenna performance and result in higher design complexity. Antenna tuners help address these challenges to ensure fast and stable wireless connection everywhere. Infineon antenna tuners can be found in a variety of applications, such as smartphones, laptops, smartwatches, mobile routers, smart metering or asset tracking devices. In this forum, you can post your questions about Infineon antenna tuners and the coupler to find support from the community for your next project.
Recent discussions
Hi Infineon,
Could you help to provide the data of IBIS model for BGS12WN6?
Thanks.
Frankie
Hi IFX,
Could you help to provide the data of IBIS model for BGS12WN6?
Thanks.
Frankie
Hello,
I am working on a project to protect our receiver part from unwanted input power and have some amplification on the received signal.
To clarify my question, I want to convert -60dbm to 20dbm to -40 to 0dbm.
I design a system with two SP4T RF switches, but it uses many components and needs a prominent space on a PCB.
I would be grateful if you could kindly let me know your suggestion to convert (-60 up to 20) dBm to (-40 up to 0) dBm.
Best regards,
John
Show LessHello
I'm looking for a transistor to be used for RF amplification, at the single frequency of 2GHz.
The requirements are ~15dB gain, and 15-18 OP1dB.
my preference is to use high Vce (up to 10V) and lower current (15mA max)
Can you please recommend on a part?
Thanks
Show LessIn many of the foundry libraries there are options such as “nmos_rf” in addition to standard “nmos” and their layouts are pre-layed out with a guard ring around them.
This makes them a very bad choice when some kind of matching is required in Gilbert mixer or LC VCO as the transistor pairs cannot be interdigitized. Also I will eventually know every parasitic after I layout my circuit and run a parasitic extraction simulation.
So, my question is do you use rf_transistors in a given process and where is the advantage?
Show LessI have a desire to design some RF amplifiers in the S-band, around 2 GHz, mostly just to understand a little better and learn more how various styles of amplifier work. But the only RF transistors I can find, especially for power amplifiers, seem to be nearly 50$ apiece from Qorvo or Wolfspeed. Are there any cheap RF transistors I could use while I'm learning (maybe silicon instead of GaN or GaAs)? If so, what would be a good source?
I hope to do a Class A, a Class B, a Class C, and maybe a Class E, and my target Psat would be someplace between 0.5 and 5 W.
Thanks!
Show LessHi,
I am component engineer working with Honeywell Aerospace.
Can you please help to share the P1dB Compression Point (dBm) for MPN BF771E6327HTSA1.
hoping to hear from you soon.
Regards,
Rashi
Show LessHi
In many of the foundry libraries there are options such as “nmos_rf” in addition to standard “nmos” and their layouts are pre-layed out with a guard ring around them.
This makes them a very bad choice when some kind of matching is required in Gilbert mixer or LC VCO as the transistor pairs cannot be interdigitized. Also I will eventually know every parasitic after I layout my circuit and run a parasitic extraction simulation.
So, my question is do you use rf_transistors in a given process and where is the advantage?
Show LessHello,
Looking to design a broadband (100MHz to 6GHz) RF front and need an LNA. Generally use High Band only from 2.2GHz to 5.0GHz.
General targets:
- NF: <1dB
- Gain: >15dB
- OP1dB: >+10dBm
- Input no damage: +10dBm
- 3.3V @ 30mA power consumption
Thank you,
Chris
Show LessI need a medium power RF transistor in die form for a high volume hybrid amplifier application. Are parts such as BFP196, BFQ19S or BFR106 available unpackaged?
Show Less