Announcements

Curious on how you can apply Rador Sensors to Smart Home Appliances? Register for the ASEAN Smart Home Appliance Webinar here to find out how.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Radar sensor Forum Discussions

gkmbw
Level 1
10 sign-ins 5 sign-ins First reply posted
Level 1

Hello i use Radar fusion GUI do recording and get the xx.raw.txt data.

# Are_Rx_Antennas_Interleaved = 1
# Modulation_Type_Enum = 1
# Chirp_Shape_Enum = 0
# Lower_RF_Frequency_kHz = 6.0238e+07
# Upper_RF_Frequency_kHz = 6.0762e+07
# Sampling_Frequency_kHz = 1000
# ADC_Resolution_Bits = 12
# Are_ADC_Samples_Normalized = 1
# Data_Format_Enum = 0
# Chirps_per_Frame = 64
# Samples_per_Chirp = 64
# Samples_per_Frame = 12288
# Chirp_Time_sec = 6.89875e-05
# Pulse_Repetition_Time_sec = 0.000505637
# Frame_Period_sec = 0.1

# Frame_Number = 19491
0.4884
0.484005
0.477167
0.47326
0.477656

i know the data (0.484005) from analog signal do ADC convet it to value in [0, 1] in default setting.

while i have some question about the raw data.

=> first question about the data, what does the value 0.484005 or 0.477167 means?

does it means the  amplitude of the size in analog signal after convert to digtial signal?

=> second question, does the radar sensor data can convert to point cloud data, if yes, how can i do that with SDK api.

thanks

 

0 Likes
1 Solution
PalY
Moderator
Moderator 10 likes received 100 sign-ins 50 replies posted
Moderator

Hi @gkmbw ,

1. The raw data that you see in form of float values is the normalized output of ADC., that you see in the figure below. 
Screenshot (375).png

2. For point cloud data, the closest algorithm is Range Angle Image algorithm (having ordinate as range, and abscissa as angle) which is also implemented as a python wrapper in apps/py/examples/range-angle-map.py.Screenshot (374).png

Thanks and regards,
Yashraj

View solution in original post

0 Likes
1 Reply
PalY
Moderator
Moderator 10 likes received 100 sign-ins 50 replies posted
Moderator

Hi @gkmbw ,

1. The raw data that you see in form of float values is the normalized output of ADC., that you see in the figure below. 
Screenshot (375).png

2. For point cloud data, the closest algorithm is Range Angle Image algorithm (having ordinate as range, and abscissa as angle) which is also implemented as a python wrapper in apps/py/examples/range-angle-map.py.Screenshot (374).png

Thanks and regards,
Yashraj

0 Likes