Announcements

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Radar sensor Forum Discussions

Montassar-BR
Radar sensor
We are excited to announce the release of Radar Development Kit 3.5.1, which is now available for download from the Infineon Developer Center.  This r... Show More
Montassar-BR
Radar sensor
Dear Customer, we are happy to announce you the launch of our next generation of XENSIV™ Radar 24GHz DEMO kits with Sense2GoL Pulse and Distance2GoL. ... Show More
user25192
Radar sensor
Hello, I need some help regarding the position2go module. I'm trying to test the "Com_C_lib" example in the package but I'm getting these errors while... Show More
User22573
Radar sensor
Hello, my name is Kevin and I live in Seoul, Korea.I purchased the position2go evaluation board from digikey and am testing it.However, two problems (... Show More
VarunSohal
Radar sensor
Hi all, I am using a RFM69HCW radio and I am attempting to connect it to a Sense2goL pulse radar base board through the SPI interface. When attempting... Show More
checkmateeerree
Radar sensor
Hi all, I've been working on a project that requires distinguishing between cars and pedestrians. So far, I've tried using a speed threshold, but that... Show More
User22177
Radar sensor
I've been given a Sense2GoL Dev kit to research the possibility of several different applications. One of these applications relies on the ability to ... Show More
zhangli
Radar sensor

In BGT24AR4 Datasheet, there are many "see AN358", but i can not find the "Application Note AN358" on the official website? 

maculata
Radar sensor
I have a radar GUI BGT60LTR11AIP shield and the usb micro contoller. I cannot enter advanced mode -- I removed R6 and set R18 = 0 Ohm from the shield.... Show More
h_nakamura
Radar sensor
The TX output power of BGT24LTR11N16 is 2dBm(Min)/6dBm(Typ)/10dBm(Max).  The Tx output power of  BGT24LTR11N16 isn't able to change like BGT24MTR11. A... Show More
checkmateeerree
Radar sensor
Hi all, I recently discovered the Distance2Go L radar as I was looking for an Arduino-compatible FMCW radar so I could get distance information. Is it... Show More
85258
Radar sensor
Hi everyone, I am working with BGT60TR13C demo kit. I'm confusing and I've tried looking in the documentation provided with it, but there's no clear a... Show More
Forum Information

Radar sensor

In this forum you can post your questions, comments and feedback about Infineon's XENSIV™ radar sensors. Designed to support a wide range of industrial, consumer and automotive applications, Infineon’s millimeter wave (mmWave) radar portfolio offers both FMCW and Doppler radar sensors supporting 24GHz, 60GHz, 77/79GHz. Here you can also find the links to the latest board pages, GitHub, documents, tools and FAQs.