Radar sensor Forum Discussions
Dear Customer,
we are happy to announce you the launch of our next generation of XENSIV™ Radar 24GHz DEMO kits with Sense2GoL Pulse and Distance2GoL.
Following the said launch, please be informed that these XENSIV™ Radar 24GHz demo kits are therefore discontinued: Sense2Go, Sense2GoL, Distance2Go and Position2Go.
We are transferring our support capabilities towards the new kits. For the discontinued kits, we will reduce and eventually stop our support including telephone, chat, community support forum, or e-mail inquiries. We apologize for any inconvenience caused.
Please find all needed information on all our 24GHz radar products and kits on www.infineon.com/24ghz.
Sincerely,
Your Infineon team
Hello,
I have a question about CMakelist for motion_angle in "radar_SDK".
I have gotten BGT60TR13C and installed "radar_SDK" from Infineon web site.
I want to generate solution file with CMake application and CMakelist.
However it cannot generate because it have the following error in the Cmakelist for motion_angle.
Error:
- CMake Error at CMakeLists.txt:1 (include):
include could not find requested file:
TargetPlatform
- CMake Error at CMakeLists.txt:4 (detect_target_platform):
Unknown CMake command "detect_target_platform".
Could you please fix the attached Cmakelist file?
Please advise.
Shoko_s
Show LessI would like to make people/object detection system for a vehicle.
Idea is to detects people when the vehicle is going in reverse.
That means vehicle is going to be relatively slowly.
I have demo position2go kit, but I can't seem to configure it to detect reliably.
Sometimes it detects when nothing is there and sometimes it doesn't detect when there is a obstacle/people there.
Is this demo kit capable of reliable detection? Do I just need to better configure it or is there a better solution there?
Please help me, I'm willing to compensate you for your help.
Thanks for any reply in advance. Show Less
Dear Officer,
When I want to install the software of the Distance2Go product, I can not find the Distance2Go Kit. I have also referred to this question(https://community.infineon.com/t5/ModusToolbox-General/Distance2Go-Kit/m-p/364687#M2172) and the handbook for installing the software, but I find nothing.
The only software I can find is 'Distance2GoL' and the SW/HW package is called 'D2GL-HW-SW.exe' not 'D2G-HW-SW.exe' in the pdf. After I had installed the Distance2GoL software, I plugged in the radar and the Radar GUI told me 'Unkown error'.
So, could you give me an installation package for the Distance2Go Kit and 'D2G-HW-SW.exe' such that I can connect my device properly? Please do not give me the pdf link(https://www.infineon.com/dgdl/Infineon-D2G_Application_Note_AN543_v1.5-ApplicationNotes-v01_05-EN.pdf?fileId=5546d4626102d35a01614694b8b04eeb) since it doesn't work!
Thank you very much!
Unkown error
Only Distance2GoL
Hello,
At the moment I only get data when the sensor or the target is in motion.
Is it possible to output the raw data from BGT60LTR11AIP or modulate it to display reflections from standing targets.
Thanks for the effort.
Best regards
Hello. Can you provide full datasheet for radar BGT60TR13C. I'm trying to integrate this radar in our product for object detection, but in datasheet https://www.infineon.com/dgdl/Infineon-BGT60TR13CDataSheet-DataSheet-v01_00-EN.pdf?fileId=8ac78c8c7d718a49017d94bac88e5d43 there is not enough information about registers for sensor configuration.
Show LessHi,
I am confused about the physical meaning of raw data in time domain (Normalized ADC values: the Amplitude in the picture. I want to make use of the raw data to compute the features I need). And what is the meaning of "Range" in Units Configuration?
Show Less
Hello,
I am currently using the Position2Go and found that to increase the number of chirps above 16, I need to decrease the number of samples per chirp in the config.h. If I keep the samples per chirp at 256 while increasing the number of chirps, the extract data C code exits with error "\Debug\Extract_Data.exe (process 9660) exited with code -1." (All the other default values from the config.h are unchanged)
Is there a way to have 64 chirps with 256 samples?
Thank you!
Show Less
Hi,
I am using the Sense2GoL Pulse and trying out the sample codes. When I tried the Radar Pulsed Doppler LED code, it isn't showing any response. The 1st warning is as follows.
WARNING: library BGT24LTR11-Pulsed-Doppler-Radar claims to run on cortex-m4 architecture(s) and may be incompatible with your current board which runs on arm architecture(s).
Afterwards
Library BGT24LTR11-Pulsed-Doppler-Radar has been declared precompiled:
Using precompiled library in C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\libraries\BGT24LTR11-Pulsed-Doppler-Radar\src\cortex-m4
C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\variants\XMC4700\startup_XMC4700.S: Assembler messages:
C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\variants\XMC4700\startup_XMC4700.S:241: IT blocks containing more than one conditional instruction are deprecated in ARMv8
C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\variants\XMC4700\startup_XMC4700.S:272: IT blocks containing more than one conditional instruction are deprecated in ARMv8
C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\libraries\BGT24LTR11-Pulsed-Doppler-Radar\src\cortex-m4\libRadar_S2GL_Pulsed_Doppler_lib.a(datastore_data.o): warning: definition of `ds_default_algo_settings' overriding common
C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\libraries\BGT24LTR11-Pulsed-Doppler-Radar\src\cortex-m4\libRadar_S2GL_Pulsed_Doppler_lib.a(datastore.o): warning: common is here
C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\libraries\BGT24LTR11-Pulsed-Doppler-Radar\src\cortex-m4\libRadar_S2GL_Pulsed_Doppler_lib.a(datastore_data.o): warning: definition of `ds_default_device_settings' overriding common
C:\Users\hasit\AppData\Local\Arduino15\packages\Infineon\hardware\arm\1.4.0\libraries\BGT24LTR11-Pulsed-Doppler-Radar\src\cortex-m4\libRadar_S2GL_Pulsed_Doppler_lib.a(datastore.o): warning: common is here
Sketch uses 72728 bytes (3%) of program storage space. Maximum is 2048000 bytes.
Global variables use 24776 bytes of dynamic memory.
--------------------------
Infineon XMC Flasher Lite
Copyright Infineon Technologies 2017
--------------------------
Windows 10
Operating System: Windows 10
Initialisation
--------------------------
Windows 10
Loading JLink Library...
JLink Library Version: V7.82b
Configuring Device
Device Name : XMC4700-2048
Interface : SWD
Speed : 4000
File Upload
--------------------------
Uploading C:\Users\hasit\AppData\Local\Temp\arduino_build_272415/Radar_Pulsed_Doppler_LED.ino.hex
... Done
--------------------------
... Finished Succesfully
Even so there is no response. Can someone please help out
Show LessHi
We are looking for sensor for people counting application. Please suggest us which solution is good i.e 3D TOF based sensor or radar sensor (60GHz)
Sensor module requirement
- Sensor module should support image sensing and built in data processing algorithm
- External interface: SPI/ USB
- Range (Distance): Above 10 meters
- FOV: Above 90 degree
Regards
K.Gururaja
Show LessHi All,
I wonder if the raw ADC (baseband) data is in I and Q format? I see only one sample per ADC in the documents and not two samples at a time. I would appreciate experts input.
Thanks
Ray
Show Less