Announcements

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Radar sensor Forum Discussions

Montassar-BR
Radar sensor
We are excited to announce the release of Radar Development Kit 3.5.1, which is now available for download from the Infineon Developer Center.  This r... Show More
Montassar-BR
Radar sensor
Dear Customer, we are happy to announce you the launch of our next generation of XENSIV™ Radar 24GHz DEMO kits with Sense2GoL Pulse and Distance2GoL. ... Show More
nDonnelly
Radar sensor
Hi, I have designed a board using the BGT60LTR11AIP motion sensor in SPI mode using XMC, I have set up registers like the example provided in REF BGT6... Show More
shybreak
Radar sensor
用BGT60TR13C在Radar Fusion GUI 采集数据并录制,怎么处理数据啊,得到的文件类型是npy,有三根天线接收到的数据,这三组数据怎么结合呢?
Frank-W
Radar sensor
Hello, I just did a simple test of BGT60TR13C with me sitting still right in front of the radar sensor (~50 cm). I have collected the data for 1 min a... Show More
BYHuang011011
Radar sensor
Hi, I'm currently developing the firmware of a radar system based on BGT60TR13C and STM32H7. I read the instruction of Radar Baseboard MCU 7 but still... Show More
fabulous
Radar sensor
Dear community, I am currently comparing the performance of my custom board using the BGT60ATR24C to the evalualtio board from Infineon (SHIELD_60ATR2... Show More
Skd9
Radar sensor
Hello,I'm trying to run the example c-scripts provided in the sdk using VS22  and face the following error. I should mention that when using the infin... Show More
fbenetello
Radar sensor
Hello, I have a BGT60LTR11AIP device in SPI mode. I am wondering if it is possible to detect human presence even in conditions where the target is imm... Show More
Janis
Radar sensor

Dear developers,

In which frequency range can the frequency of the BGT60LTR11AIP be influenced via the "Vtune" pin?

Thanks

Translation_Bot
Radar sensor
I saw in the data sheet documentation that there are three modes of data flow in FIFO. Does each ADC correspond to an RX antenna? If so, is it necessa... Show More
TinkerML
Radar sensor
Hello everybody! I'm trying to port the BGT60TR13C library at the link https://github.com/Infineon/sensor-xensiv-bgt60trxx for STM32F415 MCU. Almost t... Show More
Forum Information

Radar sensor

In this forum you can post your questions, comments and feedback about Infineon's XENSIV™ radar sensors. Designed to support a wide range of industrial, consumer and automotive applications, Infineon’s millimeter wave (mmWave) radar portfolio offers both FMCW and Doppler radar sensors supporting 24GHz, 60GHz, 77/79GHz. Here you can also find the links to the latest board pages, GitHub, documents, tools and FAQs.