Announcements

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
mjdesrosiers
Level 1
Level 1
First question asked Welcome!

Hello, I'm trying to determine if an Infineon radar product might work for my application. I need to measure the velocity of an object moving at ~1000 m/s.

Can either the BGT24LTR11 or BGT60LTR11AIP measure objects moving so fast? I'm thinking of using a CW mode for simplicity's sake.

 

Thanks,

Michael

0 Likes
1 Solution
Siddharth_H
Moderator
Moderator
Moderator
100 solutions authored 50 likes received First question asked

Hi @mjdesrosiers ,

The maximum speed you can measure with BGT60TR13C is ~112 m/s, so it is not possible to measure such high speeds of upto 1000 m/s. BGT24LTR11 or BGT60LTR11AIP can also not measure speeds of 1000 m/s.

Thankyou,

Siddharth.

View solution in original post

0 Likes
1 Reply
Siddharth_H
Moderator
Moderator
Moderator
100 solutions authored 50 likes received First question asked

Hi @mjdesrosiers ,

The maximum speed you can measure with BGT60TR13C is ~112 m/s, so it is not possible to measure such high speeds of upto 1000 m/s. BGT24LTR11 or BGT60LTR11AIP can also not measure speeds of 1000 m/s.

Thankyou,

Siddharth.

0 Likes