Announcements

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
stjischl
Level 1
Level 1
5 questions asked 5 replies posted 10 sign-ins

Hi,

I am curious about the location of the transmitting antenna of BGT60TR13C.

stjischl_0-1706963411621.png

From the diagram in the application notes, we can see that the antennas are not in a perfect grid.
In fact Tx is breaking the grid in only one axis. It's on the same height as Rx2, but a different width that Rx1.

What is the reason behind that?

Thanks

0 Likes
1 Solution
Deepa_V
Moderator
Moderator
Moderator
50 likes received 250 replies posted 5 likes given

Hi @stjischl ,

When oriented as in the figure, the radar sensor will emit vertical polarization. Thus, the E-plane is vertical and the H-plane is horizontal. The free-space wavelength of 60 GHz, denoted by lambda, is about 5 mm. The horizontal spacing between receive antenna 1 (Rx1) and receive antenna 3 (Rx3) as well as the vertical spacing between receive antenna 2 (Rx2) and Rx3 is lambda over 2. This enables angular measurements perpendicular to the chips surface providing a horizontal range of ±90° using Rx1 and Rx3 and a vertical range of ±90° using Rx2 and Rx3 respectively.

The other geometric changes were made considering the Directivity, Antenna gain, scan angle and maximum isolation between the transmitter and receiver antenna. 

Best Regards,

Deepa

View solution in original post

1 Reply
Deepa_V
Moderator
Moderator
Moderator
50 likes received 250 replies posted 5 likes given

Hi @stjischl ,

When oriented as in the figure, the radar sensor will emit vertical polarization. Thus, the E-plane is vertical and the H-plane is horizontal. The free-space wavelength of 60 GHz, denoted by lambda, is about 5 mm. The horizontal spacing between receive antenna 1 (Rx1) and receive antenna 3 (Rx3) as well as the vertical spacing between receive antenna 2 (Rx2) and Rx3 is lambda over 2. This enables angular measurements perpendicular to the chips surface providing a horizontal range of ±90° using Rx1 and Rx3 and a vertical range of ±90° using Rx2 and Rx3 respectively.

The other geometric changes were made considering the Directivity, Antenna gain, scan angle and maximum isolation between the transmitter and receiver antenna. 

Best Regards,

Deepa