Announcements

Curious on how you can apply Rador Sensors to Smart Home Appliances? Register for the ASEAN Smart Home Appliance Webinar here to find out how.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Radar sensor Forum Discussions

TommyS
Level 1
First like given First question asked Welcome!
Level 1

 Anyone has technical recommendations for a low--cost  (24GHz+) radar sensor that can be incorporated into a device that measures the velocity of a single small metal object?  

Here are the parameters:
single small solid metal object, such as lead pellets/balls, between 4.5mm to 8.5mm diameter
- distance envelope of object from radar sensor: 12cm-2m traveling away from sensor at zero angle
-velocity: minimum:  200 km/h - 1300 km/h   (prefer 200-km/h to 4800 km/h)        /200 fps-1110 fps  or  200 fps - 4500 fps/
 
What would be the detection-zone of such radar in front of the sensor for such a small object?  For example:  the radar can measure a 4.5mm diameter object from 25cm-65cm (that would be a 40cm long detection-zone) in front of the sensor.
0 Likes
1 Solution
HoneyDhandhukia
Moderator
Moderator 5 likes given 250 sign-ins 25 solutions authored
Moderator

Hello @TommyS ,

All our products are designed and tested for human target (RCS) detection. Thus, they have not been tested for such high velocity and smaller objects. Please go through our product selection guide for 24GHz radar sensors documentation and boards.

You can also refer to the following thread for similar content for 24GHz radar sensors. Thread: https://community.infineon.com/t5/Radar-sensor/Doppler-radar-sensor/td-p/343330 

Best Regards,

Honey

View solution in original post

1 Reply
HoneyDhandhukia
Moderator
Moderator 5 likes given 250 sign-ins 25 solutions authored
Moderator

Hello @TommyS ,

All our products are designed and tested for human target (RCS) detection. Thus, they have not been tested for such high velocity and smaller objects. Please go through our product selection guide for 24GHz radar sensors documentation and boards.

You can also refer to the following thread for similar content for 24GHz radar sensors. Thread: https://community.infineon.com/t5/Radar-sensor/Doppler-radar-sensor/td-p/343330 

Best Regards,

Honey