- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
I 'm using SPI mode to configure the parameters for the radar sensor .
I am configuring the following :
FREQUENCY_61_1HZ_VALUE = 0xF72,
PULSE_WIDTH_5MICRO_S = 0x00,
DUTY_CYCLE_REPETITION_250MICRO_S = 0x00,
TX_POWER_DBM_4_5 = 0x07,
PGA_10_DB = 0x00,
HOLD_TIME_1S = 0x08,
SENSITIVITY_1 = 0x0780,
Everything worked steadily until I configured the sensitivity to pass level 8
Although there are no detected objects in the detection area , TDet pin are constantly fluctuating at the detection level and are not detected.
Is it interference? , do you have a solution to this problem?
Solved! Go to Solution.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @trung,
Please note that there is no need to make changes to PLL frequency word and Medium power gain amplifier gain control.
As already suggested you can set the sensitivity/threshold for the required range and set the Baseband PGA gain at the maximum possible value such that there are no false detections. Set at the maximum value of gain and try reducing the gain to achieve a level where there are no false detections. In the given application as already mentioned, PGA gain can be kept at 35 dB.
Thanks and regards,
George
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @trung,
I believe you are referring to BGT60LTR11AIP.
Could you please let me know whether "pass level 8" refers to sensitivity_8?
If that is the case, the sensitivity is very high at sensitivity_8. The radar can detect movement at farther points compared to the performance at sensitivity_1. The testing should be done more carefully at this level. After setting the threshold you can try approaching from a farther point and please avoid all the other movements in the radar range.
Please let me know whether the suggestion helped in getting the issue solved.
Thanks and regards,
George
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @George_T
Thanks for your answer!
I tried with a sensitivity of 8,9,10,11,12,13,14. TDet signal pin jumps between 2 levels 0-1 when there is no object in the zone
This my config Pulsed Mode for register of BGT60LTR11AIP with spi communication
Did I write the value to the register of the radar like that ? Is there a problem with it?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @trung,
I tried configuring the BGT60LTRAIP mmic via SPI with the settings shared and is working fine. So there is no issue with the register configuration. So the issue could be with the measurement environment.
At this level of sensitivity (0x0050) radar will detect very fine movements at a distance more than 6 m. Hence in the measurement setup please ensure there is no unwanted movements in this range.
I would suggest to start with sensitivity_4 (0x0280), which is already working, for which the range is less. Increase the sensitivity levels in steps keeping in mind that detection range also increases. Avoid unwanted movements in the radar range so that radar can detect the actual movement.
One other suggestion is to set the Register 15 to 0x4000 instead of 0x4020, while setting for the second time. It will just make the TDet active low.
Please let me know the results.
Thanks and regards,
George
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @George_T
Thanks for Your answer!
Can you give me suggestions for configuring Radar 's registers.
Detection range : 5m, 3m, 2m.
Ceiling mounting location.
Capable of detecting small movements.
Example:
- The one who sits and reads the book
- People who work with laptops
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @trung ,
You could use table 5 (page no: 7) in User's guide to BGT60LTR11AIP as reference for setting the threshold register (Register-2) for required radar range.
As mentioned in the document each entry has 0.5 m range more than the previous value. For example, the value of 0x0380 (896) can be chosen for a range of 2 m and a value of 0x00C0 (192) for range of 5 m. Please note that these are not exact values, but can be used as reference. Some tuning is required for achieving the required range.
Thanks and regards,
George
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @George_T
Thanks for your answer!
What is Baseband PGA gain?
When I configurate PGA down level from 10 ->35 DB with Sensitivity 8 ->15.
No interference occurs when reading signals from Tdet pins.
When I tried to configure PGA: 40-45-50 DB with Sensitivity of 8- 14, The signal read form Tdet is constantly being changed when there is no object in the zone.
Could the cause the circuit design by me is not responsive to high power when PGA with level 40-45-50?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @trung,
Happy to know that the radar is responding properly.
PGA refers to Programmable Gain Amplifier, which amplifies the received signal.
A higher gain can cause false detection which may be happening in your case.
Thanks and regards,
George
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @George_T
Thanks for your answer!
These are parameters that affect the object detection distance .
- PLL frequency word
- Medium power amplifier gain control
- Baseband PGA gain setting
- Sensitivity
So what parameters should I adjust to reduce the object detection distance so that the Radar works well with high sensitivity and stability?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi @trung,
Please note that there is no need to make changes to PLL frequency word and Medium power gain amplifier gain control.
As already suggested you can set the sensitivity/threshold for the required range and set the Baseband PGA gain at the maximum possible value such that there are no false detections. Set at the maximum value of gain and try reducing the gain to achieve a level where there are no false detections. In the given application as already mentioned, PGA gain can be kept at 35 dB.
Thanks and regards,
George