Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Radar sensor Forum Discussions

AEnes
Level 1
Level 1
10 sign-ins First like given 5 sign-ins

Hi everyone,

I want to develop a circuit like "sense2gol" card but I need a more documentions and to begin scheamatics so if you have more docs and schematics design please write a comment.

 

Thanks everyone.

Regrads.

0 Likes
1 Reply
Deepa_V
Moderator
Moderator
Moderator
First like given 25 likes received 50 solutions authored

Hi @AEnes ,

Do you have the same MMIC used in Sense2GoL demo board which is BGT24LTR11 and the same  32-bit ARM® Cortex™-M0 based XMC1302 microcontroller in mind for your development? If yes, please note that the Sense2GoL board has been discontinued from our end (Ref: https://community.infineon.com/t5/Radar-sensor/Discontinued-Products-XENSIV-Radar-mmWave-24GHz-DEMO-... )and hence, we would not be able to provide you with the associated hardware files and the only documents available would be the Application Note AN597 which you can use as reference. 

If you are not particular about the Microcontroller, then you can use the newer demo board Sense2GoL Pulse  for the reference design which uses BGT24LTR11 MMIC with XMC4700 Microcontroller. For the hardware files on the same, Please install the Radar Sense2GoL Pulse package from the Infineon Developer Center and navigate to C:\IFX_S2GLP-HW-SW_V2.0.0\Hardware.

Hope this helps !

Best Regards,

Deepa

0 Likes