Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Radar sensor Forum Discussions

MathieuC
Level 1
First reply posted First like given First question asked
Level 1

Hi every one,

My questions are about the KIT BGT60TR13C EMBEDD( https://www.youtube.com/watch?v=pUuSCDY14nw)

By downloading the config tool on this page, one can raise an alarm if a presence is detected. Also, the config tool returns the range of the detection.

My objective is to get the raw data from the MADC integrated in the BGT60TR13C chip with this KIT BGT60TR13C EMBEDD.

Is it possible ?

I don't know if it is possible because I think that puzzle pieces are missing:

- I have downloaded  the modus toolbox and the BSP of this product  is available in the project creator under PSoC6 BSPs but there is only an HelloWorld and an empty project, there is no project allowing presence detection.

- The config tool available online allows to reflash the board, but I could not find the bin file firmware anywhere on the web. Does anyone manage to find a firmware for this board and reflash the board with it ?

- Also, I could not find the board schematic. I only know that the MCU is a PSoC6, that the radar chip is the BGT60TR13C and that those two components are linked with SPI communication. 

 

Thank you very much in advance for your help

0 Likes
3 Replies
HoneyDhandhukia
Moderator
Moderator 25 solutions authored 50 replies posted 10 likes received
Moderator

Hello @MathieuC ,

The KIT BGT60TR13 EMBEDDED comprises of PSoC6 MCU, you can flash your own firmware to process the data.

Yet we are looking into the query from our end and will get back to you soon!

Meanwhile please refer to the Presence detection and sensing solution and KIT CSK BGT60TR13C as reference which consist of the same components(PSoC6 and BGT60TR13C).

Also go through the document for further information on the board:https://www.infineon.com/dgdl/Infineon-Infineon-XENSIVTM_KIT_CSK_BGT60TR13C-UserGuide-UserManual-v01... 

Hope this helps!

Best Regards,

Honey 

HoneyDhandhukia
Moderator
Moderator 25 solutions authored 50 replies posted 10 likes received
Moderator

Hello @MathieuC ,

What kind of firmware you require for flashing on the kit ? 

Regards,

Honey

0 Likes
MathieuC
Level 1
First reply posted First like given First question asked
Level 1

Hi Honey,

I need the firmware PresenceDetect_1.3.0 (156a4bc). It is the firmware currently on the board as returned by the config tool (see screenshot joined).

Do you know where I can find it ?

Would it be possible to obtain the source code of this  firmware as an example helping programming the KIT BGT60TR13C EMBEDD ? 

There is only an hello world and an empty app in the ModusToolbox (see screenshots joined)

Thank you very much for your reply. It helps a lot.

0 Likes